<?xml version="1.0" encoding="utf-8"?><PCNbody xmlns:xsd="http://www.w3.org/2001/XMLSchema" xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns="http://www.smartpcn.org/images/files/VDMA24903Schema/PCNbody"><masterData pcnFormatVersion="SmartPCN_3.08"><pcnNumber>000000299681</pcnNumber><pcnTitle>CPV10&amp;14 customer request - update</pcnTitle><pcnAlertType>Minor</pcnAlertType><pcnType>PCN</pcnType><pcnMfrName>Festo SE &amp; Co. KG</pcnMfrName><pcnProductCategory>DOCU</pcnProductCategory><pcnIssueDate>2026-01-05</pcnIssueDate><pcnAddInfo> -</pcnAddInfo><pcnRevision>1</pcnRevision><contacts><contact pcnContactType="Manufacturer"><pcnCustomerNumber> -</pcnCustomerNumber><pcnDunsNumber>123456789</pcnDunsNumber><pcnBusinessUnit> -</pcnBusinessUnit><pcnCompany>Festo SE &amp; Co. KG</pcnCompany><pcnEmail>productchange@festo.com</pcnEmail><address><pcnStreet>Ruiter Straße 82</pcnStreet><pcnZipCode>73734</pcnZipCode><pcnCity>Esslingen</pcnCity><pcnCountry>DE</pcnCountry></address></contact></contacts></masterData><difference><pcnChangeTitle>CPV10&amp;14 customer request - update</pcnChangeTitle><pcnChangeDetail>In connection with customer request there is need to be included the following 
changes on the CPV modules that are covering exchange from REV. 9  to REV. 10 
After switching on and off from the PL the device stop to respond. This behavior 
should be solved with Rav 10.

</pcnChangeDetail><pcnRiskAssessment> -</pcnRiskAssessment><pcnFirstDelivery>2026-04-01</pcnFirstDelivery><pcnFeedbackUntil>2026-04-01</pcnFeedbackUntil><pcnChangeIdentificationMethod>decreased the impedance of FB (IC1 pin 2). Divider is decreasing the noise on FB, 
which was causing an unexpected reset of during Dark tests, respectively - locking 
the CPV device. 
Also with the change will be removal one resistor: This update is preventing the 
discharge of capacitor, through transistor during short drops of PL (e.g. detected 
during performing Siemens&apos;Dark test).
And last is integration of SW update: Reg 0x6, bit 7 was wrongly set to &quot;1&quot;, which 
was disabling LDO, decreasing the pressure on it to 2,75 V. This is making the 
device more noise resistant.</pcnChangeIdentificationMethod><pcnEffectiveDate>2026-04-01</pcnEffectiveDate></difference><ItemNumbers><ItemNumber><itemMfrNumber>000000000001564984</itemMfrNumber><itemMfrTypeIdent>CPV14-GE-PT-8</itemMfrTypeIdent><itemMfrName>El. interface   CPV14-GE-PT-8</itemMfrName><itemCategory>RAWM</itemCategory><itemRev>9</itemRev><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FUNCT"><itemChangeText>FUNCTION</itemChangeText></itemChange><itemChange itemChangeType="CHARA"><itemChangeText>CPV</itemChangeText></itemChange></itemChanges></ItemNumber><ItemNumber><itemMfrNumber>000000000001565761</itemMfrNumber><itemMfrTypeIdent>CPV10-GE-PT-8</itemMfrTypeIdent><itemMfrName>El. interface   CPV10-GE-PT-8</itemMfrName><itemCategory>RAWM</itemCategory><itemRev>9</itemRev><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FUNCT"><itemChangeText>FUNCTION</itemChangeText></itemChange><itemChange itemChangeType="CHARA"><itemChangeText>CPV</itemChangeText></itemChange></itemChanges></ItemNumber><ItemNumber><itemMfrNumber>000000000008193248</itemMfrNumber><itemMfrTypeIdent>CPV10-FB-8-IO-L</itemMfrTypeIdent><itemMfrName>Flat module     CPV10-FB-8-IO-L</itemMfrName><itemCategory>RAWM</itemCategory><itemRev>9</itemRev><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FUNCT"><itemChangeText>FUNCTION</itemChangeText></itemChange></itemChanges></ItemNumber><ItemNumber><itemMfrNumber>000000000008193251</itemMfrNumber><itemMfrTypeIdent>CPV14-FB-8-IO-L</itemMfrTypeIdent><itemMfrName>Flat module     CPV14-FB-8-IO-L</itemMfrName><itemCategory>RAWM</itemCategory><itemRev>9</itemRev><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FUNCT"><itemChangeText>FUNCTION</itemChangeText></itemChange></itemChanges></ItemNumber><ItemNumber><itemMfrNumber>000000000008231268</itemMfrNumber><itemMfrTypeIdent>CPV10-FB-8-IO-L:PD</itemMfrTypeIdent><itemMfrName>Flat module     CPV10-FB-8-IO-L:PD</itemMfrName><itemCategory>RAWM</itemCategory><itemRev>9</itemRev><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FUNCT"><itemChangeText>FUNCTION</itemChangeText></itemChange></itemChanges></ItemNumber><ItemNumber><itemMfrNumber>000000000008231269</itemMfrNumber><itemMfrTypeIdent>CPV14-FB-8-IO-L:PD</itemMfrTypeIdent><itemMfrName>Flat module     CPV14-FB-8-IO-L:PD</itemMfrName><itemCategory>RAWM</itemCategory><itemRev>9</itemRev><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FUNCT"><itemChangeText>FUNCTION</itemChangeText></itemChange></itemChanges></ItemNumber></ItemNumbers><pcnLifeCycleData><pcnSOP>2026-04-01</pcnSOP><pcnEOS>2026-04-01</pcnEOS><pcnEOPeffDate>2026-04-01</pcnEOPeffDate><pcnLTD>2026-04-01</pcnLTD><pcnEOSR>2026-04-01</pcnEOSR></pcnLifeCycleData></PCNbody>