Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA - 202305 - Security Advisory - Vulnerable Wibu CodeMeter Runtime in Several Festo Products

A vulnerability in the Wibu CodeMeter Runtime, which is part of the installation packages of several Festo products, was found.

 

An attacker exploiting the vulnerability in WIBU CodeMeter Runtime in server mode could gain full access to the affected server via network access without any user interaction. This could lead to remote code execution and escalation of privileges giving full admin access on the host system for an already authenticated user (logged in locally to the PC).

1.1.0
FSA-202206 - Security Advisory - Vulnerable WIBU-SYSTEMS CodeMeter Runtime Vulnerable WIBU-SYSTEMS CodeMeter Runtime in multiple Festo products
1.0.1
Designer Studio 21 CFR Part 11 Compliance Designer Studio 21 CFR Part 11 Compliance

Designer Studio includes a set of functions for responding to the requirements specified in FDA 21 CFR Part 11. The standard is in-tended to provide a solution for securely handling electronic records and electronic signatures in industrial applications.

1.10
09/02/2026
Festo AX Energy Insights Festo AX Energy Insights

This document describes how to set up AX Energy Insights from connectivity to asset onboarding and monitoring of electrical and pneumatic energy consumption

1.20
03/12/2025
Festo AX Energy Insights Node-RED pneumatic data from CPX-AP-I with Modbus TCP Festo AX Energy Insights Node-RED flow: Getting pneumatic data from Festo CPX-AP-I-EP with Modbus TCP protocol

This document describes how to get the pneumatic data from the Festo CPX-AP-I-EP with the Modbus TCP protocol.

 

1.20
09/03/2026
Festo AX Energy Insights Node-RED: energy data from Sentron/MA770 with Modbus Festo AX Energy Insights Node-RED flow: Getting energy data from Siemens Sentron PAC or Phoenix Contact MA770 with Modbus protocol

This document describes how to get electric data from the Siemens Sentron PAC 2200/3200/4200 and Phoenix Contact MA770 with the Modbus protocol.

 

1.10
13/12/2025
Festo AX Motion Insights Pneumatic General Information for set-up and monitoring MIP

This document describes how to set up AX Motion Insights Pneumatic from connectivity to asset onboarding and monitoring of pneumatic actuators.

1.70
06/11/2025
Festo Motion Package - User Guide Festo Motion Package - User Guide

A guide to commission and program single axis using Festo Motion Package in Festo edge controller CEPE. Drive used is a CMMT-AS-C2-3A-MP-S1.

Other quick start guide shows the steps to get an example system working with Festo Robotic as part of Festo Motion Package. In the end user will be able to start programming his own application.

1.20
12/02/2026