Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202406 - Security Advisory - Several Codesys Gateway v2 vulnerabilities in Codesys provided by Festo

An unauthenticated attacker would be able to send crafted requests to cause the CODESYS Gateway Server V2 to allocate excessive memory or consume all available TCP client connections. Besides, passwords are insufficiently checked during login.

 

All versions of the following CODESYS V2 product prior version V2.3.9.38 are affected:

 

• CODESYS Gateway Server


The identified vulnerabilities could lead to denial-of-service attacks, exhaustion of TCP connections, and unauthorized access to the system.

2.0.0
Designer Studio 21 CFR Part 11 Compliance Designer Studio 21 CFR Part 11 Compliance

Designer Studio includes a set of functions for responding to the requirements specified in FDA 21 CFR Part 11. The standard is in-tended to provide a solution for securely handling electronic records and electronic signatures in industrial applications.

1.10
09/02/2026
Festo AX Energy Insights Festo AX Energy Insights

This document describes how to set up AX Energy Insights from connectivity to asset onboarding and monitoring of electrical and pneumatic energy consumption

1.30
29/05/2026
Festo AX Energy Insights Node-RED pneumatic data from CPX-AP-I with Modbus TCP Festo AX Energy Insights Node-RED flow: Getting pneumatic data from Festo CPX-AP-I-EP with Modbus TCP protocol

This document describes how to get the pneumatic data from the Festo CPX-AP-I-EP with the Modbus TCP protocol.

 

1.30
24/07/2026
Festo AX Energy Insights Node-RED: energy data from Sentron/MA770 with Modbus Festo AX Energy Insights Node-RED flow: Getting energy data from Siemens Sentron PAC or Phoenix Contact MA770 with Modbus protocol

This document describes how to get electric data from the Siemens Sentron PAC 2200/3200/4200 and Phoenix Contact MA770 with the Modbus protocol.

 

1.20
24/07/2026
Festo AX Motion Insights Pneumatic General Information for set-up and monitoring MIP

This document describes how to set up AX Motion Insights Pneumatic from connectivity to asset onboarding and monitoring of pneumatic actuators.

1.80
29/05/2026
Festo Motion Package - User Guide Festo Motion Package - User Guide

A guide to commission and program single axis using Festo Motion Package in Festo edge controller CEPE. Drive used is a CMMT-AS-C2-3A-MP-S1.

Other quick start guide shows the steps to get an example system working with Festo Robotic as part of Festo Motion Package. In the end user will be able to start programming his own application.

1.40
14/10/2026
Motion Insights Pneumatic Function Block for Festo PLC Motion Insights Pneumatic Function Block for Festo PLC; Library is included

This Application Note explains about Motion Insights Pneumatic function block and also shows integration of function block in CODESYS software.

1.10
23/10/2026
Set Date and Time for Festo PLC CECC; FDT; Codesys, Putty

How to read and write Date & Time from the command prompt.

1.10
08/01/2019