Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202208 - Security Advisory - Unsafe default Codesys configuration Multiple Festo products contain an unsafe default Codesys configuration

The products are shipped with an unsafe configuration of the integrated CODESYS Runtime environment. In this case no default password is set to the CODESYS PLC and therefore access without authentication is possible.

 

With a successful established connection to the CODESYS Runtime the PLC-Browser commands are available. Thus granting the possibilities to e.g. read and modify the configuration file(s), start/stop the application and reboot the device.

1.0.1
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
FSA-202401 - Security Advisory - Several Codesys Vulnerabilities in Festo Products

Several high severity vulnerabilities in CODESYS V3 affecting Festo products could lead to Remote Code Execution or Denial of Service.

1.0.0
FSA-202602: Multiple OpenSSL vulnerabilities affect Festo AX OS in CEPE

Festo AX OS versions 25.0.1.46 and 25.9.2.4, which are based on PLCnext by Phoenix Contact, used by the Festo product CEPE are affected by multiple OpenSSL vulnerabilities. The vulnerabilities are identified as CVE-2025-15467 and CVE-2025-69419. Attacks may be possible when maliciously crafted firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects are uploaded and processed by the affected system. In the device context, exploitation typically requires a logged-in user with high privileges or the processing of attacker-supplied cryptographic objects.

 

A successful attack using manipulated firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects may lead to memory corruption, application crash, or denial of service. Depending on the affected code path, execution context, platform protections, and toolchain mitigations, execution of malicious code may be possible. This can jeopardize confidentiality, integrity, and availability of the affected system.

1.0.0
CDPX serial communication and configuration using Fuction Blocks and CodeSys V3.5 CDPX-X-A-W-7; Example project included

This document explains how you will Send and Receive data in CDPX Panel by using Serial communication RS-232 using CODESYS V3.5 SP12.

1.10
02/03/2020
CDPX-X-B-W-xx Manual CDPX-X-B-W-xx Manual

This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.

1.30
13/03/2023
CDPX-X-E1-W-xx Manual CDPX-X-E1-W-xx Manual

This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.

1.30
13/03/2023
CDPX-X-E2-W-5-EX2 Manual CDPX-X-E2-W-5-EX2 Manual

This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.

1.30
11/02/2025
CDPX-X-E2-W-xx-EX2 Manual CDPX-X-E2-W-xx-EX2 Manual

This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.

1.30
11/02/2025
Checkbox CHB-C-N Telnet communication CHB-C-N; CheckKon; Designer Studio

This Application Note give an example for the Checkprogram

selection by telnet communication. Further on it shows how to influence different system parameter setting by telnet access.

1.10
01/03/2018
CMMT-AS Servo Drive Parametrization via CDSB-A1 Operator Unit CMMT-AS; CDSB-A1

This document describes how to export parameter sets from the Festo Automation Suite CMMT-AS Plug-in to a CDSB-A1 operating panel, download it to the drive and activate it.

1.10
17/09/2019
CMMT-AS-MP Servo Drive Control with Festo CDPX-X-E1-W-xx Operator Panel through Profinet CMMT-AS-MP; Festo CDPX-X-E1-W-xx; Profinet; Sample Code included

This application note explains how to control the CMMT-AS servo drive via Profinet network in Festo CDPX-E operator panels. The user will be able to control the Festo drives in point to-point mode using the sample code provided. The manual refers to the following models CDPX-X-E1-W-7, CDPX-X-E1-W-10 and CDPX-X-E1-W-15.

1.10
11/01/2024
Commissioning of CMMO-ST-C5-1-LKP CTEU-EP and CAPC via Logix Designer CMMO-ST-C5-1-LKP; CTEU-EP; CAPC-F1-E-M12

The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP in I-Port mode with CTEU-EP and CAPC-F1-E-M12 via Logix Designer.

1.10
13/06/2016
Commissioning of CMMO-ST-C5-1-LKP in I-Port mode with CTEU-PN and CAPC-F1-E-M12 via TIA Portal V13 CMMO-ST-...-LKP; CTEU-PN; CAPC-F1-E-M12

 

 

The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP in I-Port mode with CTEU-PN and CAPC-F1-E-M12 via TIA Portal V13

1.10
25/04/2016
Designer Studio CDPX; Designer Studio 2.0

Praxis tips

1.10
28/02/2017
Designer Studio 21 CFR Part 11 Compliance Designer Studio 21 CFR Part 11 Compliance

Designer Studio includes a set of functions for responding to the requirements specified in FDA 21 CFR Part 11. The standard is in-tended to provide a solution for securely handling electronic records and electronic signatures in industrial applications.

1.10
09/02/2026
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
EtherNet/IP IO-Link Integration CTEU-EP, CPX-FB36, CPX-CTEL-LK

Controlling IO-Link Devices with Festo EtherNet/IP Products

1.30
28/07/2016
How to implement data exchange between CDPX and MSSQL databases How to implement data exchange between CDPX and MSSQL databases

This application note helps the user to implement data exchange between CDPX and MSSQL databases.

1.10
06/03/2026
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
OPC UA communication between Siemens PLC and Festo CDPX Panels OPC UA communication, Siemens TIA PLC, CDPX; Sample project included

This application note helps the user to establish OPC UA communication between Siemens TIA PLC and Festo CDPX panels.

1.30
03/01/2025
Security white paper for Festo controllers

This document is intended to provide users of Festo control products with an introduction and support on how Festo controllers can be used as securely as possible from the point of view of cyber security.

V03
25/05/2023
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.