|
|
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols
Incomplete documentation of remote accessible functions and protocols in Festo products
Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.
Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.
|
1.2.1
|
Security AdvisoryFile and language versions
|
|
|
FSA-202602: Multiple OpenSSL vulnerabilities affect Festo AX OS in CEPE
Festo AX OS versions 25.0.1.46 and 25.9.2.4, which are based on PLCnext by Phoenix Contact, used by the Festo product CEPE are affected by multiple OpenSSL vulnerabilities. The vulnerabilities are identified as CVE-2025-15467 and CVE-2025-69419. Attacks may be possible when maliciously crafted firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects are uploaded and processed by the affected system. In the device context, exploitation typically requires a logged-in user with high privileges or the processing of attacker-supplied cryptographic objects.
A successful attack using manipulated firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects may lead to memory corruption, application crash, or denial of service. Depending on the affected code path, execution context, platform protections, and toolchain mitigations, execution of malicious code may be possible. This can jeopardize confidentiality, integrity, and availability of the affected system.
|
1.0.0
|
Security AdvisoryFile and language versions
|
|
|
CANopen in CODESYS V3
CODESYS V3, CPX-FB14, CTEU-CO, CMMP-...-M0/M3, EMCA-CO
This document describes what each CAN parameter in the CODESYS V3 programming environment does, as well as show the available Function Blocks to implement diagnostics or pa-rameterization within the PLC’s Task.
|
1.10 04/08/2017
|
Application NoteFile and language versions
|
|
|
Commissioning of CMMO-ST-C5-1-LKP CTEU-EP and CAPC via Logix Designer
CMMO-ST-C5-1-LKP; CTEU-EP; CAPC-F1-E-M12
The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP in I-Port mode with CTEU-EP and CAPC-F1-E-M12 via Logix Designer.
|
1.10 13/06/2016
|
Application NoteFile and language versions
|
|
|
Commissioning of CMMO-ST-C5-1-LKP in I-Port mode with CTEU-PN and CAPC-F1-E-M12 via TIA Portal V13
CMMO-ST-...-LKP; CTEU-PN; CAPC-F1-E-M12
The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP in I-Port mode with CTEU-PN and CAPC-F1-E-M12 via TIA Portal V13
|
1.10 25/04/2016
|
Application NoteFile and language versions
|
|
|
Commissioning of CTEU-EP in Modbus/ TCP mode
CTEU-EP; VAEM-L1-S-8-PT; SPAU-..-LK-..
This application node includes examples how to establish a Modbus/TCP communication with the CTEU-EP node.
|
1.10 28/03/2017
|
Application NoteFile and language versions
|
|
|
CTEU-EP + VTUG Valve Terminal with Emerson DeltaV using Ethernet/IP Protocol
CTEU-EP + VTUG Emerson DeltaV Ethernet/IP Protocol Example project included
This application note gives detailed explanation of integration procedure and library for Festo VTUG + CTEU-EP which allows user to integrate & control VTUG + CTEU-EP with Emerson DeltaV DCS using EtherNet/IP protocol
|
1.10 21/06/2023
|
Application NoteFile and language versions
|
|
|
CTEU-EP + VTUG Valve Terminal with Emerson DeltaV using Modbus TCP
CTEU-EP + VTUG Emerson DeltaV using Modbus TCP; Example project included
This application note gives detailed explanation of integration procedure and library for Festo VTUG + CTEU-EP which allows user to integrate & control VTUG + CTEU-EP with Emerson DeltaV DCS using Modbus TCP.
|
1.10 21/06/2023
|
Application NoteFile and language versions
|
|
|
CTEU-EP ModbusTCP Slave/Server to Micrologix1400 Master/Client
CTEU-EP ModbusTCP to Micrologix1400; Example project included
Festo CTEU-EP (Slave/Server) ModbusTCP communication to Allen Bradley MicroLogix1400 PLC (Master/Client)
The CTEU-EP bus node is used as part of a CPX terminal and for communication as a participant in networks with the protocol ModbusTCP.
This document has information combined from multiple resources for the in-tention of reducing the effort of a user who is configuring this application type.
|
1.10 08/01/2021
|
Application NoteFile and language versions
|
|
|
Driver Block Library for PCS7
Driver Block Library for PCS7
Commissioning devices using the PCS7 driver library- for CTEU and CPX Bus Nodes.
|
1.10 19/01/2026
|
Application NoteFile and language versions
|
|
|
EMC - Checklist
General
A checklist to avoid EMC trouble
|
1.10 03/03/2023
|
Application NoteFile and language versions
|
|
|
EtherNet/IP IO-Link Integration
CTEU-EP, CPX-FB36, CPX-CTEL-LK
Controlling IO-Link Devices with Festo EtherNet/IP Products
|
1.30 28/07/2016
|
Application NoteFile and language versions
|
|
|
Information on substances in our products
Substances in our products; Compliance
Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.
|
V3.5 17/10/2026
|
Application NoteFile and language versions
|
|
|
PCS7 V10 Compatibility
PCS7 V10 Compatibility
This application note guides the user to migrate and resolve errors in PCS7 V10.1 SP1 where CTEU_PCS7 and CPX_PCS7 libraries are installed.
|
1.10 19/01/2026
|
Application NoteFile and language versions
|