|
|
FSA-202208 - Security Advisory - Unsafe default Codesys configuration
Multiple Festo products contain an unsafe default Codesys configuration
The products are shipped with an unsafe configuration of the integrated CODESYS Runtime environment. In this case no default password is set to the CODESYS PLC and therefore access without authentication is possible.
With a successful established connection to the CODESYS Runtime the PLC-Browser commands are available. Thus granting the possibilities to e.g. read and modify the configuration file(s), start/stop the application and reboot the device.
|
1.0.1
|
Security AdvisoryFile and language versions
|
|
|
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols
Incomplete documentation of remote accessible functions and protocols in Festo products
Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.
Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.
|
1.2.1
|
Security AdvisoryFile and language versions
|
|
|
FSA-202401 - Security Advisory - Several Codesys Vulnerabilities in Festo Products
Several high severity vulnerabilities in CODESYS V3 affecting Festo products could lead to Remote Code Execution or Denial of Service.
|
1.0.0
|
Security AdvisoryFile and language versions
|
|
|
FSA-202602: Multiple OpenSSL vulnerabilities affect Festo AX OS in CEPE
Festo AX OS versions 25.0.1.46 and 25.9.2.4, which are based on PLCnext by Phoenix Contact, used by the Festo product CEPE are affected by multiple OpenSSL vulnerabilities. The vulnerabilities are identified as CVE-2025-15467 and CVE-2025-69419. Attacks may be possible when maliciously crafted firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects are uploaded and processed by the affected system. In the device context, exploitation typically requires a logged-in user with high privileges or the processing of attacker-supplied cryptographic objects.
A successful attack using manipulated firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects may lead to memory corruption, application crash, or denial of service. Depending on the affected code path, execution context, platform protections, and toolchain mitigations, execution of malicious code may be possible. This can jeopardize confidentiality, integrity, and availability of the affected system.
|
1.0.0
|
Security AdvisoryFile and language versions
|
|
|
CDPX serial communication and configuration using Fuction Blocks and CodeSys V3.5
CDPX-X-A-W-7; Example project included
This document explains how you will Send and Receive data in CDPX Panel by using Serial communication RS-232 using CODESYS V3.5 SP12.
|
1.10 02/03/2020
|
Application NoteFile and language versions
|
|
|
CDPX-X-B-W-xx Manual
CDPX-X-B-W-xx Manual
This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.
|
1.30 13/03/2023
|
Application NoteFile and language versions
|
|
|
CDPX-X-E1-W-xx Manual
CDPX-X-E1-W-xx Manual
This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.
|
1.30 13/03/2023
|
Application NoteFile and language versions
|
|
|
CDPX-X-E2-W-5-EX2 Manual
CDPX-X-E2-W-5-EX2 Manual
This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.
|
1.30 11/02/2025
|
Application NoteFile and language versions
|
|
|
CDPX-X-E2-W-xx-EX2 Manual
CDPX-X-E2-W-xx-EX2 Manual
This Application Note describes the main features of the Festo operator panels. This operational guidelines described below, is information which relates to the device, installation, transportation, storage, assembly, use and maintenance.
|
1.30 11/02/2025
|
Application NoteFile and language versions
|
|
|
Checkbox CHB-C-N Telnet communication
CHB-C-N; CheckKon; Designer Studio
This Application Note give an example for the Checkprogram
selection by telnet communication. Further on it shows how to influence different system parameter setting by telnet access.
|
1.10 01/03/2018
|
Application NoteFile and language versions
|
|
|
CMMT-AS-MP Servo Drive Control with Festo CDPX-X-E1-W-xx Operator Panel through Profinet
CMMT-AS-MP; Festo CDPX-X-E1-W-xx; Profinet; Sample Code included
This application note explains how to control the CMMT-AS servo drive via Profinet network in Festo CDPX-E operator panels. The user will be able to control the Festo drives in point to-point mode using the sample code provided. The manual refers to the following models CDPX-X-E1-W-7, CDPX-X-E1-W-10 and CDPX-X-E1-W-15.
|
1.10 11/01/2024
|
Application NoteFile and language versions
|
|
|
Designer Studio
CDPX; Designer Studio 2.0
|
1.10 28/02/2017
|
Application NoteFile and language versions
|
|
|
Designer Studio 21 CFR Part 11 Compliance
Designer Studio 21 CFR Part 11 Compliance
Designer Studio includes a set of functions for responding to the requirements specified in FDA 21 CFR Part 11. The standard is in-tended to provide a solution for securely handling electronic records and electronic signatures in industrial applications.
|
1.10 09/02/2026
|
Application NoteFile and language versions
|
|
|
EMC - Checklist
General
A checklist to avoid EMC trouble
|
1.10 03/03/2023
|
Application NoteFile and language versions
|
|
|
How to implement data exchange between CDPX and MSSQL databases
How to implement data exchange between CDPX and MSSQL databases
This application note helps the user to implement data exchange between CDPX and MSSQL databases.
|
1.10 06/03/2026
|
Application NoteFile and language versions
|
|
|
Information on substances in our products
Substances in our products; Compliance
Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.
|
V3.5 17/10/2026
|
Application NoteFile and language versions
|
|
|
OPC UA communication between Siemens PLC and Festo CDPX Panels
OPC UA communication, Siemens TIA PLC, CDPX; Sample project included
This application note helps the user to establish OPC UA communication between Siemens TIA PLC and Festo CDPX panels.
|
1.30 03/01/2025
|
Application NoteFile and language versions
|
|
|
Security white paper for Festo controllers
This document is intended to provide users of Festo control products with an introduction and support on how Festo controllers can be used as securely as possible from the point of view of cyber security.
|
V03 25/05/2023
|
Application NoteFile and language versions
|