Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA - 202305 - Security Advisory - Vulnerable Wibu CodeMeter Runtime in Several Festo Products

A vulnerability in the Wibu CodeMeter Runtime, which is part of the installation packages of several Festo products, was found.

 

An attacker exploiting the vulnerability in WIBU CodeMeter Runtime in server mode could gain full access to the affected server via network access without any user interaction. This could lead to remote code execution and escalation of privileges giving full admin access on the host system for an already authenticated user (logged in locally to the PC).

1.1.0
FSA-202301 - Security Advisory - Video.js Cross-Site-Scripting (XSS) vulnerability in LX Appliance

A vulnerability in the Video.js package could allow a user of LX Appliance, with a high privilege account (i.e., with the "Teacher" role), to craft a malicious course and launch an XSS attack.

1.0.0
FSA-202603: Two critical PHP vulnerabilities in several Festo Didactic products

Festo Didactic FactoryViews and MES4 deployed along with xampp bundle an Apache web server with PHP. The bundled version of PHP is vulnerable to the two critical vulnerabilities CVE-2026-109618 and CVE-2026-109619 (commonly referred to as PHP2Shell). These vulnerabilities allow an attacker to remotely execute code on the FactoryViews or xampp host
system.


A successful attack on a vulnerable PHP installation allows the attacker to remotely execute malicious code on the FactoryViews or xampp host system with the privileges of the user account running the server application.

2.0.0
REACh EC Regulation 1907/2006/EC (REACh) - Festo Didactic SE Registration, Evaluation, Authorization and Restriction of Chemicals

REACh
SCIP
Certificate