Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Robotino View 4 Installer

Robotino View is the interactive graphical programming environment for Robotino.

With Robotino View, control programs for Robotino can be created and executed.

4.4.6
25/11/2022
Robotino4 Image

you need to download all 3 files  - follow the .txt instruction 

Introduction on how to create a USB Stick to restore Robotino OS / image (operating system)


Robotino has a SSD that stores the operating system.
A bootable USB stick is used to initially install the Robotino OS to a new SSD or
overwrite the OS on a SSD already in use.


*****Create a bootable USB-Stick*****

If you are using the USB-stick that shipped with Robotino you can skip to step number 4.
If you use a new USB follow Step1-3:
1) Download the Robotino custom image. (e.g. CoreCustom_20211029.iso)
2) Take a USB-Stick and format it (quick format will do)
3) Use UNetbootin (https://unetbootin.github.io/) to install this custom image to the USB stick.

-----
4) Download a Robotino4 image and it's md5 file. (With Firefox you need to right-click the file and choose save link.)
5) Check the integrity of the image using md5 (http://www.withopf.com/tools/md5/)
Run md5 -Check:imagefilename.fsa.md5.

-----
6) Copy the image files (.fsa,.f01,...) into the /images/ directory of your USB-stick.
e.g. robotino4-4.20.10.fsa and robotino4-4.20.10.f01
Note: if images folder is missing, copy to boot folder.

7) Attach monitor and keyboard to your Robotino.
8) Plug the USB stick into any of Robotino's USB port.
9) Please do not continue without plugging in Robotino to it's power supply.
10) Power on Robotino and hit the
F7 (for Robotino Professional with Core i5),
F11 (for Robotino Basic with Atom) as long as you can see the BIOS startup screen.

11) Select your USB stick from the list (not the UEFI entry).
12) Select Microcore from the list - this will start the automatic updater.
13) After booting into tinycore type restore.sh and press Enter to start the restore process.

furter reference https://www.openrobotino.org/

4.20.10.f01
27/02/2024
SCADA for LVDAC-EMS Version 1.31.00
SMART Home Rasyberry Pi 4 Image

Systemvoraussetzungen:

  • Raspberry Pi 4 4GB RAM
  • SD-Card 32GB
1.0
29/04/2024
Software for 2kW Four-Quadrant Dynamometer Version 2.00.00
TIA V15 SkillsConveyor Siemens TIA V15 Example Program SkillsConveyor standalone

Siemens TIA V15 Example Program SkillsConveyor without modules (standalone) for show cases and faires, shows a continues run with SkillsConveyor.

07/01/2026
TIA V15 SkillsConveyor with Distributing and Sorting Siemens TIA V15 Example Program

Example program for SkillsConveyor with SkillsPackage Distributing and Sorting Package

07/01/2026
TIA V17 SkillsConveyor with Distributing and Sorting Siemens TIA V17 Example Program

Example program for SkillsConveyor with SkillsPackage Distributing and Sorting Package

TIA V19 SkillsConveyor Siemens TIA V19 Example Program SkillsConveyor standalone

Siemens TIA V19 Example Program SkillsConveyor withouth modules (standalone) for show cases and fairs, shows a continues run with SkillsConveyor.

 

07/01/2026
TP1135 Smart Home Image Raspberry PI 4 Image
1.0
01/07/2024
USB Treiber Festo Didactic

USB driver setup EasyPort, DriveLab, PSU Remote, MecLab

2.15