Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node VTEM; CPX-FB38

Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node

1.10
24/09/2018
Festo CPX and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects CPX-FB36 and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects

How to extract data from CPX-FB36 systems using the built-in auto-discovery feature of Factory Talk Edge Gateway by Rockwell Automation.  What are the use cases of this data, and how to supplement it by using Factory Talk Smart Objects.

1.10
06/12/2022
Festo VTEM Motion Terminal Commissioning with Keyence KV-8000 PLC through EtherNet/IP Festo VTEM Motion Terminal Commissioning with Keyence KV-8000 PLC through EtherNet/IP; Library is included

This Application Note provides a detailed procedure for integrating the VTEM Motion Terminal from Festo with Keyence KV-8000 PLCs via the EtherNet/IP communication network. It also describes the library used for controlling (Device Control) the VTEM Motion Terminal

1.20
28/11/2025
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
Malfunction codes VTEM Festo Motion Terminal (VTEM)

The following tables contain all the malfunction codes and sub-codes relevant to the application that can be stored in the diagnostic memory of the Festo Motion Terminal (VTEM).

2.10
12/09/2023
Motion Terminal Quick Reference PLC programming VTEM

VTEM Motion Terminal Quick Reference PLC programming

1.80
02/05/2023
Safety Sub-Functions in Connection with Motion Terminal VTEM Motion Terminal VTEM

Safety Sub-Functions in Connection with Motion Terminal VTEM

1.33
23/11/2018
Supported drives VTEM Festo Motion Terminal (VTEM)

This list contains all Festo drives approved for the Festo Motion Terminal (VTEM) and the corresponding value that must be entered in the

"drive type" system parameter (ID 20) in order to be able to operate the respective drive with a Motion App. FW 4.24

2.10
12/09/2023
VTEM BSSO Compensation VTEM BSSO Compensation for low volume flow rate

This Application Note describes the procedure of BSSO compensation, a feature that can be used to enhance the control performance in applications with low volume flow rates.

1.10
24/03/2025
VTEM Commissioning with Omron PLC by EtherCAT Using CPX-FB37 VTEM with Omron PLC; EtherCAT using CPX-FB37

This Application Note gives detailed procedure to integrate VTEM Motion Terminal with Omron PLC through EtherCAT communication Network using CPX-FB37. It also includes information on the function blocks to operate Festo VTEM Motion Terminal.

1.10
16/10/2023
VTEM Firmware Download Instructions for V4.12.0 VTEM

This document provides a step-by-step explanation of how to download the newest VTEM Firmware using Festo Field Device Tool. This Application Note describes a one-time migration which is required for all firmware versions older than 4.12.0. If firmware is already 4.12.0 or higher the migration step with bootloader-5.1.0 and misc-1.0.0 is not necessary.

1.40
23/07/2019
VTEM Motion Terminal commissioning with Mitsubishi FX5U-Series PLC by Modbus Simple CPU VTEM with Mitsubishi FX5U-Series PLC by Modbus; Library included

This Application Note Gives Detailed Procedure to Integrate VTEM Motion Terminal with Mitsubishi FX5U-series PLC through Modbus Simple CPU Communication Network. Also Describe Library and Function block to control the VTEM Motion Terminal from Festo.

V1.10
25/05/2023
VTEM Motion Terminal commissioning with Mitsubishi Q-Series PLC through CC-Link network VTEM Motion Terminal with Mitsubishi; CC-Link network; Library included

This Application Note gives detailed procedure to integrate VTEM Motion Terminal with Mitsubishi Q-series PLC through CC-Link  Communication Network. Also describe Library and Function block  to control the VTEM Motion Terminal from Festo.

1.10
05/12/2022
VTEM Motion Terminal commissioning with Mitsubishi R-Series PLC by Modbus Simple CPU communication VTEM with Mitsubishi R-Series PLC by Modbus; Library included

This Application Note gives detailed procedure to integrate VTEM Motion Terminal with Mitsubishi R-series PLC through Modbus Simple CPU communication Network. Also describe Library and Function block to control the VTEM Motion Terminal from Festo.

V1.10
25/05/2023
VTEM MOTION TERMINAL commissioning with SIEMENS S7-300 PLC through PROFINET network VTEM MOTION TERMINAL; SIEMENS S7-300 PLC; PROFINET; Library included

This Application Note gives detailed procedure to integrate VTEM Motion Terminal with SIEMENS S7-300 Controller in Profinet communication network. Also Describe Library for the control (Device Control) of the Motion Terminal VTEM from Festo.

 

Supported Systems :                                                                              

−         Tested with S7-300

1.10
05/12/2022
VTEM MotionApp #33 Positioning VTEM; GAMM; MA33

Commissioning & Troubleshooting Guide

1.20
07/06/2021
VTEM with Beckhoff PLC through EtherCAT VTEM with Beckhoff PLC through EtherCAT; Library is included

This Application Note gives detailed procedure to integrate VTEM

Motion Terminal with Beckhoff PLC through EtherCAT

Communication Network. Also describe Library and Function

block to control the VTEM Motion Terminal from Festo.

1.10
06/01/2026
VTEM with Keyence KV-X PLC through EtherCAT VTEM with Keyence KV-X PLC through EtherCAT; Library is included

This Application Note explains how to integrate the VTEM Motion Terminal and the function block library for the Festo VTEM Motion Terminal through EtherCAT with Keyence KV-X PLC in KV STUDIO programming environment.

1.10
02/10/2026
VTEM with LS PLC through EtherNetIP VTEM with LS PLC through EtherNetIP; Library is included

This Application Note gives detailed procedure to integrate VTEM Motion Terminal with LS Electric PLC through EtherNet/IP communication network. Also, describes library and function blocks  to control the VTEM Motion Terminal from Festo.

1.10
05/08/2025
VTEM with LS PLC through Modbus TCP VTEM with LS PLC through Modbus TCP; Library is included

This Application Note gives detailed procedure to integrate VTEM Motion Terminal with LS Electric PLC through Modbus TCP communication network. Also, describes library and function blocks  to control the VTEM Motion Terminal from Festo.

1.10
05/08/2025
VTEM with Mitsubishi I-QR PLC through EtherNet/IP VTEM with Mitsubishi I-QR PLC through EtherNet/IP; Library is included

This Application Note explains how to integrate the VTEM Motion Terminal and the function block library for the Festo VTEM Motion Terminal through EtherNet/IP with Mitsubishi i-QR PLC in GX Works3 programming environment.

1.10
05/09/2025
VTEM with Omron PLC through Ether-Net/IP VTEM with Omron PLC through Ether-Net/IP; Library is included

This Application Note explains how to integrate the VTEM Motion Terminal and the function block library for the Festo VTEM Motion Terminal through EtherNet/IP with Omron PLC in Sysmac Studio programming environment.

1.10
05/09/2025
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.