Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Mitsubishi PLC with Festo PLC Through Modbus TCP Mitsubishi PLC with Festo PLC Through Modbus TCP; Library included

This application note describes the procedure for configuring Modbus TCP communication between a Mitsubishi PLC and a Festo Controller.

1.10
02/01/2025
Modbus TCP/IP Communication between Siemens and Codesys Controller CPX-E-CEC

This application note helps the user to establish Modbus com-munication between Siemens PLC and Codesys PLC.

It explains the configurations needed in both the controllers in order to achieve Modbus communication between them.

It also explains the Function Blocks needed in Siemens PLC side to establish Modbus communication.

1.10
18/09/2019
ProfiNet Communication between CPX-E-CEC-C1-PN with S7-1200/1500 PLC CPX-E-CEC-P1-PN; Siemens S7-1200/1500 PLC

Brief explanation on how to communicate CPX-E-CEC-P1-PN with Siemens S7-1200 PLC.

1.10
27/03/2019
Security white paper for Festo controllers

This document is intended to provide users of Festo control products with an introduction and support on how Festo controllers can be used as securely as possible from the point of view of cyber security.

V03
25/05/2023
SFAB-.-PNLK with Festo PLC through EtherCAT using CPX-AP IO-Link SFAB-.-PNLK with Festo PLC through EtherCAT using CPX-AP IO-Link; Library is included

This Application Note explains how to integrate the SFAB IO Link Flow Sensor and the function block library for the Festo SFAB Flow Sensor through EtherCAT using the Festo CPX-AP IO Link with a Festo PLC in the CODESYS programming environment.

1.10
20/10/2026
This application note helps the user to understand the File Handling CPX-E-CEC

This application note helps the user to understand the File Han-dling operations of Codesys PLC’s.

The application note explains the File handling functions of Codesys controller.

The application note also explains data logging operation by writing the PLC data to a csv file in the USB memory.

1.10
22/07/2019
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.