Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202208 - Security Advisory - Unsafe default Codesys configuration Multiple Festo products contain an unsafe default Codesys configuration

The products are shipped with an unsafe configuration of the integrated CODESYS Runtime environment. In this case no default password is set to the CODESYS PLC and therefore access without authentication is possible.

 

With a successful established connection to the CODESYS Runtime the PLC-Browser commands are available. Thus granting the possibilities to e.g. read and modify the configuration file(s), start/stop the application and reboot the device.

1.0.1
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
FSA-202401 - Security Advisory - Several Codesys Vulnerabilities in Festo Products

Several high severity vulnerabilities in CODESYS V3 affecting Festo products could lead to Remote Code Execution or Denial of Service.

1.0.0
FSA-202602: Multiple OpenSSL vulnerabilities affect Festo AX OS in CEPE

Festo AX OS versions 25.0.1.46 and 25.9.2.4, which are based on PLCnext by Phoenix Contact, used by the Festo product CEPE are affected by multiple OpenSSL vulnerabilities. The vulnerabilities are identified as CVE-2025-15467 and CVE-2025-69419. Attacks may be possible when maliciously crafted firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects are uploaded and processed by the affected system. In the device context, exploitation typically requires a logged-in user with high privileges or the processing of attacker-supplied cryptographic objects.

 

A successful attack using manipulated firmware, key files, PKCS#12 files, CMS/PKCS#7 content, or digitally signed objects may lead to memory corruption, application crash, or denial of service. Depending on the affected code path, execution context, platform protections, and toolchain mitigations, execution of malicious code may be possible. This can jeopardize confidentiality, integrity, and availability of the affected system.

1.0.0
Alarm Handling at Festo Controllers Alarm Handling at Festo Controllers; CPX-E-CEC-x; CPX-CEC-*-V3

This Application Note describes the limitations of alarm configuration
on Festo PLC with Codesys runtime 3.5.15.x

1.10
03/03/2022
Codesys MQTT IIOT Library with Festo PLC Codesys MQTT IIOT Library from Codesys; Library not included

This document outlines the usage of the MQTT Client, MQTT Publish and MQTT subscribe function blocks from the MQTT CLIENT_SL library.

1.10
09/09/2024
CODESYS OPC DA server CODESYS Development System >= V3.5 SP12

This application note describes the license dependency with the CODESYS OPC DA server and possible alternatives for CODESYS Development System >= V3.5 SP12

1.20
22/07/2020
Commissioning of CMMT-AS in Festo Automation Suite with CPX-E-CEC-M1-PN CMMT-AS-...-EC; CPX-E-CEC-M1-PN; Example project included

This application note describes step by step how you configure a CMMT-AS-EC with CPX-E-CEC-M1-PN in Automation Suite and how you can use the SoftMotion libraries.

1.10
17/09/2019
Commissioning of IO-Link Devices over EtherCAT in Codesys V3 CPX-E-4IOL; CPX-E-EC; Codesys V3

The application note contains a step by step explanation how to

commission of IO-Link Devices connected to CPX-E-4IOL trough EtherCAT Fieldbus module CPX-E-EC in Codesys V3

1.10
05/06/2018
CPX-E-EP Integration with Omron Sysmac PLC through EtherNet/IP communication CPX-E-EP, Omron Sysmac, ETH/IP; NJ301; Example project included

A brief explanation of the this document describes about Integration
of Festo CPX-E-EP Expansion Modules
( IO-Link Master's, Digital Input's, Digital Output's, Analog Inputs'
& Analog Output's ) with Omron Sysmac PLC via Ethernet-
IP Protocol.
It also describes about the Integration of Festo CPX-E-EP
Modules with Omron NJ301 Series PLC.

1.10
13/04/2021
CPX-E-EP IO's Access in Allen-Bradley PLC CPX-E-EP Expansion Modules, Allen-Bradley

This Document Describes about Access of CPX-E-EP Expansion Modules ( Digital Input's, Digital Output's, Analog Inputs' & Ana-log Output's) with AB PLC via EtherNet-IP Protocole. It also de-scribes about the Hardware Configuration of CPX-E-EP Module & Expa

1.10
22/07/2019
CPX-IO Setup Computer Environment for Integration with Python CPX-IO Setup Computer Environment for Integration with Python

A step by step guide to set up computer environment for Python and Festo cpx-io python library to communicate with and control a CPX-E or CPX-AP system by Modbus TCP. CPX-IO stands for “CPX Input/Output”

1.10
03/07/2024
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
EtherNet/IP Device description file (eds file) CPX-E-CEC-C1/M1-EP Controller Version 1.1

EtherNet/IP Device description file (eds file)

CPX-E-CEC-C1/M1-EP Controller Version 1.1

EtherNet/IP Device description file (eds file)

for Festo CPX-E-CEC-C1/M1-EP Controller
Supported systems:
Controller CPX-E-CEC-C1-EP
Controller CPX-E-CEC-M1-EP

V1.1
25/09/2020
FESTO Controller Modbus TCP/IP Communication With Allen-Bradley PLC Festo PLC; Rockwell

This Application note gives detailed explanation about Festo PLC Modbus TCP/IP communication with Allen-Bradley PLC as Master & Slave

1.10
22/07/2019
Festo Positioning CNC Robotics Library (FPosCR Lib) V3.5.18.50 (EVO2.1) Festo Positioning CNC Robotics Library (FPosCR Lib) V3.5.18.50 (EVO2.1); Library is included

Festo Positioning CNC Robotics Library provides CNC and robotic motion functionalities for Festo gantry systems.

1.20
06/03/2026
Festo Synchronized Drive Control Festo Synchronized Drive Control

The FestoSynchronizedDriveControl_library offers function
blocks and methods to synchronize motion of 2 ore more axis.

Library in download-file included.

 

1.10
12/01/2022
FPosCR Integration with Beckhoff PLC through Modbus TCP FPosCR Integration with Beckhoff PLC through Modbus TCP; Library is included

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate with Beck-hoff TwinCAT 3 PLC in TwinCAT 3 programming environment using Modbus TCP communication.

1.10
05/08/2025
FPosCR Integration with Mitsubishi PLC through PROFINET FPosCR Integration with Mitsubishi PLC through PROFINET; Library is included

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in Mitsubishi iQ-R PLC in GX Works3 programming environment using PROFINET communication

1.10
23/02/2026
FPosCR Integration with Omron PLC through EtherNet/IP FPosCR Integration with Omron PLC through EtherNet/IP; Library is included

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in Omron Sysmac Studio programming environment using EtherNet/IP communication.

1.10
05/08/2025
FPosCR Integration with Rockwell PLC through EtherNet/IP FPosCR Integration with Rockwell PLC through EtherNet/IP; Library is included

This Application Note describes how to use the host AOI of the FPosCR from Festo & how to integrate in Rockwell Studio 5000 programming environment using EtherNet/IP communication.

1.10
05/08/2025
FPosCR Integration with Siemens PLC through Profinet FPosCR Integration with Siemens PLC through Profinet; Library is included

This Application Note describes how to use the host function blocks of the FPosCR from Festo & how to integrate them in Siemens TIA Portal programming environment using Profinet communication.

1.10
05/08/2025
FPosCR server integration with Festo PLC FPosCR server integration with Festo PLC; Library is included

This Application Note describes how to use the host sever Function Block of the FPosCR from Festo & how to integrate in CODESYS programming environment using Modbus/TCP, EtherNet/IP and PROFINET communication.

1.20
05/03/2026
How to mount SMB (CIFS) share CECC-…; CPX-CEC-...-V3 , CPX-E-CEC

This application note describes how to establish a SMB (CIFS) share with Festo PLCs CECC-.. and CPX-CEC-..-V3, CPX-E-CEC

1.20
03/08/2020
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
Integration of Flow Monitoring Function Block with Festo PLC Integration of Flow Monitoring Function Block with Festo PLC; Library is included

This Application Note explains how to integrate different Flow monitoring function blocks with Festo PLC and it shows how to configure the function blocks and monitoring and getting the flow data from the function blocks

 

1.10
30/09/2025
Integration of FPosCR Client with Festo PLC through Modbus TCP Integration of FPosCR Client with Festo PLC through Modbus TCP

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in CODESYS programming environment using Modbus/TCP communication.

1.20
15/04/2026
Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through Ether-Net/IP Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through Ether-Net/IP

This Application note explains the procedure for integrating the Keyence KV 8000 PLC with the Festo CPX-E-CEC PLC using the KV Studio environment and CODESYS software through EtherNet/IP.

1.10
05/08/2025
Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through OPC-UA Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through OPC-UA

This Application note explains the procedure for integrating the Keyence KV 8000 PLC with the Festo CPX-E-CEC PLC using the KV Studio environment and CODESYS software through OPC-UA.

1.10
07/08/2025
Integration of Omron NX102 PLC with Festo CPX-E-CEC through OPC UA Omron NX102 PLC with Festo CPX-E-CEC through OPC UA; Library included

The application note explains the procedure for integrating the Omron NX102 PLC with the Festo CPX-E-CEC PLC using the Sysmac Studio environment and Codesys software through OPC UA.

1.10
09/06/2025
Show 7 more results ...
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.