Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Cleanability of media-separated solenoid valves Cleanability of media-separated solenoid valves

Cleanability of media-separated solenoid valves in application with bacteria, proteins and other biological compounds.

Cleaning of bacteria, endotoxins and TOC shown using the example of contamination with E.coli bacteria suspension and a commercially available PCR-Kit

1.10
10/10/2024
Declaration of Contamination VTOE, VTOI, VYKA, EHMD, NLFA

In order to protect our employees as well as our equipment, we need information from you on the application for which the returned goods were used. The enclosed declaration is compulsory and binding and may only be completed and signed by authorised personnel.

Returned goods must be accompanied by a completed and signed declaration in order for Festo to perform an inspection and fault analysis. We reserve the right to reject shipments that do not meet this requirement.

1.20
27/07/2021
Dispensing on the fly Dispensing on the fly; Dispensing liquids while the dispense head is in motion

This application note covers the following topics:
• The challenges of dispensing on the fly.
• Parameters to consider for dispensing on the fly.
• How to define the system and calculate the right parameter values to obtain       accurate dispensing results.

1.10
04/12/2024
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
Flushability of media separated valves Flushability of media separated valves

Flushability of media separated valves describes the performance of flushing liquid out of a valve with another liquid with as less volume as possible. A good valve design with little dead volume and therefore a good flushability is important when using media separated valves in laboratory applications e.g. for cleaning processes or with expensive liquids. A flushability test with two different liquids refers as an indicator of good valve design.

This application note covers the following topics:

  • Description of a test setup to make the small internal volume and the flow-optimized design visible.
  • Comparison of the flushability performance of different media separated valves.
1.10
16/12/2024
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
Interpretation and analysis of Liquid Handling results Interpretation and analysis of Liquid Handling results; Definitions

This Application Note describe the most common terms about the evaluation of results of a dispensing or pipetting application. In particular: accuracy, trueness, precision, repeatability, reproducibility, coefficient of Variances (CV), mean and standard deviation as well as maximum permissible error.

1.20
25/08/2023
Reduction of the heat input of media-separated valves into the flowing fluid

The application note describes the influence of heat input in media-separated valves on the flowing fluid. It compares the heat input from different manufacturers, flow rates and provides suggestions for reduction.

1.10
25/07/2024
VYKA extended application information VYKA extended application information

Description of application test results and technical features of the VYKA valve that are not included in the regular datasheet values.

1.30
21/09/2023
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.