Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Latest

Festo Motion Package - User Guide 21/10/2026 Festo Motion Package - User Guide

A guide to commission and program single axis using Festo Motion Package in Festo edge controller CEPE. Drive used is a CMMT-AS-C2-3A-MP-S1.

Other quick start guide shows the steps to get an example system working with Festo Robotic as part of Festo Motion Package. In the end user will be able to start programming his own application.

1.40
14/10/2026
Firmware (VBH) 19/10/2026 Firmware for serial vacuum subbase (VBH)

Supported systems:

  • Manifold sub-base for vacuum VABX-A-S-VE-BH-VB010H (8213836)
  • Valve terminal VTUX-A-S- (8000805)
  • Valve terminal VTUX-A-S-APA- (8000815)
  • Subbase VABX (8000870)
1.7.3
31/07/2026
Firmware VP (Vacuum switching unit) 19/10/2026 Firmware serial VABX-A-S-VP-VH

Supported systems:

  • Valve terminal VTUX-A-S- (8000805)
  • Valve terminal VTUX-A-S-APA- (8000815)
  • Subbase VABX...(8000870)
1.7.3
31/07/2026

Top downloads

Terms of use for electronic documentation
FCT - Festo Configuration Tool - PlugIn
Setup for Festo Configuration Tool with CMAX plugIn
  • Festo Configuration Tool V1.3.1.1
  • CMAX PlugIn V2.3]
  • CMAX PlugIn V2.2
  • CMAX PlugIn V1.8
  • CMAX PlugIn V1.1
  • CMAX PlugIn V1.0


Version changes:
Version 2.3 Support of new firmware features
  • Record list with 128 records[*/]
  • Seperated target position and target force in the control data[*/]
  • Sign of Life bit[*/]
  • Control clamping unit of DGCI externally[*/]
  • Secondary actual value transmits error and warning[*/]
Other
  • The PlugIn can be used in Japanese language[*/]
  • A firmware version can be defined which is to be used for the component[*/]


Supported systems:
  • Axis controller CPX-CMAX-C1-1 (548932)
  • Terminal CPX (197330)
2.3.1.333
13/09/2017
Festo AX Motion Insights Pneumatic General Information for set-up and monitoring MIP

This document describes how to set up AX Motion Insights Pneumatic from connectivity to asset onboarding and monitoring of pneumatic actuators.

1.80
29/05/2026