Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Convert project FCT Convert project

(Servicevideo)

Update firmware (Ethernet) FCT: Update firmware (Ethernet)

(Servicevideo)

Update firmware (USB) FCT Update firmware (USB)

(Servicevideo)

Update plug-in FCT Update plug-in

(Servicevideo)

FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
Commissioning of CMMO-...-LKP in IOLink mode with CompctLogix CMMO-ST-C5-1-LKP; CompactLogix 5370 Controller; Point IO module 1734-AENTR

Commissioning of CMMO-ST-C5-1-LKP in IO-Link mode with the Point IO module 1734-AENTR and 4IOL master

1.10
14/06/2016
Commissioning of CMMO-ST-...-LKP in IO-Link mode with Codesys V3 CMMO-ST-...-LKP

The application note contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP as IO-Link device in Codesys V3.

1.20
25/04/2016
Commissioning of CMMO-ST-...-LKP Modbus/TCP with Codesys V3 CMMO-ST-...-LKP

The application node contains a step by step explanation how to configure a CMMO-ST-...-LKP as Modbus/TCP server in

Codesys V3.

1.20
19/04/2016
Commissioning of CMMO-ST-C5-1-LKP CTEU-EP and CAPC via Logix Designer CMMO-ST-C5-1-LKP; CTEU-EP; CAPC-F1-E-M12

The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP in I-Port mode with CTEU-EP and CAPC-F1-E-M12 via Logix Designer.

1.10
13/06/2016
Commissioning of CMMO-ST-C5-1-LKP in I-Port mode with CTEU-PN and CAPC-F1-E-M12 via TIA Portal V13 CMMO-ST-...-LKP; CTEU-PN; CAPC-F1-E-M12

 

 

The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP in I-Port mode with CTEU-PN and CAPC-F1-E-M12 via TIA Portal V13

1.10
25/04/2016
Commissioning of CMMO-ST-C5-1-LKP in Modbus/TCP mode with TIA Portal V13 CMMO-ST-...-LKP

 

The application node contains a step by step explanation how to configure a CMMO-ST-C5-1-LKP as Modbus/TCP server in TIA Portal V13.

1.10
25/04/2016
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
I-Port event/error list CMMO-ST-...LKP; CTEU-...

A list of CMMO events and errors are transmitted via I-Port

1.10
17/01/2018
MITSUBISHI Q PLC with FESTO motor controller via MODBUS/TCP with example proram CMMP-AS-...-M3; CMMP-AS-...-M0; CMMO-ST-...-LKP

This document shows how to use Mitsubishi PLC MODBUS/TCP communications to control the FESTO motor controller via FHPP (Festo Handling Positioning Profile).

1.10
08/01/2019
MITSUBISHI Q series PLC with CMMx via Modbus TCP + example program CMMP-AS-...-M0; CMMP-AS-...-M3; CMMO-ST-...-LKP

This document shows how to use Mitsubishi PLC MODBUS/TCP communications to control the FESTO motor controller via FHPP (Festo Handling Positioning Profile).

1.10
06/10/2017
ModbusTCP Client Sample CMMO-ST-...-LKP; Visual Studio C#

A ModbusTCP Client Sample program for Visual Studio

1.10
11/02/2016
Power Supply Stepper CMMS-ST, CMMO-ST, SVG

How to choose the correct current rating of the power supplies used for motor controllers

1.10
19/05/2016
Safety Sub-Function STO Servo Drive CMMT-ST-…-S0 With Stepper Motors: STO, Category 3, up to PL e. With EC Motors: STO, Category 3, up to PL d

Application Note for the realization of the safety sub-function safe torque off (STO) with category 3 and up to PL e for stepper motors or category 3 and up to PL d for EC motors. This Application Note contains possible circuits for the servo drive CMMT-ST-…-S0.

1.0
08/07/2019
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-ST-…-S0 With Stepper Motors: SS1-t, STO, Category 3, up to PL e. With EC Motors: STO, Category 3, up to PL d

Application Note for the realization of the safety sub-functions safe stop 1 (SS1) and safe torque off (STO) with category 3 and up to PL e. This Application Note contains possible circuits for the servo drive CMMT-AS-…-S1.

1.0
08/07/2019
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.