Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202201 - Security Advisory - Festo Controller CECC-X-M1 Product Family Pre-Authentication Command Injection Vulnerability

The Festo controller CECC-X-M1 product family in multiple versions are affected by a preauthentication command injection vulnerability. Any person who is able to gain access to the webserver would be able to run arbitrary system commands on the device with root privileges.

 

Affected Festo products:

  • Controller CECC-X-M1 (4407603) - Firmware CECC-X <= 3.8.14 affected
  • Controller CECC-X-M1 (8124922) - Firmware CECC-X 4.0.14
    affected
  • Controller CECC-X-M1-MV (4407605) - Firmware CECC-X <=
    3.8.14 affected
  • Controller CECC-X-M1-MV (8124923) - Firmware CECC-X 4.0.14
    affected
  • Controller CECC-X-M1-MVS1 (4407606) - Firmware CECC-X <=
    3.8.14 affected
  • Controller CECC-X-M1-MVS1 (8124924) - Firmware CECC-X 4.0.14
    affected
  • Controller CECC-X-M1-YYJKP (4803891) - Firmware CECC-X <=
    3.8.14 affected
  • Controller CECC-X-M1-YSL1 (8082793) - Firmware CECC-X <=
    3.8.14 affected
  • Controller CECC-X-M1-YSL2 (8082794) - Firmware CECC-X <=
    3.8.14 affected
  • Servo Press Kit YJKP (8077950) - Firmware CECC-X <=
    3.8.14 affected
  • Servo Press Kit YJKP (8058596) - Firmware CECC-X <=
    3.8.14 affected
1.1.1
FSA-202202 - Security Advisory - Festo Controller CECC-S,-LK,-D Family Firmware <= 2.3.8.1 Multiple Vulnerabilities in CODESYS V3 Runtime System

The Festo controller CECC product family is affected by multiple vulnerabilities in the CODESYS V3 runtime.

1.0.1
FSA-202203 - Security Advisory - Festo Controller CECC-S,-LK,-D Family Firmware = 2.4.2.0 Multiple Vulnerabilities in CODESYS V3 Runtime System

The Festo controller CECC product family is affected by multiple vulnerabilities in the CODESYS V3 runtime.

1.0.1
FSA-202208 - Security Advisory - Unsafe default Codesys configuration Multiple Festo products contain an unsafe default Codesys configuration

The products are shipped with an unsafe configuration of the integrated CODESYS Runtime environment. In this case no default password is set to the CODESYS PLC and therefore access without authentication is possible.

 

With a successful established connection to the CODESYS Runtime the PLC-Browser commands are available. Thus granting the possibilities to e.g. read and modify the configuration file(s), start/stop the application and reboot the device.

1.0.1
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
FSA-202401 - Security Advisory - Several Codesys Vulnerabilities in Festo Products

Several high severity vulnerabilities in CODESYS V3 affecting Festo products could lead to Remote Code Execution or Denial of Service.

1.0.0
Boot Application loading without CoDeSys V3.5 CECC; CPX-CEC (V3)

A brief explanation on how to load a new project to a Festo PLC over Ethernet without the use of the CoDeSys 3.5 software

1.10
05/07/2016
CECC-LK as IO-Link Master connected to Balluff RFID Device and data carriers CECC-LK; Balluff RFID

The application note contains a step by step explanation how to configure a Balluff RFID read/write system as IO-Link device connected to CECC-LK in Codesys V3

1.10
01/12/2016
CECC-LK as IO-Link Master Connected to SDAT CECC-LK; SDAT

The application note contains a step by step explanation how to configure a SDAT sensor as IO-Link device connected to CECC-LK in Codesys V3.

1.10
01/12/2016
CODESYS OPC DA server CODESYS Development System >= V3.5 SP12

This application note describes the license dependency with the CODESYS OPC DA server and possible alternatives for CODESYS Development System >= V3.5 SP12

1.20
22/07/2020
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
FESTO Controller Modbus TCP/IP Communication With Allen-Bradley PLC Festo PLC; Rockwell

This Application note gives detailed explanation about Festo PLC Modbus TCP/IP communication with Allen-Bradley PLC as Master & Slave

1.10
22/07/2019
FPosCR server integration with Festo PLC FPosCR server integration with Festo PLC; Library is included

This Application Note describes how to use the host sever Function Block of the FPosCR from Festo & how to integrate in CODESYS programming environment using Modbus/TCP, EtherNet/IP and PROFINET communication.

1.20
05/03/2026
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.4
12/10/2026
Integration of FPosCR Client with Festo PLC through Modbus TCP Integration of FPosCR Client with Festo PLC through Modbus TCP

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in CODESYS programming environment using Modbus/TCP communication.

1.20
15/04/2026
Modbus TCP/IP Communication between Siemens and Codesys Controller CPX-E-CEC

This application note helps the user to establish Modbus com-munication between Siemens PLC and Codesys PLC.

It explains the configurations needed in both the controllers in order to achieve Modbus communication between them.

It also explains the Function Blocks needed in Siemens PLC side to establish Modbus communication.

1.10
18/09/2019
Security white paper for Festo controllers

This document is intended to provide users of Festo control products with an introduction and support on how Festo controllers can be used as securely as possible from the point of view of cyber security.

V03
25/05/2023
Set Date and Time for Festo PLC CECC; FDT; Codesys, Putty

How to read and write Date & Time from the command prompt.

1.10
08/01/2019
YHBP - Servopneumatic Balancer Kit Design diagram PLd Example design diagram for a PLd Servopneumatic Balancerkit.

Example design diagram for a PLd Servopneumatic Balancerkit.

1.10
25/01/2022
YHBP - Servo-pneumatic Balancer Kit Software Update and backup YHBP - Servo-pneumatic Balancer Kit Software Update and backup

This Application Note explain the update process of the application
software of the CECC-D-BA Balancer controller.
And the backup and restore function of the configuration-files.
Reading of log-data.

1.10
25/01/2022
YHBP - Servopneumatic Balancer-Kit - Design diagram PLb YHBP - Servopneumatic Balancer-Kit - Design diagram PLb

Example design diagram for a PLb Servopneumatic Balancerkit.

1.10
25/01/2022
YHBP-Servopneumatic Balancerkit - Description of host function blocks and Modbus in CODESYS YHBP-Servopneumatic Balancerkit; Host function blocks; Modbus Library included

This application note describes how to use the host function
blocks of the servopneumatic balancerkit YHBP in CODESYS
(V3). The additional document explain the communication via Modbus TCP. 

Library in download-file included. 

1.10
25/01/2022
YJKP with Keyence KV-X PLC through EtherNet/IP YJKP with Keyence KV-X PLC through EtherNet/IP; Library is included

This Application Note describes how to use and integrate the Festo's host function blocks for the YJKP-Servo Press Kit into Keyence KV STUDIO projects with KV-X PLCs over an EtherNet/IP network.

1.10
01/09/2026
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.