|
|
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols
Incomplete documentation of remote accessible functions and protocols in Festo products
Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.
Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.
|
1.2.1
|
Security AdvisoryFile and language versions
|
|
|
Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node
VTEM; CPX-FB38
Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node
|
1.10 24/09/2018
|
Application NoteFile and language versions
|
|
|
Festo CPX and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects
CPX-FB36 and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects
How to extract data from CPX-FB36 systems using the built-in auto-discovery feature of Factory Talk Edge Gateway by Rockwell Automation. What are the use cases of this data, and how to supplement it by using Factory Talk Smart Objects.
|
1.10 06/12/2022
|
Application NoteFile and language versions
|
|
|
Festo VTEM Motion Terminal Commissioning with Keyence KV-8000 PLC through EtherNet/IP
Festo VTEM Motion Terminal Commissioning with Keyence KV-8000 PLC through EtherNet/IP; Library is included
This Application Note provides a detailed procedure for integrating the VTEM Motion Terminal from Festo with Keyence KV-8000 PLCs via the EtherNet/IP communication network. It also describes the library used for controlling (Device Control) the VTEM Motion Terminal
|
1.20 28/11/2025
|
Application NoteFile and language versions
|
|
|
Information on substances in our products
Substances in our products; Compliance
Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.
|
V3.4 12/10/2026
|
Application NoteFile and language versions
|
|
|
Malfunction codes VTEM
Festo Motion Terminal (VTEM)
The following tables contain all the malfunction codes and sub-codes relevant to the application that can be stored in the diagnostic memory of the Festo Motion Terminal (VTEM).
|
2.10 12/09/2023
|
Application NoteFile and language versions
|
|
|
Motion Terminal Quick Reference PLC programming
VTEM
VTEM Motion Terminal Quick Reference PLC programming
|
1.80 02/05/2023
|
Application NoteFile and language versions
|
|
|
Safety Sub-Functions in Connection with Motion Terminal VTEM
Motion Terminal VTEM
Safety Sub-Functions in Connection with Motion Terminal VTEM
|
1.33 23/11/2018
|
Application NoteFile and language versions
|
|
|
Supported drives VTEM
Festo Motion Terminal (VTEM)
This list contains all Festo drives approved for the Festo Motion Terminal (VTEM) and the corresponding value that must be entered in the
"drive type" system parameter (ID 20) in order to be able to operate the respective drive with a Motion App. FW 4.24
|
2.10 12/09/2023
|
Application NoteFile and language versions
|
|
|
VTEM BSSO Compensation
VTEM BSSO Compensation for low volume flow rate
This Application Note describes the procedure of BSSO compensation, a feature that can be used to enhance the control performance in applications with low volume flow rates.
|
1.10 24/03/2025
|
Application NoteFile and language versions
|
|
|
VTEM Commissioning with Omron PLC by EtherCAT Using CPX-FB37
VTEM with Omron PLC; EtherCAT using CPX-FB37
This Application Note gives detailed procedure to integrate VTEM Motion Terminal with Omron PLC through EtherCAT communication Network using CPX-FB37. It also includes information on the function blocks to operate Festo VTEM Motion Terminal.
|
1.10 16/10/2023
|
Application NoteFile and language versions
|
|
|
VTEM Firmware Download Instructions for V4.12.0
VTEM
This document provides a step-by-step explanation of how to download the newest VTEM Firmware using Festo Field Device Tool. This Application Note describes a one-time migration which is required for all firmware versions older than 4.12.0. If firmware is already 4.12.0 or higher the migration step with bootloader-5.1.0 and misc-1.0.0 is not necessary.
|
1.40 23/07/2019
|
Application NoteFile and language versions
|
|
|
VTEM Motion Terminal commissioning with Mitsubishi FX5U-Series PLC by Modbus Simple CPU
VTEM with Mitsubishi FX5U-Series PLC by Modbus; Library included
This Application Note Gives Detailed Procedure to Integrate VTEM Motion Terminal with Mitsubishi FX5U-series PLC through Modbus Simple CPU Communication Network. Also Describe Library and Function block to control the VTEM Motion Terminal from Festo.
|
V1.10 25/05/2023
|
Application NoteFile and language versions
|
|
|
VTEM Motion Terminal commissioning with Mitsubishi Q-Series PLC through CC-Link network
VTEM Motion Terminal with Mitsubishi; CC-Link network; Library included
This Application Note gives detailed procedure to integrate VTEM Motion Terminal with Mitsubishi Q-series PLC through CC-Link Communication Network. Also describe Library and Function block to control the VTEM Motion Terminal from Festo.
|
1.10 05/12/2022
|
Application NoteFile and language versions
|
|
|
VTEM Motion Terminal commissioning with Mitsubishi R-Series PLC by Modbus Simple CPU communication
VTEM with Mitsubishi R-Series PLC by Modbus; Library included
This Application Note gives detailed procedure to integrate VTEM Motion Terminal with Mitsubishi R-series PLC through Modbus Simple CPU communication Network. Also describe Library and Function block to control the VTEM Motion Terminal from Festo.
|
V1.10 25/05/2023
|
Application NoteFile and language versions
|
|
|
VTEM MOTION TERMINAL commissioning with SIEMENS S7-300 PLC through PROFINET network
VTEM MOTION TERMINAL; SIEMENS S7-300 PLC; PROFINET; Library included
This Application Note gives detailed procedure to integrate VTEM Motion Terminal with SIEMENS S7-300 Controller in Profinet communication network. Also Describe Library for the control (Device Control) of the Motion Terminal VTEM from Festo.
Supported Systems :
− Tested with S7-300
|
1.10 05/12/2022
|
Application NoteFile and language versions
|
|
|
VTEM MotionApp #33 Positioning
VTEM; GAMM; MA33
Commissioning & Troubleshooting Guide
|
1.20 07/06/2021
|
Application NoteFile and language versions
|
|
|
VTEM with Beckhoff PLC through EtherCAT
VTEM with Beckhoff PLC through EtherCAT; Library is included
This Application Note gives detailed procedure to integrate VTEM
Motion Terminal with Beckhoff PLC through EtherCAT
Communication Network. Also describe Library and Function
block to control the VTEM Motion Terminal from Festo.
|
1.10 06/01/2026
|
Application NoteFile and language versions
|
|
|
VTEM with Keyence KV-X PLC through EtherCAT
VTEM with Keyence KV-X PLC through EtherCAT; Library is included
This Application Note explains how to integrate the VTEM Motion Terminal and the function block library for the Festo VTEM Motion Terminal through EtherCAT with Keyence KV-X PLC in KV STUDIO programming environment.
|
1.10 02/10/2026
|
Application NoteFile and language versions
|
|
|
VTEM with LS PLC through EtherNetIP
VTEM with LS PLC through EtherNetIP; Library is included
This Application Note gives detailed procedure to integrate VTEM Motion Terminal with LS Electric PLC through EtherNet/IP communication network. Also, describes library and function blocks to control the VTEM Motion Terminal from Festo.
|
1.10 05/08/2025
|
Application NoteFile and language versions
|
|
|
VTEM with LS PLC through Modbus TCP
VTEM with LS PLC through Modbus TCP; Library is included
This Application Note gives detailed procedure to integrate VTEM Motion Terminal with LS Electric PLC through Modbus TCP communication network. Also, describes library and function blocks to control the VTEM Motion Terminal from Festo.
|
1.10 05/08/2025
|
Application NoteFile and language versions
|
|
|
VTEM with Mitsubishi I-QR PLC through EtherNet/IP
VTEM with Mitsubishi I-QR PLC through EtherNet/IP; Library is included
This Application Note explains how to integrate the VTEM Motion Terminal and the function block library for the Festo VTEM Motion Terminal through EtherNet/IP with Mitsubishi i-QR PLC in GX Works3 programming environment.
|
1.10 05/09/2025
|
Application NoteFile and language versions
|
|
|
VTEM with Omron PLC through Ether-Net/IP
VTEM with Omron PLC through Ether-Net/IP; Library is included
This Application Note explains how to integrate the VTEM Motion Terminal and the function block library for the Festo VTEM Motion Terminal through EtherNet/IP with Omron PLC in Sysmac Studio programming environment.
|
1.10 05/09/2025
|
Application NoteFile and language versions
|