Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
Alarm Handling at Festo Controllers Alarm Handling at Festo Controllers; CPX-E-CEC-x; CPX-CEC-*-V3

This Application Note describes the limitations of alarm configuration
on Festo PLC with Codesys runtime 3.5.15.x

1.10
03/03/2022
Codesys MQTT IIOT Library with Festo PLC Codesys MQTT IIOT Library from Codesys; Library not included

This document outlines the usage of the MQTT Client, MQTT Publish and MQTT subscribe function blocks from the MQTT CLIENT_SL library.

1.10
09/09/2024
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
Festo Synchronized Drive Control Festo Synchronized Drive Control

The FestoSynchronizedDriveControl_library offers function
blocks and methods to synchronize motion of 2 ore more axis.

Library in download-file included.

 

1.10
12/01/2022
FPosCR Integration with Beckhoff PLC through Modbus TCP FPosCR Integration with Beckhoff PLC through Modbus TCP; Library is included

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate with Beck-hoff TwinCAT 3 PLC in TwinCAT 3 programming environment using Modbus TCP communication.

1.10
05/08/2025
FPosCR Integration with Mitsubishi PLC through PROFINET FPosCR Integration with Mitsubishi PLC through PROFINET; Library is included

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in Mitsubishi iQ-R PLC in GX Works3 programming environment using PROFINET communication

1.10
23/02/2026
FPosCR Integration with Omron PLC through EtherNet/IP FPosCR Integration with Omron PLC through EtherNet/IP; Library is included

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in Omron Sysmac Studio programming environment using EtherNet/IP communication.

1.10
05/08/2025
FPosCR Integration with Rockwell PLC through EtherNet/IP FPosCR Integration with Rockwell PLC through EtherNet/IP; Library is included

This Application Note describes how to use the host AOI of the FPosCR from Festo & how to integrate in Rockwell Studio 5000 programming environment using EtherNet/IP communication.

1.10
05/08/2025
FPosCR Integration with Siemens PLC through Profinet FPosCR Integration with Siemens PLC through Profinet; Library is included

This Application Note describes how to use the host function blocks of the FPosCR from Festo & how to integrate them in Siemens TIA Portal programming environment using Profinet communication.

1.10
05/08/2025
FPosCR server integration with Festo PLC FPosCR server integration with Festo PLC; Library is included

This Application Note describes how to use the host sever Function Block of the FPosCR from Festo & how to integrate in CODESYS programming environment using Modbus/TCP, EtherNet/IP and PROFINET communication.

1.20
05/03/2026
How to mount SMB (CIFS) share CECC-…; CPX-CEC-...-V3 , CPX-E-CEC

This application note describes how to establish a SMB (CIFS) share with Festo PLCs CECC-.. and CPX-CEC-..-V3, CPX-E-CEC

1.20
03/08/2020
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.4
12/10/2026
Integration of Flow Monitoring Function Block with Festo PLC Integration of Flow Monitoring Function Block with Festo PLC; Library is included

This Application Note explains how to integrate different Flow monitoring function blocks with Festo PLC and it shows how to configure the function blocks and monitoring and getting the flow data from the function blocks

 

1.10
30/09/2025
Integration of FPosCR Client with Festo PLC through Modbus TCP Integration of FPosCR Client with Festo PLC through Modbus TCP

This Application Note describes how to use the host Function Block of the FPosCR from Festo & how to integrate in CODESYS programming environment using Modbus/TCP communication.

1.20
15/04/2026
Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through Ether-Net/IP Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through Ether-Net/IP

This Application note explains the procedure for integrating the Keyence KV 8000 PLC with the Festo CPX-E-CEC PLC using the KV Studio environment and CODESYS software through EtherNet/IP.

1.10
05/08/2025
Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through OPC-UA Integration of Keyence KV 8000 with Festo CPX-E-CEC PLC through OPC-UA

This Application note explains the procedure for integrating the Keyence KV 8000 PLC with the Festo CPX-E-CEC PLC using the KV Studio environment and CODESYS software through OPC-UA.

1.10
07/08/2025
Lizenzhandling auf Festo Steuerungen Lizenz Datei auf Festo Steuerung; Festo App World

Beschreibung, wie Lizenzen aus der Festo App World auf Festo
Steuerungen verwendet werden können.

1.10
15/03/2021
Mitsubishi PLC with Festo PLC Through Modbus TCP Mitsubishi PLC with Festo PLC Through Modbus TCP; Library included

This application note describes the procedure for configuring Modbus TCP communication between a Mitsubishi PLC and a Festo Controller.

1.10
02/01/2025
Security white paper for Festo controllers

This document is intended to provide users of Festo control products with an introduction and support on how Festo controllers can be used as securely as possible from the point of view of cyber security.

V03
25/05/2023
This application note helps the user to understand the File Handling CPX-E-CEC

This application note helps the user to understand the File Han-dling operations of Codesys PLC’s.

The application note explains the File handling functions of Codesys controller.

The application note also explains data logging operation by writing the PLC data to a csv file in the USB memory.

1.10
22/07/2019
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.