“When companies in the machining world think of growth, they mainly think of more staff and more machines.” In the meeting room of Cellro’s office in Veenendaal, The Netherlands, Director Arnoud de Kuijper explains that it is not the general response of machining companies to focus on automation and digitalisation. “Industry 4.0 is still not widely adopted in these circles and that's what opens up opportunities for us. Our mission is to enable production companies to use this innovation and to play a leading role in it.”

De Kuijper realises that this is easier said than done. “The industry is increasingly moving towards producing small batches and many different products in all sorts of sizes. How can you support that? We want to deliver the flexibility that customers need, but we don't want to reinvent the wheel for every order,” he says, outlining the challenge. “So we have to use standard products and a configure-to-order model with many variables. That is the basis for how we now deal with robotics, grippers and the rest of our technology.”

For Cellro, which for years has specialised in automation solutions for CNC machines, this insight heralded a major transition. “Software has become our biggest differentiator,” says De Kuijper. “We install the hardware at our customers' premises and, thanks to ever better software, we offer them new functionalities.” The focus right now is mainly on Europe. “Especially in the German-speaking countries, there are many machining companies which have a relatively low level of automation. We also see opportunities in the US and Asia, but initially we will concentrate on building up our presence in the region.”

Trouble-free operation

In the workshop, Product Manager Bram de Koning shows Cellro's Elevate, an impressive system that can fully automatically load one or more types of turning, milling or other machines. “We regard the Elevate mainly as a strong logistics solution,” says De Koning, pointing to the four-metre high tower. “It offers a large storage capacity so that users can easily leave it running overnight or even over the weekend without worrying about it.”

De Koning explains that he and his colleagues didn’t sit around doing nothing during the pandemic. About the electrical cabinets he says: “Everything used to be in one big box and was run by one big software project. That made scaling down more difficult. The communication to the CNC machines, which was always custom-made, was also a problem. We thought we could and should do better”.

Cellro rebuilt the hardware and software and distributed them over several electrical cabinets. “On the left is the base cabinet with the majority of the intelligence,” explains De Koning. “This is where the core processes such as the job manager, planning, etc. are run. This cabinet is the same for each machine and each cell.” Of course, the Cellro engineers continue to tinker with the software and can update systems in the field remotely and thus implement improvements.

The control of the Elevate lift has now been separated and placed in a different cabinet with its own PLC. Other product families in the Cellro range also have their own control cabinet. The machine communication is now also kept apart from the basic hardware. “The interface cabinet translates the instructions from our systems into the format in which the CNC machines want to receive them, and vice versa,” says De Koning. “The advantage of this configuration is that we can send this interface to the machine builder or system integrator in advance so that they can already arrange the handshake. That saves a lot of time. We have become much more modular.”