Why end cushioning?
Cost pressures and increasing product demand make it necessary to increase production speeds in automated manufacturing processes. This reduces the cycle time of the machine and thus the throughput time, resulting in more products per unit time.
In order to achieve these higher speeds, it is necessary for the various components in the production facilities to move faster. And with pneumatic cylinders, this leads to greater amounts of energy being released when the fast-moving cylinder has to stop again. In order to manage this in a proper, safe and controlled way, proper damping of the end position is necessary. This absorbs the kinetic or kinetic energy as efficiently as possible, minimising wear and tear and shocks.
Three types of end cushioning
There are roughly three methods for damping specific pneumatic cylinders.
Elastic damping
Within the installations in which pneumatic cylinders are used, elastic and pneumatic damping are the most frequently applied forms of damping. This is partly due to the good price/performance ratio and partly to the amount of energy that must be absorbed. Hydraulic damping, for example, is more common when damping very large forces that do not actually occur in a pneumatic cylinder.
We will now describe the most important properties, limitations and possible applications for each type of damping.
Adjustable pneumatic damping (PPV)
When dynamic forces increase, additional damping is required to prevent overloading of the pneumatic cylinder and the system. With the adjustable air cushioning (recognisable by the abbreviation PPV), a specific volume of air is trapped in the end chamber of the cylinder. The air output - and thus the degree of damping - can be manually adjusted with an adjustment screw.
The required setting of the exhaust air cushioning depends on the mass of the cylinder, the speed at which it is moving at the moment of damping, the acceleration (or own deceleration): speed at which the cylinder should come to a stop, the working pressure and the resistance in the cylinder. A certain amount of experience is required to make the correct setting. When this is lacking, a trial and error process, starting with a relatively high damping, is a solution to reach the optimal setting. During the service life of the cylinder, optimal damping can only be maintained if the setting is regularly checked and adjusted if necessary.