Electric motors convert electrical energy into mechanical motion. An electric motor, regardless of its specific type, consists of several key components that work together:
In this white paper, we will look at the various advantages and disadvantages of different motor technologies.
The most well-known and the most obvious ones are the power requirements and the available voltage, i.e. will a standard power supply network with 400 VAC or 230 VAC or batteries be used.
However, by examining an application in more detail, it quickly becomes apparent that there are other parameters too. These include the torque required, how precisely the motion needs to be controlled, or if the motor is simply used to drive something.
Other questions that may be asked are: what is the inertia of the load, so that the motion can be controlled?
Read all about this in our white paper.
Power Connections
The motor receives electrical power through its power connections. These connections can supply either alternating current (AC) or direct current (DC), depending on the motor design. The power flows into the stator windings, which create a magnetic field essential for motor operation.
Stator and Rotor
The stator is the stationary part of the motor that houses the windings. The rotor, connected to the rotor shaft, is the rotating component. Depending on the motor type, the rotor may contain permanent magnets or electromagnets. The interaction between the magnetic fields of the stator and rotor generates torque, causing the rotor shaft to turn.
Cooling System
Motors often work under demanding conditions, making cooling a critical factor. Effective cooling helps maintain performance and prolongs motor life. Many motors include a fan at the front and air intake vents at the back to facilitate airflow and dissipate heat during operation.
Encoder
Some motors are equipped with an encoder, a device that monitors the position of the rotor shaft in real time. This feedback is vital for precise control in applications requiring accurate positioning or speed regulation.
Brake
While not typically used to slow the motor down, a brake serves as a holding mechanism. It keeps the motor shaft steady when the motor is stopped, preventing unwanted movement especially in vertical applications and ensuring safe operations.
Electric motors are broadly categorized based on their power source—Direct Current (DC) motors and Alternating Current (AC) motors—and further classified by construction and control methods.
DC motors operate on direct current and are common in applications requiring variable speed and torque control. They come in four main types:
These traditional motors use carbon brushes and a commutator to deliver current to the rotor windings. They are simple, low-cost, and easy to control, but brushes wear out over time, requiring maintenance. They are often found in household appliances, toys, and hand tools.
A modern alternative where the rotor contains permanent magnets, and the stator has windings. Electronic controllers replace brushes for commutation, providing higher efficiency, less noise, and reduced maintenance. BLDC motors are compact, capable of high speeds, and used in drones, electric bikes, and compact robots.
Specialized DC motors designed for precise positioning without feedback in many cases. Stepper motors move in discrete steps, making them ideal for controlled motion applications like 3D printers, compact CNC machines, and robotics. Hybrid stepper motors combine features of reluctance and permanent magnet motors for enhanced performance.
These convert electrical energy directly into linear motion, useful in applications requiring precise linear positioning.
AC motors run on alternating current and are widely used in industrial and commercial applications.
Asynchronous motors operate with the rotor spinning at a speed slightly different from the stator’s magnetic field—a difference known as slip. This slip induces current in the rotor, generating torque. The design is robust and simple but offers less precise speed control compared to synchronous motors. Types include:
Synchronous motors have rotors that spin at the exact same speed as the stator’s magnetic field, allowing for precise speed control. Types include:
When selecting an electric motor, understanding the application's nature is critical. Applications generally fall into two categories:
In drive applications, the motor's primary role is to provide power to keep systems running at a consistent speed or torque without the need for precise positioning. Examples include:
Key considerations here are robustness, efficiency, and cost-effectiveness. Motors like brushed DC, asynchronous induction, and synchronous reluctance are common choices due to their simplicity and durability.
These require precise positioning, repeatability, and dynamic control of speed and torque. Examples include:
Motors used here typically involve feedback systems (encoders) and advanced controllers. Stepper motors, brushless DC motors, synchronous servo motors, and linear motors are popular for these applications.
Choosing the optimal motor involves balancing multiple factors:
Selecting the right motor and controller can be challenging given the numerous variables involved. Festo offers an Electric Motion Sizing Tool, an interactive software accessible online that helps engineers:
To illustrate how to select the best motor for a specific task, let’s consider a typical life sciences application involving a liquid handling head dispensing into multiple vials.
A notable innovation is the full servo system based on stepper technology, combining the cost-effectiveness and holding torque of steppers with the dynamic performance and precise control of servo drives. These motors use vector control and field weakening to optimize speed and torque, offering a compelling alternative to more expensive synchronous servo motors.
Decentralized or cabinet-free drive solutions integrate the motor and controller into a single unit installed directly in the field. This approach reduces:
Festo’s latest decentralized servo motor solutions support multiple motor types (steppers, brushless DC) and communication protocols (Profinet, EtherCAT, Modbus TCP), providing flexibility and simplified machine architectures.
The optimal electric motor choice depends on a clear understanding of your application’s requirements. For power-driven applications with less need for precision, robust and cost-effective motors like asynchronous induction or brushed DC motors are suitable. For controlled motion requiring accuracy and dynamic response, brushless DC, stepper, and synchronous servo motors are preferred.
Emerging technologies such as hybrid stepper motors with servo drives and decentralized drive solutions offer new opportunities to enhance performance while reducing costs and complexity.
To make the best choice: