The rotary function in Koppert's so-called cup filler is no longer driven entirely pneumatically, but using the rotary drive unit ERMS from the Festo Simplified Motion Series. This allows Koppert's customers to benefit from the simplicity of pneumatics but the speed and accuracy of servo technology. Moreover, the total solution provides all the possibilities to collect data for optimisation and maintenance purposes.

For Koppert
Finally, the solution is also a pleasure to work with for the machine builder himself. For example, the turntable features a sealed hollow shaft that allows an integrated feed-through for pipes and hoses. Furthermore, it provides a standardised mounting interface and integrated end-position detection. This makes installation during machine assembly easy.

Roshan concludes, "I am very happy with this final result. Through good consultation sessions with Festo and the combination of their expertise and our knowledge of our customers, the machine has become faster but not more complex. A good starting point to see where we can use the SMS even further. Soon, for example, we will apply different Simplified Motion actuators such as the EPCS for linear motion. An ideal concept for a variety of machines."