A stepper motor is a type of DC motor designed to move in discrete steps, allowing precise control of angular position without the need for feedback systems in many cases. Unlike traditional brushed DC motors that rotate continuously, stepper motors divide a full rotation into a number of equal steps, enabling accurate open-loop positioning.
Stepper motors operate by energizing coils in a specific sequence, causing the rotor to move incrementally. Each pulse sent to the motor corresponds to a step, and by counting these pulses, the motor’s position can be controlled precisely. This makes stepper motors ideal for applications requiring repeatability and accuracy without complex feedback mechanisms.
In this white paper, we will look at the various advantages and disadvantages of different motor technologies.
The most well-known and the most obvious ones are the power requirements and the available voltage, i.e. will a standard power supply network with 400 VAC or 230 VAC or batteries be used.
However, by examining an application in more detail, it quickly becomes apparent that there are other parameters too. These include the torque required, how precisely the motion needs to be controlled, or if the motor is simply used to drive something.
Other questions that may be asked are: what is the inertia of the load, so that the motion can be controlled?
Read all about this in our white paper.
Stepper motors are widely used in applications where precise, repeatable positioning is required but the complexity and cost of closed-loop servo systems are not justified. Common uses include:
New generations of stepper motors combine the simplicity of stepper motors with the performance of servo systems. Key features include:
This new class of stepper motors offers servo-like performance at a fraction of the cost, making them ideal for applications where traditional servo motors might be overkill.
For applications requiring precise positioning with moderate speed and torque, stepper motors are often the most cost-effective choice. They excel in:
However, if your application demands high speed, dynamic response, or very high torque, brushless DC or synchronous servo motors might be more appropriate.
Accurate motor selection requires detailed application data and simulation. Advanced sizing tools like Festo’s Electric Motion Sizing Tool help by:
These tools reduce design time, technical risks, and total cost of ownership.
Stepper motors, especially when combined with modern control techniques like vector control and field weakening, can be highly energy efficient. Tools are also available to estimate energy consumption and carbon footprint, helping companies make environmentally responsible choices.
Stepper motors continue to be a versatile, dependable, and economical choice for many motion control applications. Their ability to deliver precise positioning without the need for complex feedback systems makes them especially well-suited for:
With ongoing innovations such as closed-loop stepper motors and integrated drive solutions, stepper technology is evolving to meet more demanding industrial requirements—offering servo-like performance with reduced complexity and cost.
For engineers and designers, utilizing advanced sizing tools and consulting with experts can help ensure the selection of the most suitable motor solution—whether that be a stepper motor, brushless DC motor, or servo motor—tailored to your unique application needs.