Pneumatic pressure is the force created by compressed air within a system. This pressurised air is the energy source that powers a wide range of devices β from cylinders and grippers to valves and actuators β enabling movement, clamping, lifting, and precise control in automated processes.
In a typical system, air is drawn in by a compressor, filtered to remove moisture and particles, and then stored in a receiver tank. From there, it travels through air preparation units, regulators, and valves before reaching the end devices. Each of these components plays a role in maintaining the correct pressure and ensuring consistent performance.
Pressure is expressed in the SI unit megapascals (MPa), but in industry bar and psi are also widely used (1 bar = 0.1 MPa = 14.5 psi).
The required level depends on the application β for example:
Understanding how pressure is generated, transmitted, and maintained is essential for effective system design. Insufficient pressure can lead to slow or incomplete movements, while excessive pressure can result in increased wear, noise, and energy consumption. Therefore, balancing pneumatic pressure is one of the most important factors for achieving energy-efficient automation.
According to guidance from the British Compressed Air Society (BCAS), lowering system pressure can deliver meaningful energy savings β around 5% for a 10% pressure reduction, or up to 7% per bar depending on system design and demand.
Too low a pressure, however, causes inefficiencies such as sluggish actuator movement, too low feed forces, incomplete cycles, or inconsistent product quality β all of which can lead to downtime and higher costs.
Getting pressure βrightβ supports sustainability, cost control, and machine longevity.
Accurate and continuous pressure monitoring is essential for maintaining system reliability, safety, and efficiency. Even small deviations in pressure can affect cycle times, product quality, and energy use, especially in high-precision applications such as packaging, assembly, or laboratory automation.
Monitoring ensures that air pressure stays within the defined range for each process. It also helps detect early signs of leaks, clogged filters, or regulator faults, allowing for preventative maintenance rather than costly downtime.
Common monitoring devices include:
With the growing focus on energy efficiency and predictive maintenance, many manufacturers are integrating smart pressure monitoring systems into their machines.
Digital sensors connected via IO-Link or fieldbus networks transmit real-time pressure data to control systems or dashboards. This enables:
Flow and pressure sensors such as SFAM-EMD, together with energy efficiency modules such as MSE6, can provide measurement and diagnostic data at machine level and help monitor, analyse, and optimise compressed air usage across pneumatic systems.
By combining these sensors with intelligent controllers and dashboards, engineers gain complete transparency over the entire compressed air network β from the compressor station to the actuator.
Reliable pressure monitoring is not just about safety; itβs about optimising performance, energy use, and maintenance planning. The more accurately a system can track and respond to pressure variations, the more efficient and sustainable its operation will be.
Maintaining optimal pneumatic pressure requires both the right components and careful system design. A well-regulated system ensures stable operation, protects downstream equipment, and reduces unnecessary energy consumption.
Key components for pressure control include:
These valves ensure the machine or circuit receives the defined pressure required for the application. To minimise pressure drop and protect the valve from contaminants, a strainer or filter should be installed upstream of the regulator.
Ready to optimise your compressed air preparation?
π Download our whitepaper: Answers to the 5 most frequently asked questions about air prep
Pressure drop is a common challenge in pneumatic systems and can significantly affect performance and efficiency. Even small pressure losses can reduce actuator speed, increase cycle times, and raise overall energy consumption.
Compressed air preparation: from functions to ISO compliance
Explore how to meet ISO 8573-1:2010, ensure proper air quality, and make smart choices for soft-start and pressurisation modules.
π Download our whitepaper: Answers to the 5 most frequently asked questions about air prep