A lab workflow is the full sequence of tasks, people, instruments, and data that turn a sample into a reliable result.
This includes:
Modern workflows mix manual and automated steps. They cover how samples are tracked, how instruments work together, and how data moves into lab information systems.
A good workflow treats these parts as a single, connected, scalable system rather than separate tasks. Planning this way helps labs handle more work, get consistent results, improve safety, and reduce disruptions. It often decides if a lab can keep up with growing demand and grow smoothly.
Labs that depend on manual operations or isolated automation often experience:
Manual labelling, transcription, and handling increase the risk of mislabelled samples, double-dispensed reagents, skipped wells, or misplaced specimens. Late error detection can delay turnaround, compromise study integrity, or affect patient care.
Weak or inconsistent tracking increases the risk of mis-sorted, misplaced, or mixed samples, jeopardising workflow integrity.
Repetitive tasks such as uncapping tubes, pipetting, or plate handling can lead to strain injuries and lower job satisfaction, thereby increasing turnover and training costs.
Workflows relying on manual steps or rigid setups struggle to scale. Expansion often demands major redesigns, extra space, or equipment replacement incompatible with automation.
These challenges impact turnaround time, quality, compliance, and operational resilience, especially as sample volumes and expectations increase.
Labs with streamlined, well‑planned workflows, supported by the right level of automation, can:
Optimised workflows enhance commercial and organisational outcomes by boosting efficiency and reducing errors.
The risks and benefits above demonstrate that workflow design directly influences lab performance, quality, and scalability.
Effective workflows rest on three core principles:
1. Take a holistic, end‑to‑end view of the process.
2. Plan for scalability and flexibility from the start.
3. Integrate automation and digitalisation strategically, with people and ergonomics in mind.
The following sections explain how to put these principles into practice.
Effective workflow design starts by mapping the entire process, not just optimising individual instruments or tasks. This includes: intake to reporting.
This end‑to‑end perspective helps identify bottlenecks, redundant steps, and opportunities for improvement. It also prevents the creation of “islands of automation”: stand‑alone instruments or modules that don’t integrate, use incompatible labware, or require major rework to expand.
At the same time, workflows must be future‑proof. Planning for scalability means:
Labs that skip this step often face costly retrofits, infrastructure changes, or the need to replace equipment that cannot integrate with future automation. In contrast, designing with scalability in mind from the outset ensures that today’s investment remains viable and adaptable as the lab grows.
Before investing in new equipment, it’s essential to strengthen and streamline the underlying process. Many limitations in throughput, reproducibility, and staff well‑being originate from the manual workflow itself. If a process is inefficient or inconsistent, automating it will only reproduce those inefficiencies at a higher speed.
Improvement starts with understanding the current state in detail. Labs should:
This analysis often reveals quick‑win opportunities such as reducing unnecessary sample movements, standardising protocols, and balancing workloads between staff and instruments. These changes alone can significantly increase stability and capacity, even before automation is introduced.
Standardisation is one of the strongest enablers of both quality and automation:
A modular approach makes it easier to evolve workflows over time. By designing processes in discrete, well‑defined modules, such as sample preparation, aliquoting, or extraction, labs can:
This ensures the workflow remains adaptable and scalable while maintaining consistency across the organisation.
As an automation partner, our goal is not to automate everything at once but to focus on areas where automation adds the most value and integrates seamlessly into the workflow. Automation should support, not dictate, the strategy.
Across most laboratories, three areas consistently provide the strongest return on automation:
Automating these steps reduces manual errors, removes bottlenecks, and improves throughput and reproducibility. However, automation must be integrated into the overall system rather than added as isolated units.
To avoid creating new “islands of automation,” labs should:
This approach allows automation to scale naturally as demand grows and prevents costly rework down the line.
For a deeper exploration of where automation has the biggest impact and how to plan an automation journey, see our dedicated article on laboratory automation.
Physical automation and digitalisation go hand in hand. Integrated digital systems — such as LIMS or ELNs — act as the backbone of sample and data management. These systems can:
Seamless data flow reduces transcription errors, enhances traceability, and provides near-real-time visibility into the entire workflow. Labs delaying digital integration often face labour-intensive, costly retrofits later.
Once data is connected, digital tools enable continuous optimisation:
This creates a feedback loop where real-time data drives operational decisions, helping labs meet rising demand while maintaining high-quality, reproducible results.
Working with an experienced automation partner can accelerate and de-risk a laboratory’s transformation. Partners offer insights from multiple implementations across lab types, helping teams avoid pitfalls and design solutions aligned with current needs and long-term goals.
A strong collaboration can help labs:
Successful laboratories view workflow design as a strategic, long-term initiative, not a one-off optimisation. Instead of isolated automation projects, leading organisations build integrated, flexible workflows that evolve with new technologies, regulations, and operational demands.
As expectations for speed, quality, and traceability rise, labs benefit from regularly reviewing workflows and aligning them with best practices. This continuous-improvement mindset ensures that processes remain efficient, compliant, and scalable.
Combining thoughtful workflow design with strategic automation and digitalisation enables laboratories to create systems that perform reliably today and adapt easily to the future. The result is a more resilient, productive, and future-ready operation.
Begin with a structured assessment of your existing process: map the end‑to‑end workflow, measure cycle times and error rates, identify bottlenecks, and prioritise steps that introduce the most variability or delays. Even small standardisation improvements can deliver measurable gains before automation is introduced.
Yes, several of our customer projects show how thoughtful workflow redesign, combined with modular automation, can transform laboratory performance:
• A modular “DNA Factory” for high‑throughput plant genomics
Synchron Lab Automation built a fully automated DNA‑extraction workflow capable of processing up to 40,000 samples in 24 hours, using integrated Festo handling gantries, electric axes, grippers, and barcode scanning. Manual throughput of 2 plates per day increased to 400 plates per day with just one operator.
• Near‑patient molecular diagnostic testing with Fast MDx
Fast MDx redesigned the entire diagnostic workflow to create a mobile, fully automated system for detecting respiratory pathogens. The platform processes 1,000+ samples in an eight‑hour shift with a single technician — five times more efficient than manual processing — thanks to Festo pipetting systems, 3D gantries, and integrated handling.
• High‑throughput liquid handling at MolGen
MolGen’s PurePrep TTR system automates sample preparation with precision gripping, capping/decapping, and pipetting subsystems from Festo, enabling throughputs of 320 samples per hour — far beyond what manual workflows can achieve reliably.
These examples illustrate how labs can scale throughput, reduce manual handling, and build flexible workflows by combining modular automation with a well‑designed process architecture.
Costs vary depending on workflow complexity and the scope of automation, but most labs achieve ROI within 12–36 months. Savings typically come from reduced manual work, lower error rates, improved throughput, and better utilisation of skilled staff. Modular automation enables labs to spread investment over time.
Early engagement is key. Involving analysts and technicians in the planning process, providing hands‑on training, and clearly explaining “why” the change matters all help build ownership. Automation that removes repetitive or ergonomically challenging tasks often improves morale and reduces resistance.
Well‑designed workflows support traceability, reduce manual transcription, and ensure consistent execution — all critical for compliance. Integrated digital systems strengthen audit trails, data integrity, and documentation, making it easier to demonstrate adherence to regulatory standards.