Salt spray tests are common in the automotive industry and the most frequently used method to test paints and other coatings. Components in automation technology, too, have to pass the test. In technology terms, corrosion is seen as an electrochemical reaction of a metal with its surroundings. This reaction may impair the material’s properties and the function of the component made from that material.
Almost every material rusts eventually. The best-known type of corrosion is red rust. This forms when iron or steel oxidises when exposed to damp surroundings. White rust is the corrosion product of zinc.
Festo tests the surfaces of components and new types of coating in the salt spray chamber. The parts are hung on thin hooks and are sprayed with a salt mist, often for days on end. This is much saltier than sea air and can thus reproduce exposure that is similar to years of use in damp, salty surroundings in a very short space of time. Material experts then evaluate the corrosion.