当下,现代化实验室设备、诊断仪器及医疗器械的研发与生产,正前所未有地置身于技术创新、监管要求与经济压力的多重夹击之中。 市场对设备精度、可靠性与微型化的要求日益提高,归档记录、安全保障以及与现有系统的数字集成等亦面临相同局面。
与此同时,许多制造商还正面临资源有限、成本压力攀升、专业人才缺口持续存在等困境。 系统复杂度不断增加,而产品开发与上市的时间窗口却持续收紧。
本文聚焦设备制造产业、特别是 实验室分析技术、临床诊断和医疗技术领域的设备制造所面临的核心挑战,清晰阐述创新型解决方案当下赖以生长的宏观环境与条件。
对于开发人员来说,现代化设备所要实现的紧凑结构无疑为他们带来了巨大挑战。 在实验室设备、诊断仪器和医疗器械中,必须在极其有限的空间内布局大量功能设备,比如传感器、流体结构、电子部件等。 与此同时,业界对人体工学设计、移动便携性和运输适应性的要求亦不断提高。 这就意味着,微型化部件不仅要具备强大的性能,还必须确保稳定可靠、经久耐用。 有限的安装空间要求设计者必须以创新思维进行重构和设计,精心规划系统架构 - 每一毫米都至关重要。 而这,通常会对材料的使用和设备重量带来影响。
负责开发复杂机电一体化系统的团队规模小、任务重,是很多制造商面临的共同挑战。 而在开发过程中,又普遍存在人员欠缺专业知识的问题,这一点在自动化、流体学、电子、软件集成等领域尤为突出。 从概念构思到批量生产,实验室设备、诊断仪器和医疗器械的开发始终离不开对技术的深入理解。 因此,核心优势不在驱动技术或系统集成的企业,正日益倚重外部合作伙伴,从能精准提供专业知识和资源支持的合作伙伴处受益。
设备制造行业面临的经济压力日益加剧,中小批量生产领域尤为显著。 客户既期待性能与可靠性兼备的解决方案,又要求成本效益突出。 然而新设备研发成本高昂,在产品款型多样,生产数量却有限的情况下尤其如此。 为保持市场竞争力,许多制造商正积极采用模块化组件、推进标准化进程,同时引入外部研发支持。 如此既能缩短开发周期、降低成本,又能保证质量和功能。
将流体、电子元件、机械、传感器和软件集成到一台设备中,会导致系统高度复杂化。 为确保正常运行,各接口间必须实现精密协同。 即使系统架构中的微小错位,也可能在审批或应用环节引发严重问题。 因此,以全局视角审视系统集成(最好组建跨学科团队),于成功而言至关重要。
Laboratory, diagnostic and medical devices have to work reliably and precisely for many years, often under changing environmental conditions. The requirements for accuracy, repeatability and long-term stability are very high, especially for sensitive applications such as blood analyses or molecular biological tests. A sturdy design, high-quality components and carefully considered quality assurance are crucial to prevent failures and ensuring patient safety.
For manufacturers of laboratory, diagnostic and medical devices, compliance with legal requirements such as the MDR (Medical Device Regulation), ISO 13485, FDA regulations or IEC 61010 standards is mandatory. At the same time, this is extremely complex. Documentation, traceability and validation must be taken into account as early as the development phase. Errors or omissions can lead to considerable delays, certification problems or even recalls. That is why an in-depth understanding of regulatory requirements is essential.
The time from a product idea to market launch is getting shorter and shorter. At the same time, the demand for customised variants and flexible quantities is increasing. Manufacturers must thus be able to react quickly to market changes and efficiently develop, test and produce new series devices. Agile development processes, modular platforms and close collaboration with experienced partners help to significantly shorten the time to market.
Laboratory, diagnostic and medical devices are now increasingly networked and data-capable. They communicate with hospital IT systems, cloud platforms or laboratory information systems, enabling data to be used and analysed more efficiently. This digital networking places high demands on interfaces, software architecture and, in particular, IT security.
The Cyber Resilience Act (CRA), which will come into force in December 2027, will make cyber security a mandatory part of CE labelling for all products with digital elements. Manufacturers must then ensure that all developments follow the principle of "secure by design" and "secure by default".
In addition to technical performance, the ease of maintenance and servicing of devices is becoming increasingly important. Manufacturers are faced with the task of designing systems in such a way that they require little maintenance, are easier to service and, ideally, enable predictive maintenance. The aim is to minimise downtime, extend service life and organise servicing efficiently. Modern approaches such as predictive maintenance make it possible to recognise maintenance requirements at an early stage, before a failure occurs.
Today, sustainability is a decisive competitive factor and has long since ceased to be simply a "nice to have". Manufacturers are faced with the challenge of reducing the material and energy consumption of their devices without compromising on performance or quality. Resource-saving designs, energy-efficient components and recyclable materials are key tools for combining environmental responsibility and economic success.
The challenges mentioned here make it clear that the demands placed on device manufacturers in the life science industry are high and often cannot be met with conventional standard components. Generic approaches quickly reach their limits, especially when it comes to precision, integration and regulatory safety.