自动化技术中的能源效率已经成为一个热门话题。但是可以利用的节能潜力有哪些?铅笔磨削设备解答了这一问题。该设备可以将铅笔磨削、印花并运输至灌装站,用锡纸打包后运输至仓库。通过这个示范工厂,我们能够以一种清晰且可行的方式解答有关整体能效的问题。
作为一家拥有长期前景的家族企业,无论是在公司内部还是在为客户服务之时,Festo 多年来一直专注于整体能效。始终着眼于整体价值链,从工程设计到节能产品,直到系统的高效设计,以及机械与设备的节能运行,即所谓的“绿色”生产。
展览遵循四步应用法,包括播放视频、展示互动展品(Festo 产品和解决方案)、描述可持续服务以及介绍可靠的培训课程。它所要传递的信息是:在寻找经济有效且完美协调的最佳自动化解决方案的过程中,每个区域的贡献相同。正如在参观开始之时描述的那样,Festo 可以很好地应对 21 世纪的挑战。特别是在资源短缺、气候变化和生态足迹遍布的背景下。
Using three different handling systems – pneumatic, electric and combined – station 1 demonstrates the total cost of ownership with different cycle times over an operating period of several years. Visitors can set the desired amortisation time and determine the most economical solution for them in terms of procurement and energy costs.
Decentralised valve terminals positioned very close to the actuators specifically save compressed air at station 2. But there is much more potential: animated pictures provide information about 11 additional savings opportunities. With a proportional energy consumption of 30% within the German industry sector, such measures are the future.
While station 3 focuses on Festo Energy Saving Services, station 4 describes the services of Festo Didactic. Theory and practice come together here in a sustainable way. Because knowledge leads to new solutions. Whether an energy-efficient screw compressor in the compressor block of a compressed air system or control commands for consistently improving the energy balance.
The “Experience Energy Efficiency” exhibition underlines in an impressive way how Festo is constantly treading new paths in close dialogue with customers, suppliers, leading research institutions and other companies, as a separate innovation area shows.