An important component of the RCM is its sophisticated software system, which is used in conjunction with MRI images for extremely precise positioning of the needle guides. The current images of the target area are compared with previous diagnostic scans. The robot's polymer pneumatic motors then move the needle guide to the exact position. The system is controlled by a valve terminal type MPA from Festo. The doctor then uses the MR images to guide the biopsy needle safely and accurately to the prostate to take a tissue sample for further examination.

Partial automation by a robot makes the biopsy procedure much less stressful for the patient. Thanks to the high precision of the robot, which consists of state-of-the-art polymer stepper motors, one or two tissue samples are taken from a suspicious area. In randomised systematic biopsy, on the other hand, the urologist takes 12-16 samples under ultrasound guidance.