Most motion control delays aren’t caused by the mechanics. It's the unexpected engineering work that piles up:

  • Setting up and validating safety functions can turn into an endless loop of assumptions, test runs, and missing documentation.
  • PLC integration and compatibility issues often surface late, when a drive is connected to a real controller, and the fieldbus settings don’t behave as expected.
  • Add huge commissioning effort, and you get a slow start-up, inconsistent parameters, and avoidable rework.
  • The biggest time waster is the lack of seamless tool support for sizing, configuration, and commissioning: Without a transparent data trail, every change requires new checks across safety motion control, PLC code, and commissioning steps.

A joined-up, digital toolchain tackles these issues early on, so you spend less time fixing and more time finishing.

When you compare motion control solutions, focus on what smooths out the engineering process, not just what looks good on a datasheet.

Efficient, modern motion control starts with an open architecture for your PLC. It should support common industrial Ethernet protocols so you can integrate it into established environments such as Siemens, Beckhoff, Rockwell, and Mitsubishi without redesign your control concept. That PLC flexibility lowers engineering risk for OEMs because compatibility issues show up earlier, not during commissioning.

A scalable system also needs built‑in functional safety. With safety on board the drive the need for external components is reduced and so are any late-stage surprises. Just as important is a seamless data flow across engineering tools, so you keep a consistent set of parameters from sizing through configuration to commissioning. Finally, look for a complete system with drive, motor, actuator and cables designed to work together. It means you will spend less time troubleshooting interfaces.

System Configurator: create your motion control setup

Start by defining a coherent system that fulfils your application needs using the System Configurator. It helps you configure compatible components in one workflow and keeps key parameters consistent from the outset. That continuity reduces avoidable mismatches, supports multi‑protocol planning for PLC integration, and cuts the back‑and‑forth that happens when data is spread out over separate tools.

Electric Motion Sizing: validate and refine the system you’ve configured

Once you have configured that baseline, use Electric Motion Sizing to narrow down your system parameters. Define your application and load case and let Electric Motion Sizing calculate the best solutions. You can see loads, motion profiles, and other technical data so you can confirm whether the selected drive and motor combination meets your axis requirements. Spot oversizing early on and make any adjustments before hardware decisions result in extra wiring, PLC work, and safety motion control validation.

Festo Automation Suite: commission faster with guided setup and consistent data

Your configuration is ready and your hardware on site? Then the Festo Automation Suite helps you move from design to commissioning without the need to reconfigure anything. Guided commissioning steps, parameter specification and diagnostics shorten bring‑up time and make changes easier to trace. The result is smoother commissioning, fewer avoidable faults, and faster progress when you’re integrating motion control into an actual machine.

Safety Validation Wizard: document and validate safety with less manual effort

Projects often grind to a halt at the documentation and validation stage because of safety work. The Safety Validation Wizard supports a clearer, more replicating path to record and verify your safety setup, reducing manual paperwork and ensuring you have all the proof you need of what was actually commissioned. That makes it easier to validate changes, makes safety motion control easier to audit, and allows you to move on confidently to the next step of the build.

MyFesto: keep your data connected across tools and project steps

Re-entering the same information in multiple places is a pain, but with MyFesto this becomes a thing of the past. It forms the connection point between all the tools in your workflow as it helps you transfer and reuse project data across configuration, sizing, commissioning, and safety documentation, so teams can work from the same baseline. The payoff is fewer manual handovers, fewer parameter mismatches, and a smoother path from design decisions to what will actually be running on the machine.

Functional safety works best when it’s included in the design of the motion system right from the start, rather than added later using extra modules, wiring, and workarounds. There are other ways to implement it, but integrating safety into core components such as the drive often reduces the need for external parts and keeps the safety concept consistent throughout every phase. Start by defining what “safe” means for each axis and operating mode, then choose functions such as STO, SS1, SS2, SOS, SLS, SBC and SMS that support that behaviour.

This approach makes safety motion control clear-cut and consistent. It also simplifies supplier evaluation: are the required functions easy to implement, and can you verify them without turning validation into a project of its own?

For brief explanations of each function, check our page on functional safety for electric drives.

If you’re an engineer, a complete motion system cuts the unexpected coordination work that slows projects down. When the drive, motor, actuator and cables come from one supplier, compatibility is guaranteed and there will be fewer interface questions during design and commissioning.

If you’re buying, it means fewer parts to source, approve, and manage, which lowers procurement effort and supports standardisation across machine platforms.

For the project team, commissioning and documentation are simpler because parameters, wiring guidance, and supporting materials are developed around one coherent setup. That reduces risk, speeds up build cycles, and makes motion control rollouts more predictable.

Efficient motion control doesn’t have to mean greater complexity. With a scalable approach that combines open PLC connectivity, integrated functional safety, and a connected digital workflow, you can reduce engineering effort without compromising on safety.

That has positive, practical outcomes:

  • Less effort thanks to fewer handovers and fewer last-minute changes.
  • More safety thanks to clearer validation and a more transparent document trail.
  • Faster commissioning thanks to a consistent flow of data from configuration and sizing through to start‑up.

Combine that with an integrated motion control system (matching components and supporting tools), and your project team gets a motion setup that is easier to design, easier to document, and easier to replicate across machine platforms.