SMT-8G/10G - angled mounting

One of the solutions available on the market is the SMT-8G/10G sensor. This version is suitable for grippers or short stroke cylinders with T- or C-slot and saves space due to its angled mounting. If the grippers are slightly larger, in many cases it is even possible to place two sensors in one slot. This also ensures that all electrical connections are positioned in the same plane, which is an advantage during connection.

Another special feature of this type of sensor is the LEDs that are fitted on two sides. This means that the status of the sensor can always be read from two sides, regardless of the most space-saving installation.

Despite the compact dimensions, the measuring range of these sensors is just as large as that of other common sensors.

SDBT-MSX - large sensing range

Finally, space-saving solutions can be achieved with sensors that have a large detection range. After all, the larger the detection range, the greater the possibilities for space-saving installation.

An example of such a sensor is the SDBT-MSX sensor. This version has a detection range of 20 mm and can therefore be mounted on short stroke cylinders in such a way that the sensor itself does not protrude and become mechanically vulnerable.

You can always contact Festo for advice and tips. We have the knowledge but also the experience with a large number of applications for which smart, space-saving solutions have been designed.