Simply effective control – the technology

To be able to carry out its tasks successfully, Controlled Pneumatics requires the interaction of several technologies: valves and valve terminals with piezo technology, sensors, controllers and a powerful control algorithm.

Proportional pneumatic valves such as VEAB, VPPI or Motion Terminal VTEM form the essential basis. The small VEAB, for example, reacts incredibly quickly to deviations in dancer rollers. This keeps the tension as even as possible when winding high-tech yarns. The integrated piezo technology with its speed and precision contributes a great deal. ​​

Proportional valve VPPI with its plunger coil actuator or Motion Terminal VTEM with piezo technology for pilot control are suitable when winding film or paper, for example. With the Motion Terminal, this is done via integrated motion apps.

Integrated sensor technology records and processes the data. These are made available to the higher-level controller for parameterisation and evaluation via a powerful communication technology. The specified parameters can thus be controlled almost in real time, which significantly increases production reliability.

In addition to the hardware, a powerful control algorithm that can be optimised to the specific requirement is one of the central features of Controlled Pneumatics. Our experts are constantly exchanging information to ensure that the hardware of Controlled Pneumatics works together as effectively as possible. This allows them to take into account the specific requirements of each automation solution. This is the only way to achieve optimal results.