End-of-Arm-Tooling

EOAT(End-of-arm tooling)은 로봇 또는 핸들링 시스템과 작업물 사이의 필수적인 인터페이스를 형성합니다. 로봇 팔에 부착되는 이러한 특수 툴 또는 엔드 이펙터를 사용하면 파지, 결합 또는 테스트와 같은 특정 작업을 정밀하게 수행할 수 있습니다. EOAT가 없다면 로봇과 핸들링 시스템은 기능 없는 동작 기계에 불과할 것입니다.

이러한 도구를 통해 로봇은 부품 잡기, 부품의 연결 또는 제품 테스트와 같은 특정 작업을 수행할 수 있습니다.

EOAT의 대표적인 작업:

  • 재료 핸들링: 부품의 그리핑, 리프팅, 배치하기입니다.
  • 가공: 드릴링, 그라인딩, 용접 또는 나사 조이기.
  • 품질 검사: 치수 정밀도 및 무결함의 센서 기반 제어.

EOAT는 로봇에게 복잡한 자동화 프로세스를 구현하는 데 필요한 적응 능력과 효율성을 제공합니다. 특수 툴을 사용하면 일반 매니퓰레이터(Manipulator)를 각 요구사항에 정확하게 맞춘 고도로 맞춤화된 시스템으로 만들 수 있습니다.

EOAT 옵션: 간단한 그리퍼부터 맞춤형 솔루션까지

적용 분야와 작업에 따라 사용되는 End-of-Arm-Tool은 다양합니다. 가장 중요한 유형:

Grippers

Grippers are the most commonly used EOATs. They come in various designs, from simple pneumatic or electric grippers consisting of one product to complex grippers for larger components that offer format adjustment to enable flexible gripping. They are suitable for tasks where objects need to be gripped, held and transported to another location. Robot grippers can be flexibly configured to handle objects of different shapes and sizes. These includeprecise force-fit or form-fit grippers such as parallel grippers,vacuum grippers that avoid damaging the workpiece by only gently touching it using suction cups as well asvirtually contactless Bernoulli grippers.

Machining tools

Machining tools include joining tools such as welding guns, riveting tools, screw heads and dosing units for bonding. Machining operations such as drilling, milling or grinding can also be carried out directly with EOATs. This means that the robot can be used not only as a material handling tool, but also as a production machine. They are ideal for ensuring that repetitive processing steps are carried out with a consistent level of quality and safety.

Special solutions

There are numerous special-purpose tools that have been designed for specific tasks. These include sensors for quality control, optical control systems, painting solutions or EOATs for special assembly solutions. Thanks to these special tools, the capabilities of a robot are significantly expanded and they can be used to solve complex tasks efficiently.

Trends and innovations in end-of-arm tooling

End-of-arm tooling technologies are constantly evolving and have a lasting impact on robotics and automation technology. The latest trends include:

  • Collaborative robots (cobots): EOATs for collaborative robots put safety and ergonomics squarely in the foreground. The environment of these cobots is equipped with highly sensitive sensors that enable them to recognise and adapt to obstacles in real time. This makes them ideal for use in factories where people and robots work closely together. That means tools must also be switched off safely if there is a potential hazard. Advances in software integration also improve seamless control and facilitate the integration of EOATs into existing production systems.
  • Artificial intelligence (AI): AI-supported EOATs offer significant advances for automation. They can use machine learning algorithms to optimise their movements, gripping force and task planning based on real-time data and predictions. One application example is the adaptation to different object shapes or weights, providing even greater flexibility. These types of developments help to avoid time-consuming retooling processes or the need for programming when changing tools.
  • Lightweight construction and material innovations: The use of lightweight yet sturdy materials such as carbon fibre and high-performance plastics has significantly improved the efficiency of modern EOATs. These materials not only reduce the energy consumption of robots and handling systems, but also increase their load-bearing capacity and dynamics. At the same time, they simplify the handling and servicing of the tools, which reduces operating costs. These new technologies also improve durability and corrosion resistance, even in demanding environments such as body shops or press shops.

In addition, there are innovative combinations of sensors and gripper technology on the market that are pushing the boundaries of what is feasible in automated material handling. These advances not only make EOATs more efficient, but also more versatile.