For many machine builders, functional safety still feels like a constraint. It is often not thought about until late in the project, it adds complexity and creates pressure around validation, documentation and commissioning.
That approach is no longer working.
In automotive production, especially in e-mobility applications, machines need to combine high throughput with flexible layouts and safe interaction between people and motion. At the same time, regulatory pressure is rising. New requirements for machinery, cybersecurity, and safety integration are changing what good machine design looks like.
The challenge is clear: how do you meet higher safety expectations without turning safety into a production obstacle?
The answer starts with a shift in mindset. Functional safety is not only about reducing risks. When it is correctly designed and integrated early on, it also helps improve engineering speed, machine availability, energy efficiency and future-readiness.
Many safety concepts are still developed as an afterthought. Risks are assessed late on in the process, protective measures are added afterwards, and safety functions are separate from the rest of the machine design.
That usually creates avoidable problems:
Having to address these problems means many automotive OEMs and machine builders lose time. They know safety is necessary, but they struggle because safety wasn’t built into the architecture early enough.
Functional safety should be an integral part of the machine concept, not be bolted onto it.
A better approach is to start earlier and integrate safety directly into the machine design.
That involves taking into account three points right from the beginning:
1. Risk assessment with the actual application in mind
A sound safety concept starts with understanding which parts of the process present a risk. In automotive and battery production, controlled movement, manual interaction and high-value processes are often closely linked. That raises the importance of having a precise risk assessment.
When the risk is clear, the required safety level becomes clear too. That reduces guesswork later.
2. Safety functions that match the machine architecture
The next step is to define which safety functions are needed and where they should be included in the system. This is where many teams face a trade-off between protection, complexity and flexibility.
The best approach is to match safety functions to the application, the motion profile and the machine layout from the start. That gives engineering teams more control over system behaviour and avoids overspecification.
3. Implementation that supports performance
Circuit design and component selection decide how safety worksin practice. Response times, diagnostics, restart behaviour and fault handling all affect productivity.
Good safety design protects people. It also protects output.
One of the biggest shifts in modern machine design is the move from centralised safety concepts to safety functions placed closer to the actuator.
This matters because the closer safety is the motion, the faster and more precisely the system can respond. It also simplifies architecture in modular machine sections and can reduce unnecessary energy use.
That offers real benefits:
This is the point many teams miss. Safety doesn’t have to slow a machine down. When it is integrated properly, it makes the machine run better.
There is a widespread assumption that improved safety always leads to higher energy consumption and reduced availability. In practice, the opposite is often true. When safety functions are selected and integrated correctly, they help avoid waste and increase the overall efficiency of the machine. Defined safety strategies and intelligent motion management can reduce unnecessary air consumption, lower losses and shorten cycle times — all of which contribute to a highly efficient machine concept. This is especially important in automotive production, where efficiency targets are constantly rising alongside quality and compliance requirements. Functional safety should not be considered separately from efficiency decisions. It should be part of those decisions.
In e-mobility production, the pressure is even greater. Battery manufacturing involves a combination of sensitive processes, valuable materials and demanding safety expectations. That makes it even more important to have robust, well-integrated safety concepts.
But the principle is not limited to just battery production.
Whether the application is in battery assembly, electric powertrain production or wider automotive automation, machine builders need solutions that support safe motion, simpler engineering and reliable operation. The machine must be productive while meeting current and emerging standards.
That is why a technology-neutral approach matters. Electric and pneumatic safety functions both have a role to play, and many applications benefit from the right combination of both.
Not every machine has to be redesigned from scratch. Many manufacturers and machine builders need to retrofit existing equipment to meet newer safety regulations or updated internal standards.
That is where scalable safety concepts and piggyback-style upgrades become useful. Instead of redesigning the entire system, it is easier to modernise selected safety functions, improve diagnostics or align machine sections with current requirements.
Retrofitting shouldn’t turn into a major rebuild.
The right safety architecture helps protect existing investments while making the machine easier to adapt.
Festo supports machine builders with functional safety solutions that combine engineering, safety and productivity.
That includes support for:
This matters because machine builders rarely need individual components for automotive and e-mobility applications. They need safety concepts that fulfil real machine requirements and help them move from risk analysis to implementation with less hassle.
For the most competitive machine concepts functional safety is now part of the machine performance.
That changes everything.
You can design for safer motion without overcomplicating the system. You can support current standards without creating unnecessary engineering effort. And you can improve efficiency and availability while protecting people and processes.
That is the real shift.
Functional safety is no longer a final tick box. It is part of building better automotive machines right from the start.
If you are reviewing a new machine concept or upgrading an existing automotive application, find out how integrated functional safety can reduce complexity and support more efficient machine design.