Portál podpory

Vyberte kategorii nalevo nebo použijte vyhledávání.

Vyhledat

Číslo dílu

Série

Objednací kód

Software FESTO AUTOMATION SUITE 8074657
Popis Verze
Festo Automation Suite Parameterisation, programming and maintenance of electronic devices by Festo

New Features:

  • Display of Notification, e. g. in case of new available software versions or trace recordings
  • Support for transferring licenses into devices
  • Device state "no errors" in connection area of Plug-ins now displayed in green
  • Width of project list on start page and in backstage menu can be modified


Fixed Bugs:

  • Firmware files for new devices (e. g. CMMT-AS-C5) cannot be downloaded (V1.3.2)
  • Crash at application start when used with certain Windows language packs (V1.3.2)
  • Crash when installing Plug-ins at low disk space
  • Crash at application start when installed in user folder
  • Installation fails with error code 0x80070643 in rare circumstances
  • Crash when saving if the opened project has been deleted from the file system
  • Devices not found in the network scan if the network interface is added after the application has started
  • Message "Renaming not possible" appears without reason and blocks the application
  • Multiple selection in Designer is cancelled when opening context menu
  • Error when displaying documents that have been downloaded before
1.3.2
31.01.2020
Festo Automation Suite Parameterisation, programming and maintenance of electronic devices by Festo

New Features:

  • Display of Notification, e. g. in case of new available software versions or trace recordings
  • Support for transferring licenses into devices
  • Device state "no errors" in connection area of Plug-ins now displayed in green
  • Width of project list on start page and in backstage menu can be modified


Fixed Bugs:

  • Crash when installing Plug-ins at low disk space
  • Crash at application start when installed in user folder
  • Installation fails with error code 0x80070643 in rare circumstances
  • Crash when saving if the opened project has been deleted from the file system
  • Devices not found in the network scan if the network interface is added after the application has started
  • Message "Renaming not possible" appears without reason and blocks the application
  • Multiple selection in Designer is cancelled when opening context menu
  • Error when displaying documents that have been downloaded before
1.3.1.57
29.11.2019
Festo Automation Suite Parameterisation, programming and maintenance of electronic devices by Festo

New Features:

  • PositioningDrives data import
  • Support for modular EtherCAT slaves in EtherCAT scan
  • EtherCAT slaves can be imported when importing a PLC from the device scan
  • Release notes for available and installed Plug-ins and Extensions
  • Connections in Designer now using colors for different connection types
  • Devices with identical IP address (path to the engineering interface) are tagged with a warning icon in Designer
  • Warnings for parameter pages are indicated in Plug-in navigators (similar to errors)


Fixed Bugs:

  • Misleading error message when trying to check for updates without Internet connection
  • Undocked windows cannot be moved when trying to drag certain areas of the window title bar
  • Context menu in Designer does not work correctly for multiple selections
  • Cursor cannot be set with the mouse when renaming a device


System Requirements:

  • Windows 7/10 (32/64 bit)
  • Screen resolution 1600x900 or higher recommended
1.2.1.16
06.06.2019
Festo Automation Suite Parameterisation, programming and maintenance of electronic devices by Festo

New Features:

  • EtherCAT scan (only non-modular devices)
  • Manual access also for motors, axes and gears


Fixed Bugs:

  • Firmware is not shown correctly after downloading it into the repository
  • Connections between devices get lost when copying and pasting
  • Opening the scan view while the application window is shown in reduced size might freeze the application


Known Issues:

  • After importing a modular device from the EtherCAT scan, its modules still need to be configured manually.
  • Downloading a firmware to a CMMT-AS with improper network settings stops at 10 %, and the application freezes.
1.1.1.610
16.01.2019
Festo Automation Suite Parameterisation, programming and maintenance of electronic devices by Festo

New Features:

  • English online help

 

Fixed Bugs:

  • Opening a Plug-in by double clicking the device in the navigator does not work
  • Access error message after Plug-in installation
  • Firmware file cannot be downloaded after the user interface language has been changed
  • Searching for firmware updates sporadically fails
1.0.3.6
23.07.2018
Přihlásit k odběru RSS