14/11/2016

Automation is the answer to increasing sample numbers

Automation is the answer to increasing sample numbers

Ready-to-install, precision handling solutions from Festo simplify processe
Reliable manufacturers of automation such as Festo with worldwide availability help reducing the pressure on laboratories.

Automation is the answer to increasing sample numbers

Ready-to-install, precision handling solutions from Festo simplify processes

 

The pressure on laboratories is continuing to grow: in the age of high-throughput methods, not only do results need to be obtained quickly, but traceability and reproducibility must also be guaranteed. It helps to be able to depend on reliable manufacturers of pneumatic and electric automation technology such as Festo, whose products and solutions are available worldwide.

 

Automation does not necessarily mean converting all previously manual processes to become fully automated. The transition often takes place in steps, from automating modules and automated linking of modules to fully automating entire processes, based on the needs and requirements of the laboratory. Automation is the ideal solution to the conflict of objectives between processing large numbers of samples and delivering the required high quality and reproducibility.

                                                    

Modular, linear and integrated

Individual automation concepts are flexible in the degree of automation they can provide. The overall analytical process, for example, involves steps that have to be repeated over and over again every day, such as opening sample vials. Automation helps to minimise the risk of contamination and mistakes caused by repetitive work.

 

Linear automation links modules within a process, meaning less manual work for personnel. Since samples are automatically transported from module to module or device to device, it means that laboratory technicians no longer have to interrupt their work.

 

Tracing of processes

Integrated automation solutions use extremely advanced technology. Complete processes – from preparation to reading out the results – take place within a single overall system. Automation makes processes replicable and simplifies traceability. This makes it easier to comply with legal requirements and regulations.

 

In order for cooperation with automation manufacturers such as Festo to be successful for plant manufacturers, all parties must concentrate on their key competencies. The plant manufacturers are familiar with the laboratory processes, while Festo looks after the automation of these processes, both in the liquid handling system and in the sample handling system.

 

Advancement through innovations

The days when processing individual samples inevitably meant manual processing are past. The new generation of laboratory devices and systems identifies the testing requirements of primary samples with the help of barcodes, prepares the samples for the required tests and distributes them to the corresponding test stations.

 

Automation makes process steps such as identifying, opening and aliquoting a sample as well as loading centrifuges and incubators much more efficient and reliable. Festo develops custom solutions for many of these processes, in some cases also integrating components and devices from third-party manufacturers. These custom solutions increase sample processing productivity, enabling laboratories to process more samples in the same amount of time – regardless of whether in the pre-analytical, analytical or post-analytical phase, whether in clinical or medical laboratories or whether the samples are from humans, animals or plants.

 

About Festo:

Festo AG is a global player and an independent family-owned company with its headquarters in Esslingen am Neckar, Germany. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 200 industries. Our products and services are available in 176 countries. With about 18.700 employees in 61 companies worldwide, Festo achieved a turnover of around €2.64 billion in 2015. Each year around 8 % of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Yet training services are not only provided for Festo's own staff – Festo Didactic SE also supplies basic and further training programmes in the field of automation technology for customers, students and trainees.

 

www.festo.com/lab

 

Contact:

Christopher Haug

+49(711)347-4032
+49(711)34754-4032

Festo Media Service

 
 

Photos

Caption Download
Festo press photo Chart Degree of Automation High flexibility: individual automation concepts adapt to the requirements of the laboratory. (Photo: Festo AG & Co. KG)
Festo press photo Laboratory Platform Linear automation links modules within a process. The samples are automatically transported from device to device. (Photo: Festo AG & Co. KG)
Festo press photo Scan Module High quality and reproducibility: automated documentation of the samples using a sensor helps to minimise mistakes caused by repetitive work. (Photo: Festo AG & Co. KG)
Festo Pressebild Kleinbauendes Handlingsystem Integrierte Automationsl√∂sung: Innerhalb eines Gesamtsystems lassen sich komplette Prozesse und Ergebnisse leichter nachvollziehen und r√ľckverfolgen. (Foto: Festo AG & Co. KG)