20/01/2021

New configurator from Festo

New configurator from Festo

Saves time and effort when selecting and ordering process valves
Making it easier and quicker to select the correct valve or actuator for your process application

New configurator from Festo saves time and effort when selecting and ordering process valves

 

Industrial automation specialist Festo has introduced a new online configuration tool that makes it easier and quicker to select the correct valve or actuator for your process application. Simply select a few parameters and the Festo valve configurator will suggest appropriate combinations, offering a fast, reliable and easy way for process engineers to source coordinated and ready-to-install solutions.

 

Commenting on the new valve configurator, Leon Kelly, Manager of the Process Automation Centre for Festo UK & Ireland, says:
“Configuring the optimum process automation solution for your media is child's play using the Festo online configurator. It simplifies the whole engineering and purchasing process and allows you to obtain the perfect valve unit in just a few clicks. It includes some really helpful features: for example, the configurator can generate a bill of materials to show the component breakdown. Also if you need a configuration ID for repeat orders, or a CAD model for your final configured solution, that’s not a problem – the configurator can produce those as well.”

 

The online valve configurator is ideal for selecting Festo butterfly valve units (KVZA), ball valve units (KVZB) and quarter turn actuator units (KDFP). It simplifies the specification and purchase process by ensuring that all components – from process valves, actuators, pilot valves and limit switch boxes to positioners, adapter kits and hand levers – are from a single source and are perfectly matched and pre-assembled. It is also possible to use the configurator to select an actuator unit without the process valve: ideal for automating existing process valves, or where there is a preference for a third party supply.

 

Following a step-by-step guide, the user simply chooses the required parameters in the configurator’s input menu. The configurator suggests the right solutions by taking all relevant factors into account: from the initial product search, configuration, sizing and documentation right through to ordering and delivery of the ready-to-install process valve or quarter turn actuator unit. The configurator can also accommodate unique customer-specific requests.

 

Together with the proposed solution, the configurator automatically generates an order ID for the complete combination, which can be used for placing future orders. There are also benefits in terms of documentation because the CAD data for the complete, configured unit can be downloaded. Immediate price and delivery time information also make the ordering process easier.

 

Digital journey
The online valve configurator is the latest solution from Festo designed to drive digitalisation forward and support customers as they enter the age of Industry 4.0. As an automation expert, Festo is combining its extensive knowledge of industrial applications with the latest developments in information technology to realise online applications for industrial automation best practice.

 

Festo is also using digital communication to support its customers throughout the Digital Customer Journey, guiding users safely and comprehensively through the Festo portfolio: from information procurement and configuration, through ordering and delivery, to commissioning and maintenance: as well as the technical training offered by Festo Didactic.

For more information about Festo process automation products and to access the valve configurator visit: www.festo.co.uk/process

Contact:

Nicola Meadway

+44(1252)77-5052
+44(1252)77-5015

Festo Media Service

 
 

Photos

Caption Download
Festo’s online valve configurator Select the correct valve or actuator for your process application quickly and easily