Festo Media Service

Please select a category on the left or use the search.

Caption Download
The automated chameleon tongue
Adaptive Shape Gripper 1 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 2 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Stefanie Seiler and Nenja Rieskamp These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development) (Photo: Festo AG & Co. KG)
Festo doubles revenues in the automation of battery production
Festo Press Image Electromobility Festo doubles revenues in the automation of battery production. (Photo: Festo AG & Co. KG
Astonishing space efficiency
ELGC Ideal ratio of installation to working space: the spindle axis ELGC-BS combined with the servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
EGSC Impresses with compact dimensions: mini-slide EGSC with servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
handling ELGC + EGSC Verblüffende Raumeffizienz: ELGC und EGSC kombiniert in einem Handling-System in adapterfreier „One-size-down“-Montage (eine Größe kleiner möglich) (Foto: Festo AG & Co. KG)
Flexible, yet standardized
Harwin 1 Modular design: the three stations of the Gecko assembly line for inserting, press-fitting and bending the contact pins – designed using standard components from Festo (Photo: Festo AG & Co. KG)
Flexible, yet standardized
Paul McGuiness “The modular concept developed together with Festo future-proofs our assembly lines” says Paul McGuinness, Operations Director at Harwin (Photo: Festo AG & Co. KG)
Flexible, yet standardized
Harwin 2 Everything for the servo press kit YJKP is available from a single source: drive package, controller, and application software (Photo: Festo AG & Co. KG)
Flexible, yet standardized
Harwin 3 Dynamic and precise: the compact handling system YXMx takes care of the XY movement of the connectors below the servo press (Photo: Festo AG & Co. KG)
Flexible, yet standardized
Harwin 4 Everything under control with the servo press kit YJKP: controller CECC-X and motor controller CMMP including application software. (Photo: Festo AG &Co. KG)
Flexible, yet standardized
electronics illustration image Festo – automation partner of electronics manufacturing (Photo: Festo AG & Co. KG)
First turnkey IoT solution
CPX-IoT-Gateway Secure connection to the Festo Cloud and exclusive access to individual digitalisation: the IoT gateway CPX-IoT. (Photo: Festo AG & Co. KG)
First turnkey IoT solution
Portrait Michael Hoffmeister “Festo is working closely with other companies in the German Electrical and Electronic Manufacturers’ Association and on the Platform Industry 4.0 project to create a common reference architecture,” explains Dr Michael Hoffmeister, Management Expert at Festo in the newly founded Digital Business section. (Photos: Festo AG & Co. KG)
First turnkey IoT solution
YXMx Kinematics with controller, software packages for motion tasks and condition monitoring, and an app for cloud-based visualisation: the modular positioning platform YXMx from Festo. (Photos: Festo AG & Co. KG)
Revolution in automation
Revolution in automation
Revolution in automation
Expertise in automation for clean rooms
Clean room test Festo has been conducting particle tests to determine the suitability of standard products for use in clean rooms for over 25 years. More than 80 electric and pneumatic automation product series are suitable for use in clean room class 6 and higher. (Photo: Festo AG & Co. KG)
Expertise in automation for clean rooms
ADN Automation products perfectly suited for use in clean rooms: pneumatic compact cylinder ADN (Photo: Festo AG & Co. KG)
Expertise in automation for clean rooms
DGSL Automation products perfectly suited for use in clean rooms: pneumatic mini slide DGSL (Photo: Festo AG & Co. KG)
Expertise in automation for clean rooms
EGC-BS Automation products perfectly suited for use in clean rooms: electric axis EGC-BS (Photo: Festo AG & Co. KG)
Expertise in automation for clean rooms
EXCM Automation products perfectly suited for use in clean rooms: planar surface gantry EXCM (Photo: Festo AG & Co. KG)
Expertise in automation for clean rooms
Direct measurement of particles With the direct measurement method, measurement is performed directly on the critical areas of a test object. (Photo: Festo AG & Co. KG)
Highly dynamic handling unit with control system in uncomplicated package
EXCH 1 Contactless high-speed handling unit EXCH: this Cartesian high-speed H-gantry is beating all speed records. It is 30 percent faster than any conventional Cartesian handling system while the initial costs are comparable. (Photo: Festo AG & Co. KG)
Highly dynamic handling unit with control system in uncomplicated package
EXCH 2 The innovative 3D/planar surface gantry covers a rectangular working area that is significantly larger than that of robot systems with delta kinematics, which can only work in round or kidney-shaped areas. (Photo: Festo AG & Co. KG)
Highly dynamic handling unit with control system in uncomplicated package
CMCA The innovative 3D/planar surface gantry covers a rectangular working area that is significantly larger than that of robot systems with delta kinematics, which can only work in round or kidney-shaped areas. (Photo: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling Guide Online Screen 1 DE Handling Guide Online von Festo: Damit konfigurieren und bestellen Konstrukteure und Projekteure smart und intuitiv ihre neue Systemlösung – in gerade einmal 20 Minuten. (Foto: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling Guide Online Screen 1 EN Handling Guide Online from Festo: allows design and project engineers to configure and order new system solutions intelligently and intuitively – in just 20 minutes. (Photo: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling Guide Online Screen 2 DE Strukturierte Datenabfrage und Planungssicherheit: Ein Großteil der Engineering-Kosten entfällt, detaillierte Produktkenntnisse sind unnötig. (Foto: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling Guide Online Screen 2 EN Structured data querying and planning security: a large portion of the engineering costs are eliminated and detailed product knowledge is unnecessary. (Photo: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling Guide Online Screen 3 DE Ausgewähltes Handhabungssystem im Handling-Guide Online: Das Datenblatt sowie das konfigurationsrichtige CAD-Modell stehen in allen gängigen Dateiformaten sofort zum Download zur Verfügung. (Foto: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling Guide Online Screen 3 EN Selected handling system in the Handling Guide Online: the data sheet and the correctly configurated CAD model are immediately made available for download in all common data formats. (Photo: Festo AG & Co. KG)
The right handling system in just 20 minutes
Handling With the Handling Guide Online, machine and equipment manufacturers are able to reduce time-to-market by the revolutionary amount of roughly 70% with regard to integrated handling systems. (Photo: Festo AG & Co. KG)
Show 30 more results ...