Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description
Energy saving in pneumatic systems
Energy saving in pneumatic systems

The issues related to energy saving are becoming more vital each day. In the factories or even in the small workshops, the intelligent use of every energy source and the right sizing and selection of components save significant amounts of cost, time, waste etc. Compressed air is a very important energy source for industrial production. The possibilities to save costs from production to consumption of compressed air are enormous. But everything begins with the attention of the people who work with it. The training course focuses on peoples’ attention of costs and improving the areas of compressed air production, distribution, preparation and the pneumatic circuits. This training especially matches the customers’ training needs who had already received a Festo Energy Saving Service.

CoDeSys version 3 - A hardware independent introduction to PLC programming
CoDeSys version 3 - A hardware independent introduction to PLC programming

In order to master the fast-changing requirements of embedded and PC-controlled industrial applications, it is increasingly important to master and apply different programming languages. This is complicated by the huge variety of programming software available. Differences in user-interface, functionality and commands sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

CoDeSys version 3 - A hardware independent introduction to CoDeSys
CoDeSys version 3 - A hardware independent introduction to CoDeSys

Flexibility despite a high degree of automation is one of the most important challenges in manufacturing companies. It demands the integration and networking of different controls in a complex automation system. This is complicated by the huge variety of programming software available. Differences in user interface, functionality and command sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

CoDeSys version 2 - A hardware independent introduction to PLC programming
CoDeSys version 2 - A hardware independent introduction to PLC programming

In order to master the fast-changing requirements of embedded and PC-controlled industrial applications, it is increasingly important to master and apply different programming languages. This is complicated by the huge variety of programming software available. Differences in user-interface, functionality and commands sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

CoDeSys version 2 - A hardware independent introduction to CoDeSys
CoDeSys version 2 - A hardware independent introduction to CoDeSys

Flexibility despite a high degree of automation is one of the most important challenges in manufacturing companies. It demands the integration and networking of different controls in a complex automation system. This is complicated by the huge variety of programming software available. Differences in user interface, functionality and command sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

Maintenance and Troubleshooting of electropneumatic systems using PLC controls
Maintenance and Troubleshooting of electropneumatic systems using PLC controls

This course allows you to extend your technical and methodological knowledge and to identify and eliminate faults without delay using a systematic procedure and the ability to understand the functional relationships of complex machinery.

Introduction to Electrical Drives
Introduction to Electrical Drives

As electrical drives are increasingly used in industry, many mechanical engineers and technicians are confronted with this new and initially complex technology and are expected to be able to commission and maintain it. This is a daunting prospect for anyone that has not had proper training. This course aims to provide this target group with the attitudes, skills and knowledge they need to master the basics. On completion of the training participants are able to select the most appropriate components for a given application, safely commission drives, and locate and eliminate simple faults.

Mastering machinery safety 2
Mastering machinery safety 2

Machinery can be a combination of machines. In this case we are dealing with an Integrated Manufacturing System (IMS). The information about IMS can be found in the harmonised standard EN ISO 11161:2010 Safety of machinery – Integrated manufacturing systems – Basic requirements.

Mastering machinery safety 1
Mastering machinery safety 1

Since December 2009 it is compulsory to use the “new” machinery directive 2006/42/EC. This requirement together with the harmonised standards could translate into a significant change in your organization. Other than several small modifications and additions, the new IIB declaration (referred to as the declaration of incorporation) is also introduced. Technical files and user manuals with information about transportation, installation, commissioning, adjustment, maintenance, disassembly, scraping and recycling must be created and delivered with the partially completed machinery.

Design of Pneumatic Controls
Design of Pneumatic Controls

Provide participants with the skills and knowledge to design, assemble, commission, maintain and troubleshoot advanced pneumatic control systems and equipment.

Introduction to Pneumatics
Introduction to Pneumatics

Provide participants with the skills and knowledge to assemble, commission, maintain and troubleshoot basic pneumatic control system and equipment.

Vacuum in handling technology
Vacuum in handling technology

In this training course, participants learn about the basic specifics of vacuum compared to compressed air.
The production of vacuum, selection of the right suction cups, and also opportunities for cost reduction
are mainly covered.

Subscribe to RSS