Festo Media Service

Please select a category on the left or use the search.

Caption Download
Digital Maintenance Management by App
Smartenance Smartenance: the first digital maintenance app for system operators and production managers. (Photo: Festo AG & Co. KG)
Condition monitoring in the cloud at the press of a button
Dashboard Improves operating transparency for production managers and operators: turnkey, preconfigured dashboards of Festo. (Photo: Festo AG & Co. KG)
Adding value to supply chains through additive manufacturing
Festo press photo HP Center of Excellence 1 HP’s new 150,000 sq. Ft 3D Printing and Digital Manufacturing Center of Excellence in Barcelona, Spain. (Photo: HP)
Adding value to supply chains through additive manufacturing
Festo press photo HP Center of Excellence 2 HP’s new facility integrates flexible layouts for collaboration across engineering, R&D groups, customers, and partners with fleets of the latest plastics and metals 3D production system for rapid and agile product development. (Photo: HP)
Bringing artificial intelligence directly to the machine
Festo press photo Tanja Maaß “The crucial factor is therefore bringing AI directly to the machine and interpreting data there – directly at the source – in real time”, says Tanja Maaß, Resolto’s Managing Director. (Photo: Resolto Informatik GmbH)
Bringing artificial intelligence directly to the machine
Festo press photo Resolto The Scraitec software solution from Resolto knows the healthy condition of a plant and detects every anomaly with the real-time analysis of the plant’s sensor data. (Photo: Resolto Informatik GmbH)
Bringing artificial intelligence directly to the machine
Festo press photo CPX-IOT With the Festo IoT Gateway CPX-IOT as hardware, customers can have their machine and plants monitored at field level. Field level support is provided with the ScraiField software component. (Photo: Festo AG & Co. KG)
How will the digitalisation of mechanical engineering evolve?
Dr Michael Hoffmeister “Getting started couldn’t be easier: Festo has a host of digital products from which users can already benefit”, explains Dr. Michael Hoffmeister, Executive Expert Digital Business with Festo. (Photo: Festo AG & Co. KG)
How will the digitalisation of mechanical engineering evolve?
Smartenance Smartenance: This software program from Festo is a digital maintenance manager for production managers and plant operators, available for download as an app. (Photo: Festo AG & Co. KG)
How will the digitalisation of mechanical engineering evolve?
Plattform Industrie 4.0 Plattform Industrie 4.0, the digitalisation initiative of the Federal Republic of Germany: Since 2018 Festo has – in the person of Chief Technology Officer Dr. Frank Melzer (right) – held the chair of the platform’s steering committee. (Photo: Festo AG & Co. KG)
Compact, versatile powerhouse
Festo Press Image VYKA The media separated solenoid valve VYKA from Festo allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates for continuous flow applications. (Photo: Festo AG & Co. KG
Ready-to-install solutions for the lab-on-a-chip
Festo Press Image Festo LifeTech Mobile analytical devices allow fast testing to identify pathogens in the case of colds or flu-like infections as well as other bacterial or viral diseases. (Photo: Festo AG & Co. KG)
Ready-to-install solutions for the lab-on-a-chip
Festo Press Image Valve assembly in vitro diagnostics In vitro diagnostics made easy with a ready-to-install valve block for controlling the cartridges in bench-top units. (Photo: Festo AG & Co. KG)
40,000 genetic tests per day
EGSC Synchron An electric slide EGSC moves the pipetting head down to add liquid to the microwell plates at several washing stations. (Photo: Festo AG & Co. KG)
40,000 genetic tests per day
EGC Synchron Electric axes EGC in combination with an electric slide EGSL position the pipetting head for DNA extraction. (Photo: Festo AG & Co. KG)
40,000 genetic tests per day
CPX-E Synchron CPX-E and valve terminals VTUG with IO-Link control the system. (Photo: Festo AG & Co. KG)
40,000 genetic tests per day
Niels Kruize “The collaboration with Festo provides us with tremendous added value”, Niels Kruize says, Business Development, Synchron Lab Automation (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image Head Office The corporate head office of Festo at Esslingen a.N., Germany. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image laboratory automation Festo develops intelligent, tested subsystems for the automation of liquid media and sample handling applications. The applications involve the use of both electric and pneumatic actuators with motors, controllers and handling systems, as well as grippers, sensors and camera systems. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image medical technology In medical technology, the focus is on the efficient open-loop and closed-loop control of medical gases. (Photo: Festo AG & Co. KG)
Precise switching
VAEM The valve control module VAEM from Festo makes precise switching of solenoid valves easier than ever. (Photo: Festo AG & Co. KG)
Precisely dispensed
Planar surface gantry for laboratory automation The best possible solution for system manufacturers: as well as its own components such as the planar surface gantry EXCM, Festo also integrates components from third-party manufacturers. (Photo: Festo AG & Co. KG)
Precisely dispensed
Pipetting into microplates The various process steps for adding different liquids to microplates are automated and linked in a very compact space. (Photo: Festo AG & Co. KG)
Precisely dispensed
VTOE Contactless dispensing of very small volumes: the 8-channel dispense head VTOE is a configurable complete solution comprising manifold duct plate, dosing valves and nozzles. (Photo: Festo AG & Co. KG)
Precisely dispensed
VYKA The media separated solenoid valve VYKA allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates. (Photo: Festo AG & Co. KG)
Precisely dispensed
VAEM The VAEM valve control module with holding current reduction is ideal for controlling dosing heads. (Photo: Festo AG & Co. KG)
No more oxidised wafers
Festo press photo N2 Purge When wafers need to be transported and stored in the semiconductor industry, the N2 purge system from Festo prevents oxygen from oxidising the wafers. (Photo: Festo AG & Co. KG)
Moving into the digitalised product world
Festo press photo Dr Michael Hoffmeister "We support our customers with digital solutions at every step of the value chain and thus also guide them along their individual digital customer journey," emphasises Dr Michael Hoffmeister, Executive Expert Digital Business at Festo. (Photo: Festo AG & Co. KG)
Moving into the digitalised product world
Festo press photo CPX-IoT gateway Secure connection to the Festo Cloud and exclusive access to individual digitalisation with the IoT gateway CPX-IoT. (Photo: Festo AG & Co. KG)
Moving into the digitalised product world
Festo press photo Smartenance Key Visual Smartenance makes time-consuming preventive system maintenance obsolete. (Photos: Festo AG & Co. KG)
Moving into the digitalised product world
Festo press photo Smartenance PC Tablet Phone Smartenance makes time-consuming preventive system maintenance obsolete. (Photos: Festo AG & Co. KG)
Moving into the digitalised product world
Festo press photo Dashboard CPX tablet With the IoT gateway CPX-IoT, it is possible to have preconfigured dashboards for each Festo component – with additional customisation. The dashboard is viewed in the web browser and includes diagrams and traffic lights. (Photo: Festo AG & Co. KG
Show 30 more results ...