Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Servo press kit YJKP - Updates
Servo press kit YJKP - Updates YJKP

Updates of the servo press kit YJKP:

- Firmware update of the motor controller CMMP-AS

- Firmware update of the controller CECC-X

- Software update of the application software GSAY

1.10
08/02/2017
VTEM Firmware Download Instructions for V4.12.0
VTEM Firmware Download Instructions for V4.12.0 VTEM

This document provides a step-by-step explanation of how to download the newest VTEM Firmware using Festo Field Device Tool. This Application Note describes a one-time migration which is required for all firmware versions older than 4.12.0. If firmware is already 4.12.0 or higher the migration step with bootloader-5.1.0 and misc-1.0.0 is not necessary.

1.40
23/07/2019
Malfunction codes VTEM
Malfunction codes VTEM Festo Motion Terminal (VTEM)

The following tables contain all the malfunction codes and sub-codes relevant to the application that can be stored in the diagnostic memory of the Festo Motion Terminal (VTEM).

1.50
02/12/2019
service2see: Update firmware (Ethernet)
service2see: Update firmware (Ethernet) FCT: Update firmware (Ethernet)

(Servicevideo)

service2see: Firmware aktuallisieren (USB)
service2see: Firmware aktuallisieren (USB)

(Servicevideo)

Motion Terminal Quick Reference PLC programming
Motion Terminal Quick Reference PLC programming VTEM

VTEM Motion Terminal Quick Reference PLC programming

1.30
19/05/2020
I-Port event/error list
I-Port event/error list CMMO-ST-...LKP; CTEU-...

A list of CMMO events and errors are transmitted via I-Port

1.10
17/01/2018
Quick help - Festo Dashboards
Quick help - Festo Dashboards GSAD

This application note explains in detail the function and handling of
Dashboards from Festo

1.30
04/05/2020
Commissioning of CPX-AP-I-EC-M12 in Codesys SP12 with CPX-AP-I-4IOL-M12
Commissioning of CPX-AP-I-EC-M12 in Codesys SP12 with CPX-AP-I-4IOL-M12 CPX-AP-I-EC-M12 and CPX-AP-I-4IOL-M12

This application note gives a step by step description of how to integrate a CPX-AP-I-EC-M12 into the Codesys SP12 program-ming environment and how to use the CPX-AP-I-4IOL-M12 master

1.20
19/05/2020
Supported drives VTEM
Supported drives VTEM Festo Motion Terminal (VTEM)

This list contains all Festo drives approved for the Festo Motion Terminal (VTEM) and the corresponding value that must be entered in the

"drive type" system parameter (ID 20) in order to be able to operate the respective drive with a Motion App.

1.50
19/05/2020
YJKP - Hardware Configuration and system settings
YJKP - Hardware Configuration and system settings YJKP

Configuration instructions for hardware and system settings of a YJKP system.

1.10
05/09/2019
Multi-Axis Interface CPX-CMXX Version: Rev 06
Multi-Axis Interface CPX-CMXX Version: Rev 06 Startup behaviour
1.10
02/03/2015
YJKP - Quick Start Guide EVO3
YJKP - Quick Start Guide EVO3 YJKP

Quick startup of the servo press kit YJKP:

- Scope of delivery

- Mechanical commissioning

- Electric commissioning

- Basic software steps

1.20
18/09/2019
YJKP - Homing system
YJKP - Homing system YJKP

Description how to home the drive via WebVisu and Host control

1.10
05/09/2019
Read YJKP logging data via FT
Read YJKP logging data via FT YJKP

Short step by step description to read out logging data from the YJKP via FTP

1.30
01/03/2018
Modbus on CMMP-AS- -M3/M0
Modbus on CMMP-AS- -M3/M0 CMMP-AS- - M3/M0

Connection and configuration of the motor controller CMMP-AS- -M3/M0 within a Modbus/TCP network.

1.20
23/05/2017
CMMT-AS Servo Drive Parametrization via CDSB-A1 Operator Unit
CMMT-AS Servo Drive Parametrization via CDSB-A1 Operator Unit CMMT-AS; CDSB-A1

This document describes how to export parameter sets from the Festo Automation Suite CMMT-AS Plug-in to a CDSB-A1 operating panel, download it to the drive and activate it.

1.10
17/09/2019
YJKP - Manual movement
YJKP - Manual movement YJKP

Description how to use manual functions

1.10
05/09/2019
YJKP - Operation screen in WebVisu
YJKP - Operation screen in WebVisu YJKP

Description of how to use the operation screen to start a press-ing program

1.10
05/09/2019
YJKP - System diagnosis
YJKP - System diagnosis YJKP

Description of the diagnosis elements

1.10
05/09/2019
YJKP - Adjustment force sensor
YJKP - Adjustment force sensor YJKP

Step by step description to adjust the force sensor of the YJKP

1.10
04/02/2019
CPX-AP-I with EtherNet/IP; Rockwell Systems and Others
CPX-AP-I with EtherNet/IP; Rockwell Systems and Others CPX-AP-I

How to best commission a CPX-AP-I system on EtherNet/IP. A focus will be on integration with Rockwell Logix systems, but much of the content is also applicable with any EtherNet/IP master.

1.10
05/05/2020
YJKP - application example using Web-Visu
YJKP - application example using Web-Visu YJKP

Complete application example of pressing a spring using YJKP system

- Configure sequencer

- Record a reference curve

- Configure monitoring

- Operate

1.10
05/09/2019
Servo Press Kit YJKP - Advanced Force Mode
Servo Press Kit YJKP - Advanced Force Mode YJKP

This Application Note describes the properties, operation and parameterization of the advanced force mode of the servo press kit YJKP.

1.10
05/02/2019
Servo Press Kit YJKP - Integration of host function blocks in Allen Bradley (Studio 5000 Logix Designer V26.01)
Servo Press Kit YJKP - Integration of host function blocks in Allen Bradley (Studio 5000 Logix Designer V26.01) YJKP; Allen Bradley

This application note describes how you integrate the host func-tion blocks of the servo press kit YJKP in Allen Bradley (Studio 5000 Logix Designer V26.01).

Supported systems:

- Tested with CompactLogix (1769-L24ER-QB1B)

- All compatible devices

1.10
17/11/2017
Servo press kit YJKP - Commissioning Anybus X-gateway Modbus PROFINET
Servo press kit YJKP - Commissioning Anybus X-gateway Modbus PROFINET YJKP

Commissioning of the Anybus X-gateway Modbus-TCP PROFINET in connection with the servo press kit YJKP:

- Electrical commissioning

- Mechanical commissioning

- Software commissioning

1.20
14/02/2017
Servo press kit YJKP - Parse logging data
Servo press kit YJKP - Parse logging data YJKP

Parse logging data of the servo press kit YJKP

1.10
08/02/2017
Servo press kit YJKP - force control function
Servo press kit YJKP - force control function YJKP

This Application Note describes characteristics, mode of operation, parameters configuration and application examples of the force control function of the servo press kit YJKP.

1.10
05/02/2019
VTOE-8... in combination with VAEM-VS8...
VTOE-8... in combination with VAEM-VS8... VTOE-8...; VAEM-V-S8...

 

How VTOE-8... is used in combination with VAEM-V-S8....

1.10
09/03/2020
YJKP - Evaluation methods based on a reference curve
YJKP - Evaluation methods based on a reference curve YJKP

Description of how to record/load reference curves and how to configure evaluation methods.

1.10
05/09/2019
Show 30 more results ...
Subscribe to RSS