Festo Media Service

Please select a category on the left or use the search.

Caption Download
The automated chameleon tongue
Adaptive Shape Gripper 1 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 2 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Stefanie Seiler and Nenja Rieskamp These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development) (Photo: Festo AG & Co. KG)
A Swedish recipe that really hits the spot
Volvo press image Welding process Faster and more reliable: Volvo is constantly improving its welding processes. (Photo: Volvo)
A Swedish recipe that really hits the spot
Festo press image Tip Dresser Tip dresser for articulated-arm robots: On the right the two holes for electrode milling, and on the left the compact housing with the vision system which provides the data for repositioning the electrodes. (Photo: Festo)
A Swedish recipe that really hits the spot
Festo press image static welding equipment For static welding gun systems: A fast and precise pivot arm brings the electrode milling device, the so-called tip dresser, to the electrodes after 150 spot welds have been completed. (Photo: Festo)
A Swedish recipe that really hits the spot
Festo press image Leif Winberg/Volvo and Leif Lindahl/Festo At the camera-controlled electrode milling device: Leif Winberg, Plant Engineer for Resistance Welding at Volvo in Olofström (left) and Leif Lindahl, Business Development Manager Automotive with Festo Sweden. (Photo: Festo)
A Swedish recipe that really hits the spot
Festo press image Robots Time savings: The new tip dressers significantly reduce cycle times where multiple welding robots are in use. (Photo: Festo)
A Swedish recipe that really hits the spot
Volvo press image body parts volvo Properly welded: Volvo body parts (Photo: Volvo)
Astonishing space efficiency
ELGC Ideal ratio of installation to working space: the spindle axis ELGC-BS combined with the servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
EGSC Impresses with compact dimensions: mini-slide EGSC with servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
handling ELGC + EGSC Verblüffende Raumeffizienz: ELGC und EGSC kombiniert in einem Handling-System in adapterfreier „One-size-down“-Montage (eine Größe kleiner möglich) (Foto: Festo AG & Co. KG)
First turnkey IoT solution
CPX-IoT-Gateway Secure connection to the Festo Cloud and exclusive access to individual digitalisation: the IoT gateway CPX-IoT. (Photo: Festo AG & Co. KG)
First turnkey IoT solution
Portrait Michael Hoffmeister “Festo is working closely with other companies in the German Electrical and Electronic Manufacturers’ Association and on the Platform Industry 4.0 project to create a common reference architecture,” explains Dr Michael Hoffmeister, Management Expert at Festo in the newly founded Digital Business section. (Photos: Festo AG & Co. KG)
First turnkey IoT solution
YXMx Kinematics with controller, software packages for motion tasks and condition monitoring, and an app for cloud-based visualisation: the modular positioning platform YXMx from Festo. (Photos: Festo AG & Co. KG)
Format change at the push of a button
Multi-Carrier-System® 3 Multi-Carrier-System®: the flexible modular transport system can be adapted to different formats via software at the push of a button. (Photo: Festo AG & Co. KG)
Format change at the push of a button
Recirculating conveyor system Multi-Carrier-System®: the flexible modular transport system can be adapted to different formats via software at the push of a button. (Photo: Festo AG & Co. KG)
Format change at the push of a button
Motion Terminal VTEM 3 With the Festo Motion Terminal, pneumatic functions can be controlled via apps for the first time, without having to change or modify the hardware. (Photos: Festo AG & Co. KG)
Format change at the push of a button
Motion Terminal VTEM 2 With the Festo Motion Terminal, pneumatic functions can be controlled via apps for the first time, without having to change or modify the hardware. (Photos: Festo AG & Co. KG)
Format change at the push of a button
Complete system VTEM and MCS Format change at the push of a button: two Festo innovations enable fast and straightforward format changes on just one machine – the Festo Motion Terminal VTEM and the Multi-Carrier-System® MCS. (Photo: Festo AG & Co. KG)
Format change at the push of a button
Gripper system High flexibility: Different box sizes and the matching number of products are set directly in the Multi-Carrier-System® MCS using the freely positionable carriers. The products can be individually transported, grouped and synchronously packaged on the carriers. (Photo: Festo AG & Co. KG)
Revolution in automation
Revolution in automation
Revolution in automation
Precision robot welding force
Servopneumatische Schweißzange Developed by Festo in close cooperation with experts from the automotive industry: the hardware concept of the servo-pneumatic welding gun. (Photo: Festo AG & Co. KG)
Precision robot welding force
Servo-pneumatic welding gun controller Keeps pace with Industry 4.0: the fully digitised, servo-pneumatic welding gun controller from Festo. (Photo: Festo AG & Co. KG)
Learning from Nature: Festo’s Bionic Learning Network
BionicANTs The artificial ants demonstrate how self-organising individual components can communicate with each other and solve complex tasks as a networked overall system. (Photos: Festo AG & Co. KG)
Learning from Nature: Festo’s Bionic Learning Network
BionicANTs The artificial ants demonstrate how self-organising individual components can communicate with each other and solve complex tasks as a networked overall system. (Photos: Festo AG & Co. KG)
Learning from Nature: Festo’s Bionic Learning Network
eMotionButterflies To prevent the ultra-lightweight eMotionButterflies from colliding, they are coordinated by an indoor GPS. (Photos: Festo AG & Co. KG)
Learning from Nature: Festo’s Bionic Learning Network
eMotionButterflies To prevent the ultra-lightweight eMotionButterflies from colliding, they are coordinated by an indoor GPS. (Photos: Festo AG & Co. KG)
Learning from Nature: Festo’s Bionic Learning Network
FlexShapeGripper The FlexShapeGripper can grasp, pick up and put down several very differently shaped objects in the one process. (Photos: Festo AG & Co. KG)
Learning from Nature: Festo’s Bionic Learning Network
FlexShapeGripper The FlexShapeGripper can grasp, pick up and put down several very differently shaped objects in the one process. (Photos: Festo AG & Co. KG)
Show 30 more results ...