4/18/2018

Festo Showcases Its New Solution for Variable Control of Flow Rate or Fill Level at Powder & Bulk Solids 2018

Festo Showcases Its New Solution for Variable Control of Flow Rate or Fill Level at Powder & Bulk Solids 2018

The Festo exhibit also features components for automating dispensing and conveying in clean or harsh environments.
Festo introduces at the International Powder & Bulk Solids Exhibition its new control solution.

Festo introduces at the International Powder & Bulk Solids Conference and Exhibition, Donald E. Stephens Convention Center, Rosemont, Illinois, April 24-26, its new control solution for infinitely variable flow rate and fill level based on the DFPI linear pneumatic actuator. The company also showcases its range of process valve solutions for clean or harsh environments where powders and bulk solids are dispensed from hoppers and conveyed to downstream processes. (Festo Booth # 2939)

 

The Festo DFPI linear pneumatic actuator with integrated displacement encoder controls flaps, guide plates, and louver dampers in flow-rate applications. This DFPI is also applied to variable fill-level systems. A demonstration at the Festo booth reveals the new control system’s failsafe functionality where, in the event of power or pressure failure, operations personnel manually advance the drive unit to a freely selectable safety position. This pneumatic solution offers simple maintenance and higher forces than an electrical actuator.  Shipped fully assembled and tested these linear drives are equipped with positioners and valves. Festo also supplies ready-to-install customized control cabinets that reduce engineering and assembly overhead for OEMs and end users.

 

Additional products featured at the Festo booth include:

 

  • A hazardous environment air preparation system with safety valve
  • VOFC and VOFD solenoid valves for hazardous and safety applications.
  • A clean design with high corrosion and acid resistant CRDSNU pneumatic actuator
  • Self-adjusting pneumatic cylinders for faster installation and more reliable operation

 

As a single source powders and bulk-solids automation supplier, Festo offers plug and play components, including a modular control platform; HMI; valve terminals; valve assemblies for butterfly, pinch, and ball valves; electric and pneumatic linear and rotational actuators; integrated motors/drives; sensors; and I/O. 

 

Booth personnel will inform attendees about the new Stars of Automation program that guarantees shipment of core products within 24 hours. Global guaranteed fast shipment means fewer replacement components must be carried in inventory, which lowers overhead. Stars of Automation simplifies and speeds up ordering for OEMs and end users and, in effect, reducing time to market for new automated systems.

 

 “Show attendees who know Festo as a pneumatics company will be excited to see that we offer a total process automation solution – everything from an integrated control platform for both pneumatics and electrics down to I/O,” said Craig Correia, Director, Process Industries, North America, for Festo. For more information on powders and bulk solids solutions call call Festo at 800-993-3786 and visit the Festo website www.festo.us. Be sure to stop by the Festo Booth #2939.

 

###

 

About Festo

Festo is a leading manufacturer of pneumatic and electromechanical systems, components, and controls for process and industrial automation. For more than 40 years, Festo Corporation has continuously elevated the state of manufacturing with innovations and optimized motion control solutions that deliver higher performing, more profitable automated manufacturing and processing equipment.

Connect with Festo: Facebook, LinkedIn, Twitter and YouTube

 

Contact:

Michelle Werner

+1(631)404-3176


Festo Media Service