Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Electric drives
When it comes to simplicity and costs, pneumatics is unmatched by any other form of technology. It can be used worldwide without any problems and without the need for extensive specialist know-how. If the requirements for speed, acceleration and ...
Safety Sub-Functions Electric Drives SSB with SS1-t, STO, Category 4, up to PL e and SB, Category 1, up to PL c
Safety Sub-Functions Electric Drives SSB with SS1-t, STO, Category 4, up to PL e and SB, Category 1, up to PL c CMMT-AS-…-S1

Application Note for the realization of the safety sub-function safe stopping and blocking (SSB) with the safety sub functions safe stop 1 (SS1) and safe blocking (SB). For the safety sub-function SS1 category 4, up to PL e can bereached; for safety sub-function SB category 1, PL c can be reached. This Application Note contains possible circuits for the servo drive CMMT-AS-…-S1 with holding brake in the servo motor or with an external clamping unit.

1.10
9/19/2019
Main page
Welcome to the German language Knowledgebase Wiki from Festo. In this Wiki you can find many articles on basic technical principles as well as answers to questions about our product portfolio. These range from pneumatics via electrical drive ...
Electric rotary/lifting module EHMB
Rotary modules can be used for several purposes. They can align or change the orientation of a part; they can also be used to create a compact complete handing unit. The basis for this is a rotary module with a stable bearing, which turns the ...
Electric short-stroke cylinder ADNE-LAS
Many systems require short but dynamic movements between two end positions. For example on a testing machine where components tested as "bad" have to be removed from the continuous manufacturing process. That is why Festo has integrated a linear ...
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-AS-…-S1 and CMMT-ST-…-S0, Cross Wiring of Servo Drives
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-AS-…-S1 and CMMT-ST-…-S0, Cross Wiring of Servo Drives CMMT-AS-…-S1; CMMT-ST-…-S0

Application Note for the cross wiring of several servo drives and the realization of the safety sub-functions safe stop 1 (SS1) and safe torque off (STO). Depending on the safe outputs, wiring and fault exclusions is category 3, up to PL d or category 4, up to PL e possible. This Application Note contains possible circuits for the servo drives CMMT-AS-...-S1 and CMMT-ST-…-S0.

1.10
9/17/2019
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-ST-…-S0, Cross Wiring of Servo Drives
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-ST-…-S0, Cross Wiring of Servo Drives CMMT-ST-…-S0

Application Note for the cross wiring of several servo drives and the realization of the safety sub-functions safe stop 1 (SS1) and safe torque off (STO). Depending on the safe outputs, wiring and fault exclusions is category 3, up to PL d or category 4, up to PL e possible. This Application Note contains possible circuits for the servo drive CMMT-ST-…-S0.

1.10
9/17/2019
Safety in pneumatics
At Festo, quality has many aspects – one of these is handling machines safely. This is the reason for our safety-oriented automation technology. These components ensure that optimum safety is achieved in the workplace. Festo has offered products ...
Certification
Certification as a passport for the global market - international certification and the meaning of logos on rating plates. Those who develop popular products must address the topic of international certification. More than 30,000 standards ...
EMC Construction advice
EMC Construction advice EMC

General use of EC directives

1.10
11/22/2016
Proportional Valve Technology
Proportional Valve Technology MPYE,VPWP, VPCF,VPPX,VPPM,MPPES,VPPE,VPPL,MPPE,VEAA,VEAB

This file offers detailed technical information about the

proportional valves.

1.10
6/5/2018
Holding and break-away forces on suction cups
How are the holding force and break-away force calculated? In order to determine the required holding force, you need the calculated mass, the system acceleration and the friction coefficient. The holding force required depends on the load ...
EMC - Checklist
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
8/8/2017
Photovoltaics for beginners
Photovoltaics and solar thermal energy. These are catchwords which we read almost daily in the newspapers. Festo supports the manufacturing processes which are part of these technologies in a number of different ways. But what are the actual ...
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-ST-…-S0
Safety Sub-Functions SS1-t, STO Servo Drive CMMT-ST-…-S0 With Stepper Motors: SS1-t, STO, Category 3, up to PL e. With EC Motors: STO, Category 3, up to PL d

Application Note for the realization of the safety sub-functions safe stop 1 (SS1) and safe torque off (STO) with category 3 and up to PL e. This Application Note contains possible circuits for the servo drive CMMT-AS-…-S1.

1.0
7/8/2019
Safety Sub-Function STO Servo Drive CMMT-ST-…-S0
Safety Sub-Function STO Servo Drive CMMT-ST-…-S0 With Stepper Motors: STO, Category 3, up to PL e. With EC Motors: STO, Category 3, up to PL d

Application Note for the realization of the safety sub-function safe torque off (STO) with category 3 and up to PL e for stepper motors or category 3 and up to PL d for EC motors. This Application Note contains possible circuits for the servo drive CMMT-ST-…-S0.

1.0
7/8/2019
Valves
Pneumatics without valves is like driving cars without motors - possible in theory, but unimaginable in practice.The function of valves is generally limited to controlling the flow direction or the quantity of air. Valves can be subdivided into ...
Linear motors
Today, linear motor technology is considered the most innovative drive technology for handling and automation systems. But how old is this technology? The first patent for a linear motor was registered in 1885 by Dr. Th. Burger in Berlin. The ...
Electric linear motor cylinders DNCE-LAS and DFME-LAS
Festo is the specialist for pneumatics. Therefore it is only logical that Festo has launched linear motor cylinders to the market with the same design as the pneumatic cylinders. However, one restriction must be made clear from the start: no ...
Safety Sub-Functions SS1-t: STO, Cat. 4, up to PL e Servo Drive CMMT-AS-…-S1
Safety Sub-Functions SS1-t: STO, Cat. 4, up to PL e Servo Drive CMMT-AS-…-S1 CMMT-AS-…-S1

Safety Sub-Functions SS1-t: STO, Cat. 4, up to PL e

Servo Drive CMMT-AS-…-S1

1.10
6/26/2019
Safety Sub-Functions STO, Cat. 4, up to PL e Servo Drive CMMT-AS-…-S1
Safety Sub-Functions STO, Cat. 4, up to PL e Servo Drive CMMT-AS-…-S1 CMMT-AS-...S1

Safety Sub-Functions STO, Cat. 4, up to PL e Servo Drive CMMT-AS-…-S1

1.10
2/26/2019
Safety sub-functions: SS1-t, STO category 3, up to PL d or category 4, up to PL e - Crosswiring
Safety sub-functions: SS1-t, STO category 3, up to PL d or category 4, up to PL e - Crosswiring CMMT-AS-…-S1

Application Note for the cross wiring of several servo drives and the realization of the safety sub-functions safe stop 1 (SS1) and safe torque off (STO). Depending on the safe outputs, wiring and fault exclusions is category 3, up to PL d or category 4, up to PL e possible. This Application Note contains possible circuits for the servo drive CMMT-AS-…-S1.

1.10
9/17/2019
Safety Sub-Functions Pneumatic
Safety Sub-Functions Pneumatic STO, PUS, SLS, Category 1, up to PL c

Application Note for the realization of the safety sub-functions safe torque off (STO), prevention of an unexpected start-up (PUS) and safely-limited speed (SLS) with category 1 and up to PL c. This Application Note contains possible circuits for permanent oder switchable safely-limited speed (SLS).

1.0
5/14/2019
Safety Sub-Functions Pneumatic
Safety Sub-Functions Pneumatic PUS, Category 1, up to PL c

 

Application Note for the realization of the safety sub-function prevention of an unexpected start-up (PUS) with category 1 and up to PL c. This Application Note contains possible circuits for 5/2 directional control valves.

1.4
5/14/2019
Safety Sub-Functions Pneumatic
Safety Sub-Functions Pneumatic STO, PUS, SLT, Category 1, up to PL c

Application Note for the realization of the safety sub-functions safe torque off (STO), prevention of an unexpected start-up (PUS) and safely-limited torque (SLT) with category 1 and up to PL c. This Application Note contains possible circuits for permanent oder switchable safely-limited torque (SLT).

1.0
5/14/2019
Safety Sub-Functions Pneumatic SET, PUS, Category 1, up to PL c
Safety Sub-Functions Pneumatic SET, PUS, Category 1, up to PL c Pneumatic SET, PUS, Category 1, up to PL c

Application Note for the realization of the safety sub-functions safe equilibrium of torque (SET) and prevention of an unexpected start-up (PUS) with category 1 and up to PL c. This Application Note contains a possible circuit for 5/3 directional control valves and pressure regulators.

1.10
9/19/2019
Malfunction codes VTEM
Malfunction codes VTEM Festo Motion Terminal (VTEM)

The following tables contain all the malfunction codes and sub-codes relevant to the application that can be stored in the diagnostic memory of the Festo Motion Terminal (VTEM).

1.30
5/16/2019
Configuration of CMMT-AS-EC(PN) to run 3rd party motor
Configuration of CMMT-AS-EC(PN) to run 3rd party motor CMMT-AS-...EC

This document describes how to configure and run 3rd party motors in combination with CMMT-AS-..-EC (PN) drive.

1.20
1/23/2019
Safety Sub-Functions Pneumatic
Safety Sub-Functions Pneumatic SSC, PUS, Category 1, up to PL c

 

Application Note for the realization of the safety sub-functions safe stopping and closing (SSC) and prevention of an unexpected start-up (PUS) with category 1 and up to PL c. This Application Note contains possible circuits for 5/3, 3/2 and 2/2 directional control valves and delockable check valves.

1.1
5/14/2019
Safety Sub-Functions Pneumatic SB, PUS, Category 1, up to PL c
Safety Sub-Functions Pneumatic SB, PUS, Category 1, up to PL c Pneumatic SB, PUS, Category 1, up to PL c

Application Note for the realization of the safety sub-functions safe blocking (SB) and prevention of an unexpected start-up (PUS) with category 1 and up to PL c. This Application Note contains possible circuits together with the safety sub-functions safe torque off (STO) and safe equilibrium of torque (SET).

1.10
9/19/2019
Show 17 more results ...
Subscribe to RSS
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.