|
Version 2.8.0.22
New Features:
- Available updates of installed IODD's are displayed in the navigation list.
Fixed Bugs:
Known Limitations:
- IODDs with schema 1.0 are not supported
----
IO-Link Plug-in V1.1.1.1
New Features:
- Easy configuration and trace recording from data of IO-Link devices, e.g. monitoring of connected devices, in context Diagnosis
- Extended Trace display page for analyzing recorded traces with convenient features like, Zoom in/out, hide and show channels, combing axes etc
- Start and Stop trace recordings easily via it's own button in the ribbon bar
- Generic In- and output of Index and Subindex for e.g. process data of IO-Link device through an integrated command line view
- Desired IODD-version can be selected very comfortable on the plug-in page IO-Link (in case of several IODD-files)
Fixed Bugs:
- Parameter values that are transferred to the device are reset to the initial value after a few seconds.
- Live values of the device are updated very slow in online mode
- Process data from IO-Link devices cannot be written via CPX-AP-A IO-Link master
|
IO-Link_2.8.0.22.fsx
Deutsch [de], English [en]
File size: 25 MB
Version: 2.8.0.22 (6/7/2024)
|
|
Version 2.7.0.52
IO-Link Extension V2.7.0.52
New Features:
- Searching for IODDs via part number of the device (in addition to device and vendor name)
- Display of device and vendor IDs in the "Details" section of an IODD
- IODD details can be copied to the clipboard
Fixed Bugs:
- IO-Link device is not shown in the device catalog after importing its IODD via the right sidebar of topology editor
Known Limitations:
- IODDs with schema 1.0 are not supported
----
IO-Link Plug-in V1.1.1.1
New Features:
- Easy configuration and trace recording from data of IO-Link devices, e.g. monitoring of connected devices, in context Diagnosis
- Extended Trace display page for analyzing recorded traces with convenient features like, Zoom in/out, hide and show channels, combing axes etc
- Start and Stop trace recordings easily via it's own button in the ribbon bar
- Generic In- and output of Index and Subindex for e.g. process data of IO-Link device through an integrated command line view
- Desired IODD-version can be selected very comfortable on the plug-in page IO-Link (in case of several IODD-files)
Fixed Bugs:
- Parameter values that are transferred to the device are reset to the initial value after a few seconds.
- Live values of the device are updated very slow in online mode
- Process data from IO-Link devices cannot be written via CPX-AP-A IO-Link master
|
IO-Link_2.7.0.52.fsx
File size: 25 MB
Version: 2.7.0.52 (2/16/2024)
|
|
Version 2.6.0.29
IO-Link Extension V2.6.0.29
New Features:
Known Limitations:
- Importing of an IO-Link device from the device scan section is only possible if a suitable IODD has been installed.
----
IO-Link Plug-in V1.0.0.219
New Features:
- Parameterization and configuration of all IO-Link Devices with revision V1.1
- Dynamically displaying of parameter pages and its content depending on the loaded IODD device description
- Read and write of process data possible when the plug-in is connected to the device
- Incoming device events and diagnosis messages are shown in the Plug-in context "Diagnosis"
- Device actions like e.g. Reset to factory or acknowledge error can be executed on a designed page "Device Control"
- Additional parameter information (Index/Subindex), a short description and the default value is available in pop up of each parameter (gray square)
- All device parameters are shown in a generic parameter list and can be filtered.
- Helpful explanation regarding the plug connection and wiring are shown on page "Connection"
- Imported IODD device descriptions are stored in the project file and can be loaded on other systems
- Special device information and e.g. manuals are easily and conveniently accessible via the right sidebar (only for Festo devices)
Known Limitations:
- IO-Link Devices with Revision V1.0 are not supported yet.
|
IO-Link_2.6.0.29.fsx
Deutsch [de], English [en]
File size: 11 MB
Version: 2.6.0.29 (5/30/2023)
|