|
BionicSoftHand 1
The BionicSoftHand should rotate a 12-sided “cube” so that a previously defined side points upwards at the end.
|
Image_big (.tif,3 MB)Image_small (.jpg,290 KB)Press release
|
|
BionicSoftHand 2
The BionicSoftHand is operated pneumatically for the safe and direct interaction with people.
|
Image_big (.tif,5 MB)Image_small (.jpg,499 KB)Press release
|
|
BionicSoftArm 1
The pneumatic lightweight robot BionicSoftArm is flexible from the start and is suitable for direct human-robot collaboration.
|
Image_big (.tif,4 MB)Image_small (.jpg,447 KB)Press release
|
|
BionicSoftArm_SCARA
The BionicSoftArm as a classic SCARA application with a pick-and-place task: it can work in the tightest of spaces around obstacles.
|
Image_big (.tif,3 MB)Image_small (.jpg,265 KB)Press release
|
|
Festo Press Image BionicOpter.jpg
The highly integrated system can be operated easily and intuitively via a smartphone.
|
Image_big (.tif,6 MB)Image_small (.jpg,288 KB)Press release
|
|
Festo Press Image BionicOpter2.jpg
The BionicOpter is an ultralight flying object.
|
Image_big (.tif,2 MB)Image_small (.jpg,167 KB)Press release
|
|
Festo Press Image BionicOpter_WorldGuinnessRecords.jpg
Since September 5th the BionicOpter can be observed in the Guinness World Records 2020.
|
Image_big (.tif,11 MB)Image_small (.jpg,1 MB)Press release
|
|
BionicWorkplace 1
Exciting concept study from Festo: in the BionicWorkplace, a person works with a robot arm as well as numerous assistance systems that are networked with each other.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,4 MB)Image_small (.jpg,362 KB)Press release
|
|
BionicWorkplace 2
The future in sight: a worker can intuitively control the BionicCobot using movement, touch or speech.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,5 MB)Image_small (.jpg,292 KB)Press release
|
|
BionicWorkplace 3
The future belongs to sensor technology. Sensors and camera systems record the positions of the worker, components and tools. (Photo: Festo AG & Co. KG)
|
Image_big (.tif,6 MB)Image_small (.jpg,357 KB)Press release
|
|
Festo Press Image BionicSoftHand_1
The BionicSoftHand should rotate a 12-sided cube so that a previously defined side points upwards at the end.
|
Image_big (.tif,3 MB)Image_small (.jpg,290 KB)Press release
|
|
Festo Press Image BionicSoftHand_2
The BionicSoftHand is operated pneumatically for the safe and direct interaction with people.
|
Image_big (.tif,5 MB)Image_small (.jpg,499 KB)Press release
|
|
Festo Press Image BionicSoftArm_1
The pneumatic lightweight robot BionicSoftArm is flexible from the start and is suitable for direct human-robot collaboration.
|
Image_big (.tif,4 MB)Image_small (.jpg,447 KB)Press release
|
|
Festo Press Image BionicSoftArm_2
The BionicSoftArm as a classic SCARA application with a pick-and-place task: it can work in the tightest of spaces around obstacles.
|
Image_big (.tif,3 MB)Image_small (.jpg,265 KB)Press release
|
|
Festo Press Image BionicFinWave_1
The fins of the BionicFinWave are cast out of silicone and do not require struts or support elements.
|
Image_big (.tif,3 MB)Image_small (.jpg,317 KB)Press release
|
|
Festo Press Image BionicFinWave_2, BionicFinWave_3
The underwater robot manoeuvres itself independently through a pipe system made of acrylic glass.
|
Image_big (.tif,5 MB)Image_small (.jpg,632 KB)Press release
|
|
Festo Press Image BionicFinWave_2, BionicFinWave_3
The underwater robot manoeuvres itself independently through a pipe system made of acrylic glass.
|
Image_big (.tif,7 MB)Image_small (.jpg,816 KB)Press release
|
|
Adaptive Shape Gripper 1
The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,5 MB)Image_small (.jpg,1 MB)Press release
|
|
Adaptive Shape Gripper 2
The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,6 MB)Image_small (.jpg,3 MB)Press release
|
|
Stefanie Seiler and Nenja Rieskamp
These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development)
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,7 MB)Image_small (.jpg,2 MB)Press release
|
|
Festo Press Image AquaJellies
Autonomous behaviour thanks to integrated communication
and sensor technology.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,8 MB)Image_small (.jpg,444 KB)Press release
|
|
Festo Press Image BionicWheelBot
Mechatronic overall system: intricate kinematics based on a natural model.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,3 MB)Image_small (.jpg,172 KB)Press release
|
|
Festo Press Image BionicWheelBot
The BionicWheelBot in rolling mode with extended propelling legs.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,3 MB)Image_small (.jpg,159 KB)Press release
|
|
Festo Press Image BionicFlyingFox
Despite its wingspan of 228 cm and its overall length of 87 cm, the BionicFlyingFox weighs 580 grams.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,3 MB)Image_small (.jpg,124 KB)Press release
|
|
Festo Press Image BionicFlyingFox
The wing kinematics of the BionicFlyingFox are also divided into primaries and secondaries.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,2 MB)Image_small (.jpg,124 KB)Press release
|
|
CMMT_EMMT
Servo drive system with controller CMMT-AS and motor EMMT-AS.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,29 MB)Image_small (.jpg,86 KB)Press release
|
|
CPX-IoT-Gateway
Secure access to the Festo cloud and exclusive access to individual digitalisation: the IoT gateway CPX-IoT.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,2 MB)Image_small (.jpg,72 KB)Press release
|
|
BionicWorkplace
In the BionicWorkplace, humans work together with a robot arm and numerous assistance systems that are networked with each other.
(Photo: Festo AG & Co. KG)
|
Image_big (.tif,6 MB)Image_small (.jpg,362 KB)Press release
|
|
CP Factory
Qualification for industry 4.0: With the CP Factory, Festo Didactic offers a cyber-physical learning and research platform. The platform represents the stations of a real production plant as a model. (Photo: Festo Didactic SE)
|
Image_big (.tif,43 MB)Image_small (.jpg,983 KB)Press release
|
|
Festo Press Image Award ceremony Worlddidac Award 2018
The award ceremony took place on 07 November 2018 as part of Worlddidac / Swissdidac Bern (Image source: Worlddidac)
|
Image_big (.jpg,8 MB)Image_small (.jpg,8 MB)Press release
|
|
Festo Press Image Bionics4Education_1
Bionics4Education: Holistic educational concept consisting of educational kits and digital learning environment (Image source: Festo)
|
Image_big (.tif,23 MB)Image_small (.jpg,1 MB)Press release
|
|
Festo Press Image Bionics4Education_2
Three robot models can be implemented with one modular system - ideal for interdisciplinary STEM instruction (Image source: Festo)
|
Image_big (.tif,15 MB)Image_small (.jpg,1011 KB)Press release
|