How to setup „Travel to fixed stop“ with CMMT-AS-PN by using the SINA_POS / telegram 111
Titulo:
How to setup „Travel to fixed stop“ with CMMT-AS-PN by using the SINA_POS / telegram 111
Subtítulo:
CMMT-AS-...PN
Descripción:

This document describes how to set up the CMMT-AS-...-PN in "trav-el to fixed stop" mode by using the SINA_POS function block / telegram 111 in programming environment of TIA Portal

Tipo de documento:
Application Note How to setup „Travel to fixed stop“ with CMMT-AS-PN by using the SINA_POS / telegram 111
Titulo Versión

Application Note - How to setup „Travel to fixed stop" with CMMT-AS-PN by using the SINA_POS / telegram 111

 

This document describes how to set up the CMMT-AS-...-PN in "trav-el to fixed stop" mode by using the SINA_POS function block / telegram 111 in programming environment of TIA Portal