Portal de Soporte técnico

Seleccione a la izquierda una categoría o utilice la Búsqueda.

Buscar

Numero de parte

Serie

Código de orden

Descripción
¡Aplicamos presión!
¡Aplicamos presión! Intensificación económica y específica de la presión

Nuestra experiencia al servicio del cliente

  • Protección de elementos de control frente a posibles oscilaciones de la presión
  • Aplicación de más presión en los elementos de accionamiento
  • Control sin conexiones eléctricas
Produktionswelten_en_HD_720p
SupraMotion-2-0_en_HD720p
DualWingGenerator_en_HD720p
BionicKangaroo_en_HD720p
SupraMotion_en_HD720p
SupraMotion20_SupraShuttle_en_HD1080i
SupraMotion20_SupraHandling20_en_HD1080i
SupraMotion20_SupraChanger_en_HD1080i
SupraMotion20_Demonstrator_en_HD1080i
OptoFluidic Film
Additive Manufacturing Manufacturing based on the building brick principle

Additive Manufacturing has been applied for many years in industry for the manufacture of prototypes or components in small batches.

BionicOpter - Animation

Animations of the functiones

Bionics / Future Concepts Projects 2013
Bionics / Future Concepts Projects 2013 Presentation

Bionics / Future Concepts Projects 2013

SupraMotion Potential for resource-efficient industrial automation

Resistance-free with superconductivity

Superconductors are metals, metal compounds or ceramic

materials that have a very special characteristic: their electrical

resistance suddenly drops to zero when cooled to below a

certain temperature. Once this transition temperature has been

reached, mutually repulsing electrons bind to form what are

called Cooper pairs.

This cancels out the mechanism of electrical resistance. When a

voltage is applied, the pairs conduct the electrical current without

any resistance and without losses. Once the electrical current

is put into motion, it flows uninterrupted in a closed circuit. The

magnetic fields that are generated in this way deliver a very high

energy yield.

LearningGripper Gripping and positioning through independent learning

The LearningGripper from Festo looks like an abstract form of

the human hand. The four fingers of the gripper are driven by

12 pneumatic bellows actuators with low-level pressurisation.

Thanks to the process of machine learning, it is able to teach itself

to carry out complex actions such as, for example, gripping and

positioning an object.

WaveHandling Modular conveyor with intelligent subsystems

The WaveHandling system from Festo is a pneumatic conveyor for

the targeted transportation and simultaneous sorting of objects.

It consists of numerous bellows modules that deform the surface,

creating a wave motion that transports the objects in a targeted

manner.

BionicOpter Lightweight design with intelligent kinematics

The mechanics of dragonfly flight are unique: dragonflies can man

 

oeuvre in all directions, glide without having to beat their wings

and hover in the air. Their ability to move their two pairs of wings

independently enables them to slow down and turn abruptly, to

 

 

accelerate swiftly and even to fly backwards.

ExoHand
ExoHand Animation

ExoHand

ExoHand
ExoHand Video film

ExoHand

PowerGripper
PowerGripper Animation

PowerGripper

SmartInversion
SmartInversion Animation

SmartInversion

Sound Machines 2.0
Sound Machines 2.0 Video film

Sound Machines 2.0

SmartInversion
SmartInversion Video film

SmartInversion

PowerGripper
PowerGripper Video film

PowerGripper

CogniGame
CogniGame Video film

CogniGame

Bionic Handling Assistant 3.0
Bionic Handling Assistant 3.0 Video film

Bionic Handling Assistant 3.0

Electric Dragon
Electric Dragon Video film

Electric Dragon

Bionic Learning Network 2009
Bionic Tripod 3.0 Film
18 mostrar otros resultados ...
Suscripción al RSS