Portal de Soporte técnico

Seleccione a la izquierda una categoría o utilice la Búsqueda.

Buscar

Numero de parte

Serie

Código de orden

Actualidad

Festo Automation Suite - Plug-in 14/6/2019 Plug-in for the configuration and parametrisation of the servo drive CMMT-AS

New Features:

  • Updated online help (V1.1.1)
  • Support for CMMT-AS with PROFINET interface
  • Performance improvements (loading, drive configuration page, connecting to a device, parameter synchronization)
  • Online access to user documentation for configured drive components
  • Completely revised trace functionality (better usability, more functions)
  • Improved trace configuration
  • Graphical display of the last autotuning result (requires firmware V15 or higher)
  • Operating mode can be displayed in monitored values
  • Warning in case of implausible software limits
  • Warning when disconnecting from the device if parameters have not been stored permanently
  • Calculated inertia ratio is displayed at the closed loop parameters
  • Improved handling of closed loop parameter sets
  • Improved indication of new trace recording, required restart and required reinitialization
  • Improved toolbar behaviour when reducing the window size
  • Double-clicking in a pop-up directly applies the selected list entry


Fixed Bugs:

  • User defined gear is deleted under certain circumstances (V1.1.1)
  • Version of SoftMotion driver is not displayed correctly (V1.1.1)
  • PROFINET MAC and IP address is not formatted correctly (V1.1.1)
  • Diagnosis page "I/O state" is updated sluggishly
  • User defined settings for auto tuning are not applied
  • Overall gear ratio is not calculated correctly
  • Parameter synchronization dialog is empty in some cases
  • Sorting of error messages via their category does not work properly (page "Error classification")
  • High memory consumption when accessing many parameter pages
  • Trace recording can only be read if the Plug-in is connected to the device when the trigger fires
  • Record list is not copied correctly when copying and pasting a device
  • Error log is not sorted correclty


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.30
  • CODESYS SoftMotion V4.0.14.0


Supported Systems:

  • servo drive CMMT-AS-...-11A-P3-... (5111189)
  • servo drive CMMT-AS-...-3A-... (5111184)
  • servo drive CMMT-AS-C2-11A-P3-EC-S1 (5340821)
  • servo drive CMMT-AS-C2-11A-P3-PN-S1 (5340816)
  • servo drive CMMT-AS-C2-3A-EC-S1 (5340819)
  • servo drive CMMT-AS-C2-3A-PN-S1 (5340814)
  • servo drive CMMT-AS-C3-11A-P3-EC-S1 (5340822)
  • servo drive CMMT-AS-C3-11A-P3-PN-S1 (5340817)
  • servo drive CMMT-AS-C4-3A-EC-S1 (5340820)
  • servo drive CMMT-AS-C4-3A-PN-S1 (5340815)
  • servo drive CMMT-AS-C5-11A-P3-EC-S1 (5340823)
  • servo drive CMMT-AS-C5-11A-P3-PN-S1 (5340818)
1.1.1.8
3/4/2019
FCT - Festo Configuration Tool - PlugIn 4/6/2019 Configuration and commissioning software for the motor controller CMMP-AS

 

Configuration and commissioning software for the motor controller CMMP-AS

  • FCT Plugin CMMP-AS V2.13.1.1 for Firmware V4.0.1501.2.4
  • FCT Plugin CMMP-AS V2.12.0.174 for Firmware V4.0.1501.2.4
  • FCT Plugin CMMP-AS V2.11.0.262 for Firmware V4.0.1501.2.4
  • FCT Plugin CMMP-AS V2.10.0.150 for Firmware V4.0.1501.2.4
  • FCT Plugin CMMP-AS V2.9.0.255 for Firmware V4.0.1501.2.4
  • FCT Plugin CMMP-AS V2.8.0.554 for Firmware V4.0.1501.2.3
  • FCT Plugin CMMP-AS V2.7.0.154 for Firmware V4.0.1501.2.3
  • FCT Plugin CMMP-AS V2.6.0.131 for Firmware V4.0.1501.2.3
  • Festo Configuration Tool V1.4.1.6



Supported systems:

  • Motor controller CMMP-AS-C10-11A-P3-M3 (1501328) Revision 04
  • Motor controller CMMP-AS-C10-11A-P3-M3-C1 (2106335) Revision 04
  • Motor controller CMMP-AS-C15-11A-P3-M3 (3215473)
  • Motor controller CMMP-AS-C2-3A-M3 (1501325) Revision 04
  • Motor controller CMMP-AS-C2-3A-M3-C1 (2106332) Revision 04
  • Motor controller CMMP-AS-C5-11A-P3-M3 (1501327) Revision 04
  • Motor controller CMMP-AS-C5-11A-P3-M3-C1 (2106334) Revision 04
  • Motor controller CMMP-AS-C5-3A-M3 (1501326) Revision 04
  • Motor controller CMMP-AS-C5-3A-M3-C1 (2106333) Revision 04
2.13.1.1
29/5/2019
Firmware 16/5/2019 Motion Terminal VTEM

firmware for VTEM

Supported systems:

  • Motion Terminal VTEM (8047502)
4.12.2
13/5/2019

Descargas más destacadas

CAD
Where can you obtain CAD data for Festo products? On the DVD-ROM version of the product catalogue from Festo, you can find CAD models of the products in all standard neutral formats.Our online catalogue provides up-to-date CAD data for almost all ...
FCT - Festo Configuration Tool CMMP-AS

Configuration and commissioning software for the motor controller: CMMP-AS

  • PlugIn for CMMP-AS v1.4.2.5 (FW V3.5.1501.5.3 or higher)
  • PlugIn for CMMP-AS v1.3.4.1 (FW V3.5.1501.4.3 or higher)
  • PlugIn for CMMP-AS v1.2.1.0 (FW V3.5.1501.3.1 or higher)
  • PlugIn for CMMP-AS v1.1.3.0 (FW V3.5.1501.2.1 or higher)
  • PlugIn for CMMP-AS v1.0.1.3 (FW V3.5.1501.1.1 or higher)
  • Festo Configuration Tool v1.2.1.3

    Supported systems:
  • Motor controller CMMP-AS-C10-11A-P3 (551024)
  • Motor controller CMMP-AS-C10-11A-P3-C1 (1669374)
  • Motor controller CMMP-AS-C20-11A-P3 (1366842)
  • Motor controller CMMP-AS-C2-3A (550041)
  • Motor controller CMMP-AS-C2-3A-C1 (1669371)
  • Motor controller CMMP-AS-C5-11A-P3 (551023)
  • Motor controller CMMP-AS-C5-11A-P3-C1 (1669373)
  • Motor controller CMMP-AS-C5-3A (550042)
  • Motor controller CMMP-AS-C5-3A-C1 (1669372)
1.4.2.5
1/8/2011
FCT - Festo Configuration Tool SFC-DC

Configuration and commissioning software for the motor controller: SFC-DC

  • FCT PlugIn SFC-DC V3.0.1.19 (I/O PB CO DN)
  • FCT PlugIn SFC-DC V2.3.0.204 (I/O PB CO DN)
  • FCT PlugIn SFC-DC V2.2.1.1 (I/O PB CO DN)
  • FCT PlugIn SFC-DC V2.1.0.209 (I/O PB CO)
  • FCT PlugIn SFC-DC V2.0.0.74 (I/O PB)
  • FCT PlugIn SFC-DC V1.0.1.6 (I/O)
  • Festo Configuration Tool v1.2.1.3
3.0.1.19
3/5/2013
Suscripción al RSS