21/11/2016

Gripping and transporting in suspension

Gripping and transporting in suspension

At SPS IPC Drives 2016 Festo demonstrates a future concept with superconductor technology
At the SPS IPC Drives 2016 trade fair, Festo is showcasing two innovative application concepts for superconductor technology.

Superconductors are opening up possibilities for entirely new, previously unthinkable applications in automation technology. They allow contact-free, frictionless manipulation of objects and bear great potentials for process automation: Their dust- and abrasion-free operation is ideal for the protective transport of workpieces in highly clean environments, machines can be easily cleaned and objects can even be moved from behind walls. At the SPS IPC Drives 2016 trade fair, Festo is showcasing the SupraTube and the SupraGripper – two innovative application concepts for superconductor technology.

 

Superconductors are materials which below a certain temperature can “freeze” the field of a permanent magnet at a predefined distance and can thus hold it in suspension. The resulting air gap remains stable in any spatial position. By this means, objects can be stored contact-free without any control technology and be moved with minimal expenditure of energy. Superconducting systems are suitable for bigger loads and can even work through walls and in all spatial planes across their definable hover gap. This enables objects to be handled in protected and enclosed spaces or through cladding. Areas prone to contamination or which are difficult to clean can thus be protected using smooth and easy-to-clean surfaces. If non-magnetic substances penetrate the bearing, the bearing and guiding function is not impaired. This also allows use in particularly highly contaminated areas.

 

SupraGripper: mechanical gripping despite spatial separation 

With the SupraGripper two grasping elements, each with three fingers, hover freely above two semicircular plates. This technology could enable objects to be grasped and transported within enclosed spaces – a practical solution for clean rooms or for working in liquids, gases or in vacuum.

 

The hovering effect is generated by three cryostats in all, which are installed beneath the plates and can be driven upwards or downwards. The grippers thus either hover above the plates or are set down onto them. In addition, the two plates can be rotated and precisely positioned by means of two rotary drives, so that the two grippers can be transported from one cryostat to the next.

 

To grasp an object, electrical spools fitted to the cryostats emit an impulse, which either severs the stored connection to the magnetic gripper elements or restores them, as required. This impulse causes the individual finger elements to fold upwards or downwards, which makes the grippers open or close.

 

SupraTube: rotation within an enclosed tube 

A round cryostat with superconductors is attached to the outside of each end of a liquid-filled glass tube. Inside the vertically oriented tube is a magnetic puck that is virtually tethered to the two cryostats with a levitation gap of around five millimetres and is initially suspended beneath the upper cryostat. A magnetic ring surrounding the cryostats is set into rotation by means of a stepper motor, which transfers this motion to the suspended magnet. The magnet is repelled from the cryostat by an electrical impulse and drifts downwards in a spiral motion. At the lower end, it is captured once more and centred by the superconductor in the other cryostat.

 

This exhibit shows how a controlled movement can be executed within a tube without direct intervention from the outside. In a slightly modified configuration, drive units with superconductive magnetic couplings could be fitted along the longitudinal axis of the tube in order to draw a cleaning unit through it, entirely free of contact. Alternatively, the contents of a closed container – such as hazardous substances or explosive gases – could be set in rotation.

 

Applications for production of the future

After several years of intensive research work, Festo is cooperating with partners and customers to examine their ideas for specific applications. “We are now not merely showing impressive levitation effects and the opportunities offered by superconductor technology, but are actively discussing their potential together with the automation industry. We are currently working together with selected customers towards initiating our first pilot projects”, said Georg Berner.

Contacto:

Annette Ostertag

+49(711)347-53830


Festo Media Service

 
 

Fotos

Pie de foto Download
Festo press pictures SupraGripper_1jpg With the SupraGripper two grasping elements, each with three fingers, hover freely above two semicircular plates. (Photo: Festo AG & Co. KG)
SupraGripper_2.jpg Beim SupraGripper schweben zwei Greifer mit je drei Fingern frei über zwei halbmondförmigen Platten. (Foto: Festo AG & Co. KG)
Festo press pictures SupraTube_1jpg SupraTube shows how a controlled movement can be executed within a tube without direct intervention from the outside. (Photo: Festo AG & Co. KG)
SupraTube_2jpg SupraTube shows how a controlled movement can be executed within a tube without direct intervention from the outside. (Photo: Festo AG & Co. KG)