13/11/2017

Flexible, yet standardized

Flexible, yet standardized

Servo presses and handling systems for connector assembly
The manufacturer Harwin safeguards production quality and flexibility using the servo press kit YJKP and the compact handling system YXMx.

Press   release Productronica 02/2017

 

Flexible,   yet standardized

Servo presses and handling systems for   connector assembly

 

Just   as PCBs have successfully managed to pack an increasing amount of power into   a smaller space, developers of plug   connectors are working to accommodate more power and a higher contact density   into smaller, lighter plug connectors. The family owned British manufacturer   Harwin plc relies on Festo automation to safeguard the quality and   flexibility of its production using equipment such as the servo press kit   YJKP and the compact handling system YXMx.

 

Harwin’s connectors are high quality, reliable and durable and can thus be used in harsh ambient conditions. They don’t only fit the bill for customers in industry sectors such as cost conscious consumer electronics, but also in the ultimate performance seekers such as aerospace, motor sports and the automotive industry, where extreme operating temperatures between –65 °C and +150 °C as well as severe vibrations are the order of the day. This means the connectors have to consistently be made to very high standards.

 

High standards

The response by Harwin to these market requirements has been to launch the Gecko range of connectors. These advanced connectors have a pin pitch of only 1.25 mm and are half the size and 75% lighter than micro D connectors. Their robust screw connection makes them extremely safe and reliable and able to withstand countless mating operations without damage.

 

The Gecko connector manufacturing process has been continuously refined from an initially manual process to today’s highly automated solution, capable of producing hundreds of thousands of connectors a year with a wide range of connector configurations ranging from 4 to 50 pins per connector and many PCB mounting options.

 

Modular concept

Harwin started developing a new production line with the aim of making the production of the Gecko series more efficient. Both a high level of automation and a high degree of flexibility were needed to be able to produce differently shaped and sized connectors on one assembly line. “That is why we developed a modular concept together with Festo,” explains Paul McGuinness, Operations Director at Harwin.

 

The new assembly lines at Harwin are built around the servo press kit YJKP and the compact handling system YXMx from Festo. The handling system takes care of the XY movements of the workpiece carriers and the plastic housings assembled in several of the system stations. The servo press kit, which provides easy-to-configure position- and force-controlled movement along the Z-axis, is used for press-fitting and bending the contact pins.

Standard parts

In all stations, the electric and pneumatic drives are each controlled by their own controller CECC-X together with a valve terminal CPX/MPA. “These Festo systems enable maximum standardisation and modularisation, as standard parts are used everywhere. This makes commissioning and maintenance easier,” explains McGuinness. One of the assembly lines for manufacturing the connectors consists of three central stations: for inserting, press-fitting and bending the contact pins.

 

In the first station, the workpiece carriers are equipped with the connector housings and are positioned using the compact handling system YXMx so the contact pins can be inserted. In the second station, the servo press presses the contact pins into the connector housing. The precision gripper HGPT from Festo locates the workpiece carriers holding the connector housings while the pins are fitted.

 

Dynamic and precise

The kinematics of the compact handling system enable dynamic and precise movement and ensure the connectors are precisely placed under the press-fitting tool. This works flawlessly thanks to the low moving mass. The modular servo press kit YJKP consists of a closed-loop servo motor, a mechanical axis, a motion controller, force detection as well application software. The result is precise, powerful and gentle movement of the pins to the correct position. Evaluation functions such as insertion or block force monitoring by the application software supplied detect whether the fit is within tolerance.

 

Modular and reliable

The handling system and the servo press kit are also used in the last station for bending the contact pins to the required angle. The CoDeSys software in the controller CECC-X allows comprehensive control of the servo press profile, providing position and force control throughout the cycle. The application software supplied with the servo press makes programming extremely easy thanks to an intuitive graphical user interface.

 

It makes it easy to adapt the press profile to the different connector variants without the need for special programming skills. Three valve terminals CPX controlled by the master controller CECC-X actuate the numerous electric and pneumatic grippers and actuators. “The automated modular concept ensures low production costs and high reliability, precision, repetition accuracy and flexibility,” explains automation expert McGuinness.

 

www.festo.com/yjkp

www.festo.com/yxmx

 

Text in a box:

Setting standards

The new assembly lines for electric connectors are not just setting high standards from a technical point of view, they are also a modular and scalable automation concept. The three main stations for inserting the pin contacts into the connector housings, press-fitting the pins and bending the pins are based on modules with as many standard parts as possible:

  • All three stations have a common base plate.
  • The moulded connector bodies are moved using the compact handling system YXMx.
  • All the electric and pneumatic actuators are controlled by a controller CECC-X in combination with a valve terminal CPX/MPA.
  • The press-fitting and bending stations use the servo press kit YJKP.

 

Please refer to:

Festo press photo: Harwin 1

 

                                                                          

Caption:

Modular design: the three stations of the   Gecko assembly line for inserting, press-fitting and bending the contact pins   – designed using standard components from Festo (Photo: Festo AG & Co.   KG)

 

About Festo:

Festo AG is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 40 industries. The products and services are available in 176 countries. With about 18,800 employees in over 250 branch offices in 61 countries worldwide, Festo achieved a turnover of around €2.74 billion in 2016. Each year around 8 % of this turnover is invested in research and development.

 

In this learning company, 1.5 % of turnover is invested in basic and further training. Yet training services are not only provided for Festo's own staff – Festo Didactic SE also supplies basic and further training programmes in the field of automation technology for customers, students and trainees.

 

About Harwin:

Harwin plc Europe is manufacturer of electric connectors and mechanical components for PCBs

www.harwin.com

 

 

 

 

 

 

Please refer to:

Festo press photo Paul McGuiness

 

         

Caption:

“The modular concept developed together   with Festo future-proofs our assembly lines” says Paul McGuinness, Operations   Director at Harwin (Photo:   Festo AG & Co. KG)

 

Please refer to:

Festo press photo Harwin 2

 

         

Caption:

Everything   for the servo press kit YJKP is available from a single source: drive   package, controller, and application software (Photo: Festo AG & Co. KG)

 

Please refer to:

Festo press photo Harwin 3

 

         

Caption:

Dynamic and precise: the   compact handling system YXMx takes care of the XY movement of the connectors   below the servo press (Photo: Festo AG & Co. KG)

 

Hierzu:

Festo   press photo: Harwin 4

 

       

Bildunterschrift:

Everything under control with the servo press kit   YJKP: controller CECC-X and motor controller   CMMP including application software. (Photo: Festo AG &Co. KG)

 

 

Please refer to:

Festo press photo electronics illustration   image

 

         

Caption:

Festo   – automation partner of electronics manufacturing (Photo: Festo AG & Co.   KG)

 

Press text and photos are also available online at www.festo.com/press.

Or mobile under http://m.festo.com/press.

 

For queries please contact:

Festo AG & Co. KG

Christopher Haug, Market Media Creation

phone: +49 711-347 4032, E-Mail: christopher.haug@festo.com

 

Festo in Social Media:

Facebook:    www.festo.com/facebook

Twitter:         www.festo.com/twitter

LinkedIn:      www.festo.com/linkedin

Youtube:      www.festo.com/youtube

Contacto:

Christopher Haug

+49(711)347-4032
+49(711)34754-4032

Festo Media Service

 
 

Fotos

Pie de foto Download
Harwin 1 Modular design: the three stations of the Gecko assembly line for inserting, press-fitting and bending the contact pins – designed using standard components from Festo (Photo: Festo AG & Co. KG)
Paul McGuiness “The modular concept developed together with Festo future-proofs our assembly lines” says Paul McGuinness, Operations Director at Harwin (Photo: Festo AG & Co. KG)
Harwin 2 Everything for the servo press kit YJKP is available from a single source: drive package, controller, and application software (Photo: Festo AG & Co. KG)
Harwin 3 Dynamic and precise: the compact handling system YXMx takes care of the XY movement of the connectors below the servo press (Photo: Festo AG & Co. KG)
Harwin 4 Everything under control with the servo press kit YJKP: controller CECC-X and motor controller CMMP including application software. (Photo: Festo AG &Co. KG)
electronics illustration image Festo – automation partner of electronics manufacturing (Photo: Festo AG & Co. KG)